Go to the source code of this file.
Definition in file usb_commun_cdc.h.
| #define CDC_GLOB_CLASS 0x02 |
Definition at line 48 of file usb_commun_cdc.h.
| #define CDC_COMM_CLASS 0x02 |
Definition at line 49 of file usb_commun_cdc.h.
| #define CDC_DATA_CLASS 0x0A |
Definition at line 50 of file usb_commun_cdc.h.
| #define CDC_GLOB_SUBCLASS 0x00 |
Definition at line 51 of file usb_commun_cdc.h.
| #define CDC_COMM_SUBCLASS 0x02 |
Definition at line 52 of file usb_commun_cdc.h.
| #define CDC_DATA_SUBCLASS 0x00 |
Definition at line 53 of file usb_commun_cdc.h.
| #define CDC_GLOB_PROTOCOL 0x00 |
Definition at line 54 of file usb_commun_cdc.h.
| #define CDC_COMM_PROTOCOL 0x01 |
Definition at line 55 of file usb_commun_cdc.h.
| #define CDC_DATA_PROTOCOL 0x00 |
Definition at line 56 of file usb_commun_cdc.h.
| #define SETUP_CDC_SEND_ENCAPSULATED_COMMAND 0x00 |
Definition at line 61 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_ENCAPSULATED_RESPONSE 0x01 |
Definition at line 62 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_COMM_FEATURE 0x02 |
Definition at line 63 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_COMM_FEATURE 0x03 |
Definition at line 64 of file usb_commun_cdc.h.
| #define SETUP_CDC_CLEAR_COMM_FEATURE 0x04 |
Definition at line 65 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_AUX_LINE_STATE 0x10 |
Definition at line 66 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_HOOK_STATE 0x11 |
Definition at line 67 of file usb_commun_cdc.h.
| #define SETUP_CDC_PULSE_SETUP 0x12 |
Definition at line 68 of file usb_commun_cdc.h.
| #define SETUP_CDC_SEND_PULSE 0x13 |
Definition at line 69 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_PULSE_TIME 0x14 |
Definition at line 70 of file usb_commun_cdc.h.
| #define SETUP_CDC_RING_AUX_JACK 0x15 |
Definition at line 71 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_LINE_CODING 0x20 |
Definition at line 72 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_LINE_CODING 0x21 |
Definition at line 73 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_CONTROL_LINE_STATE 0x22 |
Definition at line 74 of file usb_commun_cdc.h.
| #define SETUP_CDC_SEND_BREAK 0x23 |
Definition at line 75 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_RINGER_PARMS 0x30 |
Definition at line 76 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_RINGER_PARMS 0x31 |
Definition at line 77 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_OPERATION_PARMS 0x32 |
Definition at line 78 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_OPERATION_PARMS 0x33 |
Definition at line 79 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_LINE_PARMS 0x34 |
Definition at line 80 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_LINE_PARMS 0x35 |
Definition at line 81 of file usb_commun_cdc.h.
| #define SETUP_CDC_DIAL_DIGITS 0x36 |
Definition at line 82 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_UNIT_PARAMETER 0x37 |
Definition at line 83 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_UNIT_PARAMETER 0x38 |
Definition at line 84 of file usb_commun_cdc.h.
| #define SETUP_CDC_CLEAR_UNIT_PARAMETER 0x39 |
Definition at line 85 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_PROFILE 0x3A |
Definition at line 86 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_ETHERNET_MULTICAST_FILTERS 0x40 |
Definition at line 87 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_ETHERNET_POWER_MANAGEMENT_PATTERNFILTER 0x41 |
Definition at line 88 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_ETHERNET_POWER_MANAGEMENT_PATTERNFILTER 0x42 |
Definition at line 89 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_ETHERNET_PACKET_FILTER 0x43 |
Definition at line 90 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_ETHERNET_STATISTIC 0x44 |
Definition at line 91 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_ATM_DATA_FORMAT 0x50 |
Definition at line 92 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_ATM_DEVICE_STATISTICS 0x51 |
Definition at line 93 of file usb_commun_cdc.h.
| #define SETUP_CDC_SET_ATM_DEFAULT_VC 0x52 |
Definition at line 94 of file usb_commun_cdc.h.
| #define SETUP_CDC_GET_ATM_VC_STATISTICS 0x53 |
Definition at line 95 of file usb_commun_cdc.h.
| #define SETUP_CDC_BN_RING_DETECT 0x09 |
Definition at line 98 of file usb_commun_cdc.h.
| #define SETUP_CDC_BN_SERIAL_STATE 0x20 |
Definition at line 99 of file usb_commun_cdc.h.
| #define SETUP_CDC_BN_CALL_STATE_CHANGE 0x28 |
Definition at line 100 of file usb_commun_cdc.h.
| #define SETUP_CDC_BN_LINE_STATE_CHANGE 0x29 |
Definition at line 101 of file usb_commun_cdc.h.
1.5.3