#include "config.h"#include "conf_usb.h"#include "device_template_task.h"#include "lib_mcu/usb/usb_drv.h"#include "usb_descriptors.h"#include "modules/usb/device_chap9/usb_standard_request.h"#include "lib_mcu/wdt/wdt_drv.h"
Go to the source code of this file.
Functions | |
| void | device_template_task_init (void) |
| void | device_template_task (void) |
| void | sof_action () |
Variables | |
| volatile U8 | cpt_sof |
| U8 | buf [64] |
| U8 | rxok |
Definition in file device_template_task.c.
| void device_template_task_init | ( | void | ) |
This function initializes the hardware/software resources required for device application task.
| none |
Definition at line 81 of file device_template_task.c.
00082 { 00083 Joy_init(); 00084 Hwb_button_init(); 00085 Leds_init(); 00086 cpt_sof=0; 00087 Usb_enable_sof_interrupt(); 00088 rxok=FALSE; 00089 }
| void device_template_task | ( | void | ) |
Entry point of the device application This function links the application with the USB bus.
| none |
Definition at line 98 of file device_template_task.c.
00099 { 00100 U8 i; 00101 U8 *ptr; 00102 static U8 dummy_data; 00103 00104 //.. FIRST CHECK THE DEVICE ENUMERATION STATE 00105 if (Is_device_enumerated()) 00106 { 00107 //.. HERE START THE USB DEVICE APPLICATIVE CODE 00108 //.. The example bellow just perform a loop back transmition/reception 00109 //.. All data received wth the OUT endpoint are store in a ram buffer and 00110 //.. send back to the IN endpoint 00111 00112 //.. For example, blink a led with start of frame counter 00113 if(cpt_sof>0x7F) 00114 { Led0_on(); } 00115 else { Led0_off();} 00116 00117 //.. First interface management 00118 //.. Select the OUT endpoint declared in descriptors 00119 //.. load the endpoint with the content of a ram buffer for example 00120 Usb_select_endpoint(EP_TEMP_OUT); 00121 if ( Is_usb_receive_out()) 00122 { 00123 ptr=buf; 00124 for(i=Usb_byte_counter();i;i--) 00125 { 00126 *ptr++=Usb_read_byte(); 00127 } 00128 Usb_ack_receive_out(); 00129 rxok=TRUE; 00130 } 00131 //.. First interface management (cont) 00132 //.. Select the IN endpoint declared in descriptors 00133 //.. If we receive something, just store in the ram buffer 00134 Usb_select_endpoint(EP_TEMP_IN); 00135 if ( Is_usb_read_control_enabled()&&(rxok==TRUE)) 00136 { 00137 ptr=buf; 00138 for(i=0;i<EP_IN_LENGTH_TEMP1;i++) 00139 Usb_write_byte(*ptr++); 00140 Usb_ack_in_ready(); 00141 rxok=FALSE; 00142 } 00143 00144 //.. Second interface management (interrupt IN endpoint) 00145 //.. Just Send dummy data bytes 00146 Usb_select_endpoint(EP_TEMP_INT_IN); // Select this enpoint 00147 if (Is_usb_write_enabled()) // Check data can be loaded 00148 { // And load dummy data... 00149 Usb_write_byte(dummy_data); 00150 Usb_write_byte(dummy_data+1); 00151 Usb_write_byte(dummy_data+2); 00152 Usb_write_byte(dummy_data+3); 00153 Usb_ack_in_ready(); 00154 dummy_data+=4; 00155 } 00156 } 00157 }
Definition at line 65 of file device_template_task.c.
Referenced by device_template_task(), device_template_task_init(), and sof_action().
Definition at line 68 of file device_template_task.c.
Referenced by device_template_task(), and device_template_task_init().
1.5.3