#include "config.h"
Go to the source code of this file.
Defines | |
| #define | MMC_SECTOR_SIZE 512 |
| / 1 2 3 4 5 6 78 | <- view of MMC/SD card looking at contacts / 9 | Pins 8 and 9 are present only on SD cards | MMC/SD Card | | | |__________________| | |
| #define | byte_adr_of_block(ad) (ad<<9) |
| #define | MMC_CARD 0 |
| #define | SD_CARD 1 |
| #define | OP_UNLOCK 0x00 |
| #define | OP_LOCK 0x04 |
| #define | OP_RESET_PWD 0x02 |
| #define | OP_SET_PWD 0x01 |
| #define | OP_FORCED_ERASE 0x08 |
| #define | MMC_GO_IDLE_STATE 0 |
| initialize card to SPI-type access | |
| #define | MMC_SEND_OP_COND 1 |
| set card operational mode | |
| #define | MMC_CMD2 2 |
| illegal in SPI mode ! | |
| #define | MMC_SEND_CSD 9 |
| get card's CSD | |
| #define | MMC_SEND_CID 10 |
| get card's CID | |
| #define | MMC_SEND_STATUS 13 |
| #define | MMC_SET_BLOCKLEN 16 |
| Set number of bytes to transfer per block. | |
| #define | MMC_READ_SINGLE_BLOCK 17 |
| read a block | |
| #define | MMC_WRITE_BLOCK 24 |
| write a block | |
| #define | MMC_PROGRAM_CSD 27 |
| #define | MMC_SET_WRITE_PROT 28 |
| #define | MMC_CLR_WRITE_PROT 29 |
| #define | MMC_SEND_WRITE_PROT 30 |
| #define | SD_TAG_WR_ERASE_GROUP_START 32 |
| #define | SD_TAG_WR_ERASE_GROUP_END 33 |
| #define | MMC_TAG_SECTOR_START 32 |
| #define | MMC_TAG_SECTOR_END 33 |
| #define | MMC_UNTAG_SECTOR 34 |
| #define | MMC_TAG_ERASE_GROUP_START 35 |
| Sets beginning of erase group (mass erase). | |
| #define | MMC_TAG_ERASE_GROUP_END 36 |
| Sets end of erase group (mass erase). | |
| #define | MMC_UNTAG_ERASE_GROUP 37 |
| Untag (unset) erase group (mass erase). | |
| #define | MMC_ERASE 38 |
| Perform block/mass erase. | |
| #define | SD_SEND_OP_COND_ACMD 41 |
| Same as MMC_SEND_OP_COND but specific to SD (must be preceeded by CMD55). | |
| #define | MMC_LOCK_UNLOCK 42 |
| To start a lock/unlock/pwd operation. | |
| #define | SD_APP_CMD55 55 |
| Use before any specific command (type ACMD). | |
| #define | MMC_CRC_ON_OFF 59 |
| Turns CRC check on/off. | |
| #define | MMC_R1_BUSY 0x80 |
| R1 response: bit indicates card is busy. | |
| #define | MMC_R1_PARAMETER 0x40 |
| #define | MMC_R1_ADDRESS 0x20 |
| #define | MMC_R1_ERASE_SEQ 0x10 |
| #define | MMC_R1_COM_CRC 0x08 |
| #define | MMC_R1_ILLEGAL_COM 0x04 |
| #define | MMC_R1_ERASE_RESET 0x02 |
| #define | MMC_R1_IDLE_STATE 0x01 |
| #define | MMC_STARTBLOCK_READ 0xFE |
| when received from card, indicates that a block of data will follow | |
| #define | MMC_STARTBLOCK_WRITE 0xFE |
| when sent to card, indicates that a block of data will follow | |
| #define | MMC_STARTBLOCK_MWRITE 0xFC |
| #define | MMC_STOPTRAN_WRITE 0xFD |
| #define | MMC_DE_MASK 0x1F |
| #define | MMC_DE_ERROR 0x01 |
| #define | MMC_DE_CC_ERROR 0x02 |
| #define | MMC_DE_ECC_FAIL 0x04 |
| #define | MMC_DE_OUT_OF_RANGE 0x04 |
| #define | MMC_DE_CARD_LOCKED 0x04 |
| #define | MMC_DR_MASK 0x1F |
| #define | MMC_DR_ACCEPT 0x05 |
| #define | MMC_DR_REJECT_CRC 0x0B |
| #define | MMC_DR_REJECT_WRITE_ERROR 0x0D |
Functions | |
| void | mmc_sd_spi_init (void) |
| Low-level functions (basic management). | |
| bit | mmc_sd_init (void) |
| bit | mmc_sd_check_presence (void) |
| bit | mmc_sd_mem_check (void) |
| bit | mmc_sd_wait_not_busy (void) |
| bit | mmc_sd_get_csd (U8 *) |
| bit | mmc_sd_get_cid (U8 *) |
| void | mmc_sd_get_capacity (void) |
| bit | mmc_sd_get_status (void) |
| U8 | mmc_sd_send_and_read (U8) |
| U8 | mmc_sd_send_command (U8, U32) |
| U8 | mmc_sd_command (U8, U32) |
| bit | is_mmc_sd_write_pwd_locked (void) |
| Protection functions (optionnal). | |
| bit | mmc_sd_lock_operation (U8, U8, U8 *) |
| bit | mmc_sd_read_open (U32) |
| Functions for preparing block read/write. | |
| void | mmc_sd_read_close (void) |
| bit | mmc_sd_write_open (U32) |
| void | mmc_sd_write_close (void) |
| bit | mmc_sd_write_sector (U16) |
| Funtions to link USB DEVICE flow with MMC. | |
| bit | mmc_sd_read_sector (U16) |
| bit | mmc_sd_read_sector_to_ram (U8 *ram) |
| Functions to read/write one sector (512btes) with ram buffer pointer. | |
| bit | mmc_sd_write_sector_from_ram (U8 *ram) |
| bit | mmc_sd_erase_sector_group (U32, U32) |
Variables | |
| U8 | csd [16] |
| volatile U32 | capacity |
| volatile U32 | mmc_sd_last_block_address |
| U16 | erase_group_size |
| U8 | r1 |
| U16 | r2 |
| U8 | card_type |
| bit | mmc_sd_init_done |
Definition in file mmc_sd.h.
| #define MMC_SECTOR_SIZE 512 |
/ 1 2 3 4 5 6 78 | <- view of MMC/SD card looking at contacts / 9 | Pins 8 and 9 are present only on SD cards | MMC/SD Card | | | |__________________|
1 - CS (chip select) - wire to any available I/O pin(*) 2 - DIN (data in, card<-host) - wire to SPI MOSI pin 3 - VSS (ground) - wire to ground 4 - VDD (power, 3.3V only?) - wire to power (MIGHT BE 3.3V ONLY!) 5 - SCLK (data clock) - wire to SPI SCK pin 6 - VSS (ground) - wire to ground 7 - DOUT (data out, card->host) - wire to SPI MISO pin
Definition at line 70 of file mmc_sd.h.
Referenced by mmc_sd_read_sector_to_ram(), and mmc_sd_write_sector_from_ram().
| #define MMC_CARD 0 |
Definition at line 78 of file mmc_sd.h.
Referenced by is_mmc_sd_write_pwd_locked(), mmc_sd_erase_sector_group(), mmc_sd_get_capacity(), and mmc_sd_init().
| #define SD_CARD 1 |
| #define OP_FORCED_ERASE 0x08 |
| #define MMC_GO_IDLE_STATE 0 |
initialize card to SPI-type access
Definition at line 89 of file mmc_sd.h.
Referenced by mmc_sd_check_presence(), and mmc_sd_init().
| #define MMC_SEND_OP_COND 1 |
| #define MMC_SEND_CSD 9 |
| #define MMC_SEND_CID 10 |
| #define MMC_SEND_STATUS 13 |
| #define MMC_SET_BLOCKLEN 16 |
Set number of bytes to transfer per block.
Definition at line 95 of file mmc_sd.h.
Referenced by mmc_sd_init(), and mmc_sd_lock_operation().
| #define MMC_READ_SINGLE_BLOCK 17 |
read a block
Definition at line 96 of file mmc_sd.h.
Referenced by mmc_sd_read_sector(), and mmc_sd_read_sector_to_ram().
| #define MMC_WRITE_BLOCK 24 |
write a block
Definition at line 97 of file mmc_sd.h.
Referenced by mmc_sd_write_sector(), and mmc_sd_write_sector_from_ram().
| #define SD_TAG_WR_ERASE_GROUP_START 32 |
| #define SD_TAG_WR_ERASE_GROUP_END 33 |
| #define MMC_TAG_ERASE_GROUP_START 35 |
Sets beginning of erase group (mass erase).
Definition at line 107 of file mmc_sd.h.
Referenced by mmc_sd_erase_sector_group().
| #define MMC_TAG_ERASE_GROUP_END 36 |
Sets end of erase group (mass erase).
Definition at line 108 of file mmc_sd.h.
Referenced by mmc_sd_erase_sector_group().
| #define MMC_UNTAG_ERASE_GROUP 37 |
| #define MMC_ERASE 38 |
Perform block/mass erase.
Definition at line 110 of file mmc_sd.h.
Referenced by mmc_sd_erase_sector_group().
| #define SD_SEND_OP_COND_ACMD 41 |
Same as MMC_SEND_OP_COND but specific to SD (must be preceeded by CMD55).
Definition at line 111 of file mmc_sd.h.
Referenced by mmc_sd_init().
| #define MMC_LOCK_UNLOCK 42 |
To start a lock/unlock/pwd operation.
Definition at line 112 of file mmc_sd.h.
Referenced by mmc_sd_lock_operation().
| #define SD_APP_CMD55 55 |
Use before any specific command (type ACMD).
Definition at line 113 of file mmc_sd.h.
Referenced by mmc_sd_init().
| #define MMC_CRC_ON_OFF 59 |
Turns CRC check on/off.
Definition at line 114 of file mmc_sd.h.
Referenced by mmc_sd_check_presence(), and mmc_sd_init().
| #define MMC_R1_BUSY 0x80 |
| #define MMC_STARTBLOCK_READ 0xFE |
when received from card, indicates that a block of data will follow
Definition at line 125 of file mmc_sd.h.
Referenced by mmc_sd_get_cid(), mmc_sd_get_csd(), mmc_sd_read_sector(), and mmc_sd_read_sector_to_ram().
| #define MMC_STARTBLOCK_WRITE 0xFE |
when sent to card, indicates that a block of data will follow
Definition at line 126 of file mmc_sd.h.
Referenced by mmc_sd_lock_operation(), mmc_sd_write_sector(), and mmc_sd_write_sector_from_ram().
| #define MMC_DR_MASK 0x1F |
Definition at line 138 of file mmc_sd.h.
Referenced by mmc_sd_lock_operation(), mmc_sd_write_sector(), and mmc_sd_write_sector_from_ram().
| #define MMC_DR_ACCEPT 0x05 |
Definition at line 139 of file mmc_sd.h.
Referenced by mmc_sd_lock_operation(), mmc_sd_write_sector(), and mmc_sd_write_sector_from_ram().
| void mmc_sd_spi_init | ( | void | ) |
Low-level functions (basic management).
This function initializes the SPI communication link between the MMC_SD and the MMC_SD driver.
| none |
Definition at line 88 of file mmc_sd.c.
00089 { 00090 Spi_select_master(); 00091 Spi_set_mode(SPI_MODE_0); 00092 Spi_init_bus(); 00093 Spi_set_rate(SPI_RATE_0); // SCK freq == fosc/2. 00094 Spi_disable_ss(); 00095 Spi_enable(); 00096 }
| bit mmc_sd_init | ( | void | ) |
This function initializes the Dataflash controller & the SPI bus(over which the MMC_SD is controlled).
| none |
Definition at line 110 of file mmc_sd.c.
References card_type, cid, csd, FALSE, KO, MMC_CARD, MMC_CRC_ON_OFF, MMC_GO_IDLE_STATE, mmc_sd_get_capacity(), mmc_sd_get_cid(), mmc_sd_get_csd(), mmc_sd_init_done, mmc_sd_send_command(), mmc_sd_spi_init(), MMC_SEND_OP_COND, MMC_SET_BLOCKLEN, OK, r1, SD_APP_CMD55, SD_CARD, SD_SEND_OP_COND_ACMD, Spi_write_data, and TRUE.
00111 { 00112 U16 retry; 00113 00114 // INIT HARDWARE 00115 mmc_sd_spi_init(); 00116 00117 // RESET THE MEMORY CARD 00118 mmc_sd_init_done = FALSE; 00119 card_type = MMC_CARD; 00120 retry = 0; 00121 do 00122 { 00123 // reset card and go to SPI mode 00124 r1 = mmc_sd_send_command(MMC_GO_IDLE_STATE, 0); 00125 Spi_write_data(0xFF); // write dummy byte 00126 // do retry counter 00127 retry++; 00128 if(retry > 100) 00129 return KO; 00130 } 00131 while(r1 != 0x01); // check memory enters idle_state 00132 00133 // IDENTIFICATION OF THE CARD TYPE (SD or MMC) 00134 // Both cards will accept CMD55 command but only the SD card will respond to ACMD41 00135 r1 = mmc_sd_send_command(SD_APP_CMD55,0); 00136 Spi_write_data(0xFF); // write dummy byte 00137 00138 r1 = mmc_sd_send_command(SD_SEND_OP_COND_ACMD, 0); 00139 Spi_write_data(0xFF); // write dummy byte 00140 00141 if ((r1&0xFE) == 0) // ignore "in_idle_state" flag bit 00142 { 00143 card_type = SD_CARD; // card has accepted the command, this is a SD card 00144 } 00145 else 00146 { 00147 card_type = MMC_CARD; // card has not responded, this is a MMC card 00148 // reset card again 00149 retry = 0; 00150 do 00151 { 00152 // reset card again 00153 r1 = mmc_sd_send_command(MMC_GO_IDLE_STATE, 0); 00154 Spi_write_data(0xFF); // write dummy byte 00155 // do retry counter 00156 retry++; 00157 if(retry > 100) 00158 return KO; 00159 } 00160 while(r1 != 0x01); // check memory enters idle_state 00161 } 00162 00163 // CONTINUE INTERNAL INITIALIZATION OF THE CARD 00164 // Continue sending CMD1 while memory card is in idle state 00165 retry = 0; 00166 do 00167 { 00168 // initializing card for operation 00169 r1 = mmc_sd_send_command(MMC_SEND_OP_COND, 0); 00170 Spi_write_data(0xFF); // write dummy byte 00171 // do retry counter 00172 retry++; 00173 if(retry == 50000) // measured approx. 500 on several cards 00174 return KO; 00175 } 00176 while (r1); 00177 00178 // DISABLE CRC TO SIMPLIFY AND SPEED UP COMMUNICATIONS 00179 r1 = mmc_sd_send_command(MMC_CRC_ON_OFF, 0); // disable CRC (should be already initialized on SPI init) 00180 Spi_write_data(0xFF); // write dummy byte 00181 00182 // SET BLOCK LENGTH TO 512 BYTES 00183 r1 = mmc_sd_send_command(MMC_SET_BLOCKLEN, 512); 00184 Spi_write_data(0xFF); // write dummy byte 00185 if (r1 != 0x00) 00186 return KO; // card unsupported if block length of 512b is not accepted 00187 00188 // GET CARD SPECIFIC DATA 00189 if (KO == mmc_sd_get_csd(csd)) 00190 return KO; 00191 00192 // GET CARD CAPACITY and NUMBER OF SECTORS 00193 mmc_sd_get_capacity(); 00194 00195 // GET CARD IDENTIFICATION DATA IF REQUIRED 00196 #if (MMC_SD_READ_CID == ENABLED) 00197 if (KO == mmc_sd_get_cid(cid)) 00198 return KO; 00199 #endif 00200 00201 mmc_sd_init_done = TRUE; 00202 00203 return(OK); 00204 }
| bit mmc_sd_check_presence | ( | void | ) |
This function check the presence of a memory card
| none |
Definition at line 559 of file mmc_sd.c.
References FALSE, KO, MMC_CRC_ON_OFF, MMC_GO_IDLE_STATE, mmc_sd_init_done, mmc_sd_send_command(), OK, r1, and Spi_write_data.
00560 { 00561 U16 retry; 00562 00563 retry = 0; 00564 if (mmc_sd_init_done == FALSE) 00565 { 00566 // If memory is not initialized, try to initialize it (CMD0) 00567 // If no valid response, there is no card 00568 while ((r1 = mmc_sd_send_command(MMC_GO_IDLE_STATE, 0)) != 0x01) 00569 { 00570 Spi_write_data(0xFF); // write dummy byte 00571 retry++; 00572 if (retry > 10) 00573 return KO; 00574 } 00575 return OK; 00576 } 00577 else 00578 { 00579 // If memory already initialized, send a CRC command (CMD59) (supported only if card is initialized) 00580 /* 00581 retry = 0; 00582 while (retry != 50000) 00583 { 00584 r1 = mmc_sd_send_command(MMC_CMD2,0); // unsupported command in SPI mode 00585 Spi_write_data(0xFF); // write dummy byte 00586 if (r1 != 0) // memory must answer with an error code (with bit7=0) 00587 { 00588 if (r1 < 0x80) 00589 return OK; 00590 else 00591 { 00592 mmc_sd_init_done = FALSE; 00593 return KO; 00594 } 00595 } 00596 retry++; 00597 } 00598 */ 00599 if ((r1 = mmc_sd_send_command(MMC_CRC_ON_OFF,0)) == 0x00) 00600 return OK; 00601 mmc_sd_init_done = FALSE; 00602 return KO; 00603 } 00604 00605 return KO; 00606 }
| bit mmc_sd_mem_check | ( | void | ) |
This function performs a memory check on the MMC_SD.
| none |
Definition at line 621 of file mmc_sd.c.
References FALSE, KO, mmc_sd_check_presence(), mmc_sd_init(), mmc_sd_init_done, OK, and TRUE.
00622 { 00623 if (mmc_sd_check_presence() == OK) 00624 { 00625 if (mmc_sd_init_done == FALSE) 00626 { 00627 mmc_sd_init(); 00628 } 00629 if (mmc_sd_init_done == TRUE) 00630 return OK; 00631 else 00632 return KO; 00633 } 00634 return KO; 00635 }
| bit mmc_sd_wait_not_busy | ( | void | ) |
This function waits until the MMC/SD is not busy.
| None |
Definition at line 524 of file mmc_sd.c.
References KO, Mmc_sd_select, mmc_sd_send_and_read(), Mmc_sd_unselect, OK, and r1.
00525 { 00526 U16 retry; 00527 00528 // Select the MMC_SD memory gl_ptr_mem points to 00529 Mmc_sd_select(); 00530 retry = 0; 00531 while((r1 = mmc_sd_send_and_read(0xFF)) != 0xFF) 00532 { 00533 retry++; 00534 if (retry == 50000) 00535 { 00536 Mmc_sd_unselect(); 00537 return KO; 00538 } 00539 } 00540 Mmc_sd_unselect(); 00541 return OK; 00542 }
| bit mmc_sd_get_csd | ( | U8 * | buffer | ) |
This function reads the CSD (Card Specific Data) of the memory card
| buffer | to fill |
Definition at line 296 of file mmc_sd.c.
References FALSE, KO, mmc_sd_command(), mmc_sd_init_done, Mmc_sd_select, mmc_sd_send_and_read(), Mmc_sd_unselect, mmc_sd_wait_not_busy(), MMC_SEND_CSD, MMC_STARTBLOCK_READ, OK, r1, Spi_read_data, and Spi_write_data.
00297 { 00298 U8 retry; 00299 00300 // wait for MMC not busy 00301 if (KO == mmc_sd_wait_not_busy()) 00302 return KO; 00303 00304 Mmc_sd_select(); // select MMC_SD 00305 // issue command 00306 r1 = mmc_sd_command(MMC_SEND_CSD, 0); 00307 // check for valid response 00308 if(r1 != 0x00) 00309 { 00310 Mmc_sd_unselect(); // unselect MMC_SD 00311 mmc_sd_init_done = FALSE; 00312 return KO; 00313 } 00314 // wait for block start 00315 retry = 0; 00316 while((r1 = mmc_sd_send_and_read(0xFF)) != MMC_STARTBLOCK_READ) 00317 { 00318 if (retry > 8) 00319 { 00320 Mmc_sd_unselect(); // unselect MMC_SD 00321 return KO; 00322 } 00323 retry++; 00324 } 00325 for (retry = 0; retry <16; retry++) 00326 { 00327 Spi_write_data(0xFF); 00328 buffer[retry] = Spi_read_data(); 00329 } 00330 Spi_write_data(0xFF); // load CRC (not used) 00331 Spi_write_data(0xFF); 00332 Spi_write_data(0xFF); // give clock again to end transaction 00333 Mmc_sd_unselect(); // unselect MMC_SD 00334 return OK; 00335 }
| bit mmc_sd_get_cid | ( | U8 * | buffer | ) |
This function reads the CID (Card Identification Data) of the memory card
| buffer | to fill |
Definition at line 349 of file mmc_sd.c.
References FALSE, KO, mmc_sd_command(), mmc_sd_init_done, Mmc_sd_select, mmc_sd_send_and_read(), Mmc_sd_unselect, mmc_sd_wait_not_busy(), MMC_SEND_CID, MMC_STARTBLOCK_READ, OK, r1, r2, Spi_read_data, and Spi_write_data.
00350 { 00351 U8 retry; 00352 00353 // wait for MMC not busy 00354 if (KO == mmc_sd_wait_not_busy()) 00355 return KO; 00356 00357 Mmc_sd_select(); // select MMC_SD 00358 // issue command 00359 r1 = mmc_sd_command(MMC_SEND_CID, 0); 00360 // check for valid response 00361 if(r1 != 0x00) 00362 { 00363 Mmc_sd_unselect(); // unselect MMC_SD 00364 mmc_sd_init_done = FALSE; 00365 return KO; 00366 } 00367 // wait for data block start 00368 retry = 0; 00369 while((r2 = mmc_sd_send_and_read(0xFF)) != MMC_STARTBLOCK_READ) 00370 { 00371 if (retry > 8) 00372 { 00373 Mmc_sd_unselect(); // unselect MMC_SD 00374 return KO; 00375 } 00376 retry++; 00377 } 00378 // store valid data block 00379 for (retry = 0; retry <16; retry++) 00380 { 00381 Spi_write_data(0xFF); 00382 buffer[retry] = Spi_read_data(); 00383 } 00384 Spi_write_data(0xFF); // load CRC (not used) 00385 Spi_write_data(0xFF); 00386 Spi_write_data(0xFF); // give clock again to end transaction 00387 Mmc_sd_unselect(); // unselect MMC_SD 00388 return OK; 00389 }
| void mmc_sd_get_capacity | ( | void | ) |
This function extracts structure information from CSD array and compute the number of blocks of the memory card (stored in global U32 mmc_sd_last_block_address), its capacity in bytes (stored in global U32 capacity) and the block group size for an erase operation Here is defined the position of required fields in CSD array : READ_BL_LEN : [83:80] == data[5] && 0x0f C_SIZE : [73:72] == data[6] && 0x03 [71:64] == data[7] [63:62] == data[8] && 0xc0 C_SIZE_MULT : [49:48] == data[9] && 0x03 [47] == data[10] && 0x80 ERASE_GRP_SIZE (MMC card only) : [46:42] == data[10] && 0x7c ERASE_GRP_MULT (MMC card only) : [41:40] == data[10] && 0x03 [39:37] == data[11] && 0xe0 SECTOR_SIZE (SD card only) : [45:40] == data[10] && 0x3F [39] == data[11] && 0x80
| None |
Definition at line 424 of file mmc_sd.c.
References capacity, card_type, csd, erase_group_size, MMC_CARD, and mmc_sd_last_block_address.
00425 { 00426 U16 c_size; 00427 U8 c_size_mult; 00428 U8 read_bl_len; 00429 U8 erase_grp_size; 00430 U8 erase_grp_mult; 00431 00432 // extract variables from CSD array 00433 c_size = ((csd[6] & 0x03) << 10) + (csd[7] << 2) + ((csd[8] & 0xC0) >> 6); 00434 c_size_mult = ((csd[9] & 0x03) << 1) + ((csd[10] & 0x80) >> 7); 00435 read_bl_len = csd[5] & 0x0F; 00436 if (card_type == MMC_CARD) 00437 { 00438 erase_grp_size = ((csd[10] & 0x7C) >> 2); 00439 erase_grp_mult = ((csd[10] & 0x03) << 3) | ((csd[11] & 0xE0) >> 5); 00440 } 00441 else 00442 { 00443 erase_grp_size = ((csd[10] & 0x3F) << 1) + ((csd[11] & 0x80) >> 7); 00444 erase_grp_mult = 0; 00445 } 00446 00447 // compute last block addr 00448 mmc_sd_last_block_address = ((U32)(c_size + 1) * (U32)((1 << (c_size_mult + 2)))) - 1; 00449 if (read_bl_len > 9) // 9 means 2^9 = 512b 00450 mmc_sd_last_block_address <<= (read_bl_len - 9); 00451 00452 // compute card capacity in bytes 00453 capacity = (1 << read_bl_len) * (mmc_sd_last_block_address + 1); 00454 00455 // compute block group size for erase operation 00456 erase_group_size = (erase_grp_size + 1) * (erase_grp_mult + 1); 00457 }
| bit mmc_sd_get_status | ( | void | ) |
This function reads the STATUS regsiter of the memory card After a read the error flags are automatically cleared
| None |
Definition at line 472 of file mmc_sd.c.
References KO, Mmc_sd_select, mmc_sd_send_and_read(), Mmc_sd_unselect, mmc_sd_wait_not_busy(), MMC_SEND_STATUS, OK, r2, and Spi_write_data.
00473 { 00474 U8 retry, spireg; 00475 00476 // wait for MMC not busy 00477 if (KO == mmc_sd_wait_not_busy()) 00478 return KO; 00479 00480 Mmc_sd_select(); // select MMC_SD 00481 00482 // send command 00483 Spi_write_data(MMC_SEND_STATUS | 0x40); // send command 00484 Spi_write_data(0); // send parameter 00485 Spi_write_data(0); 00486 Spi_write_data(0); 00487 Spi_write_data(0); 00488 Spi_write_data(0x95); // correct CRC for first command in SPI (CMD0) 00489 // after, the CRC is ignored 00490 // end command 00491 // wait for response 00492 // if more than 8 retries, card has timed-out and return the received 0xFF 00493 retry = 0; 00494 r2 = 0xFFFF; 00495 spireg = 0xFF; 00496 while((spireg = mmc_sd_send_and_read(0xFF)) == 0xFF) 00497 { 00498 retry++; 00499 if(retry > 10) 00500 { 00501 Mmc_sd_unselect(); 00502 return KO; 00503 } 00504 } 00505 r2 = ((U16)(spireg) << 8) + mmc_sd_send_and_read(0xFF); // first byte is MSb 00506 00507 Spi_write_data(0xFF); // give clock again to end transaction 00508 Mmc_sd_unselect(); // unselect MMC_SD 00509 00510 return OK; 00511 }
This function sends a byte over SPI and returns the byte read from the slave.
| data_to_send | byte to send over SPI |
Definition at line 278 of file mmc_sd.c.
References Spi_read_data, and Spi_write_data.
00279 { 00280 Spi_write_data(data_to_send); 00281 return (Spi_read_data()); 00282 }
This function sends a command WITH NO DATA STATE to the SD/MMC and waits for R1 response This function also selects and unselects the memory => should be used only for single command transmission
| command | command to send (see mmc_sd.h for command list) arg argument of the command |
Definition at line 220 of file mmc_sd.c.
References mmc_sd_command(), Mmc_sd_select, Mmc_sd_unselect, and r1.
00221 { 00222 Mmc_sd_select(); // select MMC_SD 00223 r1 = mmc_sd_command(command, arg); 00224 Mmc_sd_unselect(); // unselect MMC_SD 00225 return r1; 00226 }
This function sends a command WITH DATA STATE to the SD/MMC and waits for R1 response The memory /CS signal is not affected so this function can be used to send a commande during a large transmission
| command | command to send (see mmc_sd.h for command list) arg argument of the command |
Definition at line 240 of file mmc_sd.c.
References mmc_sd_send_and_read(), r1, and Spi_write_data.
00241 { 00242 U8 retry; 00243 00244 Spi_write_data(0xFF); // write dummy byte 00245 Spi_write_data(command | 0x40); // send command 00246 Spi_write_data(arg>>24); // send parameter 00247 Spi_write_data(arg>>16); 00248 Spi_write_data(arg>>8 ); 00249 Spi_write_data(arg ); 00250 Spi_write_data(0x95); // correct CRC for first command in SPI (CMD0) 00251 // after, the CRC is ignored 00252 // end command 00253 // wait for response 00254 // if more than 8 retries, card has timed-out and return the received 0xFF 00255 retry = 0; 00256 r1 = 0xFF; 00257 while((r1 = mmc_sd_send_and_read(0xFF)) == 0xFF) 00258 { 00259 retry++; 00260 if(retry > 10) break; 00261 } 00262 return r1; 00263 }
| bit is_mmc_sd_write_pwd_locked | ( | void | ) |
Protection functions (optionnal).
This function checks if the card is password-locked Old versions of MMC card don't support this feature ! For a MMC, "lock protection" is featured from v2.1 release ! => see CSD[0]<5:2> bits to know the version : 0x0=1.x, 0x1=1.4, 0x2=2.x, 0x3=3.x, 0x4=4.0
| None |
Definition at line 653 of file mmc_sd.c.
References card_type, csd, KO, MMC_CARD, mmc_sd_get_status(), OK, and r2.
00654 { 00655 if (card_type == MMC_CARD) 00656 { 00657 if (((csd[0] >> 2) & 0x0F) < 2) // lock feature is not present on the card since the MMC is v1.x released ! 00658 return KO; 00659 } 00660 if (KO == mmc_sd_get_status()) // get STATUS response 00661 return KO; 00662 if ((r2&0x0001) != 0) // check "card is locked" flag in R2 response 00663 return OK; 00664 00665 return KO; 00666 }
This function manages locking operations for the SD/MMC card (password protection)
| U8 | operation OP_LOCK -> to lock the card (the current pasword must be specified) OP_UNLOCK -> to unlock the card (the current password must be specified) OP_RESET_PWD -> to clear the current password (the current password must be specified) OP_SET_PWD -> to set a new password to the card (the old password must have been cleared first) OP_FORCED_ERASE -> to erase completely the card and the password (no password needed) U8 pwd_lg Password length U8 * pwd Pointer on the password (char array) to send |
Definition at line 698 of file mmc_sd.c.
References KO, MMC_DR_ACCEPT, MMC_DR_MASK, MMC_LOCK_UNLOCK, mmc_sd_command(), mmc_sd_get_status(), Mmc_sd_select, mmc_sd_send_and_read(), mmc_sd_send_command(), Mmc_sd_unselect, mmc_sd_wait_not_busy(), MMC_SET_BLOCKLEN, MMC_STARTBLOCK_WRITE, OK, OP_FORCED_ERASE, r1, r2, and Spi_write_data.
00699 { 00700 bit status = OK; 00701 U8 retry; 00702 00703 // check parameters validity 00704 if ((operation != OP_FORCED_ERASE) && (pwd_lg == 0)) // password length must be > 0 00705 return KO; 00706 00707 // wait card not busy 00708 if (mmc_sd_wait_not_busy() == KO) 00709 return KO; 00710 00711 // set block length 00712 if (operation == OP_FORCED_ERASE) 00713 r1 = mmc_sd_send_command(MMC_SET_BLOCKLEN, 1); // CMD 00714 else 00715 r1 = mmc_sd_send_command(MMC_SET_BLOCKLEN, pwd_lg+2); // CMD + PWDSLEN + PWD 00716 Spi_write_data(0xFF); // write dummy byte 00717 Spi_write_data(0xFF); // write dummy byte 00718 Spi_write_data(0xFF); // write dummy byte 00719 if (r1 != 0x00) 00720 return KO; 00721 00722 // send the lock command to the card 00723 Mmc_sd_select(); // select MMC_SD 00724 00725 // issue command 00726 r1 = mmc_sd_command(MMC_LOCK_UNLOCK, 0); 00727 00728 // check for valid response 00729 if(r1 != 0x00) 00730 { 00731 status = KO; 00732 } 00733 // send dummy 00734 Spi_write_data(0xFF); // give clock again to end transaction 00735 00736 // send data start token 00737 Spi_write_data(MMC_STARTBLOCK_WRITE); 00738 // write data 00739 Spi_write_data(operation); 00740 if (operation != OP_FORCED_ERASE) 00741 { 00742 Spi_write_data(pwd_lg); 00743 for(retry=0 ; retry<pwd_lg ; retry++) 00744 { 00745 Spi_write_data(*(pwd+retry)); 00746 } 00747 } 00748 Spi_write_data(0xFF); // send CRC (field required but value ignored) 00749 Spi_write_data(0xFF); 00750 00751 // check data response token 00752 retry = 0; 00753 r1 = mmc_sd_send_and_read(0xFF); 00754 if ((r1 & MMC_DR_MASK) != MMC_DR_ACCEPT) 00755 status = KO; 00756 00757 Spi_write_data(0xFF); // dummy byte 00758 Mmc_sd_unselect(); 00759 00760 // wait card not busy 00761 if (operation == OP_FORCED_ERASE) 00762 retry = 100; 00763 else 00764 retry = 10; 00765 while (mmc_sd_wait_not_busy() == KO) 00766 { 00767 retry--; 00768 if (retry == 0) 00769 { 00770 status = KO; 00771 break; 00772 } 00773 } 00774 00775 // get and check status of the operation 00776 if (KO == mmc_sd_get_status()) // get STATUS response 00777 status = KO; 00778 if ((r2&0x0002) != 0) // check "lock/unlock cmd failed" flag in R2 response 00779 status = KO; 00780 00781 // set original block length 00782 r1 = mmc_sd_send_command(MMC_SET_BLOCKLEN, 512); 00783 Spi_write_data(0xFF); // write dummy byte 00784 if (r1 != 0x00) 00785 status = KO; 00786 00787 return status; 00788 }
| bit mmc_sd_read_open | ( | U32 | pos | ) |
Functions for preparing block read/write.
This function opens a MMC_SD memory in read mode at a given sector address (not byte address)
| pos | Sector address |
Definition at line 802 of file mmc_sd.c.
References gl_ptr_mem, and mmc_sd_wait_not_busy().
00803 { 00804 // Set the global memory ptr at a Byte address. 00805 gl_ptr_mem = pos << 9; // gl_ptr_mem = pos * 512 00806 00807 // wait for MMC not busy 00808 return mmc_sd_wait_not_busy(); 00809 }
| void mmc_sd_read_close | ( | void | ) |
| bit mmc_sd_write_open | ( | U32 | pos | ) |
This function opens a MMC_SD memory in write mode at a given sector address.
NOTE: If page buffer > 512 bytes, page content is first loaded in buffer to be partially updated by write_byte or write64 functions.
| pos | Sector address |
Definition at line 841 of file mmc_sd.c.
References gl_ptr_mem, and mmc_sd_wait_not_busy().
00842 { 00843 // Set the global memory ptr at a Byte address. 00844 gl_ptr_mem = pos << 9; // gl_ptr_mem = pos * 512 00845 00846 // wait for MMC not busy 00847 return mmc_sd_wait_not_busy(); 00848 }
| void mmc_sd_write_close | ( | void | ) |
| bit mmc_sd_write_sector | ( | U16 | nb_sector | ) |
Funtions to link USB DEVICE flow with MMC.
This function is optimized and writes nb-sector * 512 Bytes from USB controller to DataFlash memory DATA FLOW is: USB => MMC_SD NOTE:
| nb_sector | number of contiguous sectors to write [IN] | |
| gl_ptr_mem | memory ptr on MMC_SD [global][IN/OUT] |
Definition at line 1059 of file mmc_sd.c.
References gl_ptr_mem, i, Is_usb_endpoint_enabled, Is_usb_read_enabled, KO, MMC_DR_ACCEPT, MMC_DR_MASK, mmc_sd_command(), Mmc_sd_select, Mmc_sd_unselect, mmc_sd_wait_not_busy(), MMC_STARTBLOCK_WRITE, MMC_WRITE_BLOCK, OK, r1, Spi_ack_write, Spi_read_data, Spi_write_data, Usb_ack_receive_out, and Usb_read_byte.
01060 { 01061 U8 i; 01062 01063 do 01064 { 01065 // wait card not busy 01066 i=0; 01067 while (KO == mmc_sd_wait_not_busy()) 01068 { 01069 i++; 01070 if (i == 10) 01071 return KO; 01072 } 01073 01074 Mmc_sd_select(); // select MMC_SD 01075 // issue command 01076 r1 = mmc_sd_command(MMC_WRITE_BLOCK, gl_ptr_mem); 01077 // check for valid response 01078 if(r1 != 0x00) 01079 { 01080 Mmc_sd_unselect(); // unselect MMC_SD 01081 return KO; 01082 } 01083 // send dummy 01084 Spi_write_data(0xFF); // give clock again to end transaction 01085 // send data start token 01086 Spi_write_data(MMC_STARTBLOCK_WRITE); 01087 // write data 01088 //# 01089 //# Write 8x64b = 512b from the USB FIFO OUT. 01090 //# 01091 for (i = 8; i != 0; i--) 01092 { 01093 // Wait end of rx in USB EPOUT. 01094 while(!Is_usb_read_enabled()) 01095 { 01096 if(!Is_usb_endpoint_enabled()) 01097 return KO; // USB Reset 01098 } 01099 01100 Disable_interrupt(); // Global disable. 01101 01102 // SPI write principle: send a Byte then clear the SPIF flag. 01103 // Spi_write_data(Usb_read_byte()): (.) Final step to clear the SPIF bit, 01104 // (.) send a Byte read from USB, 01105 // (.) 1st step to clear the SPIF bit. 01106 Spi_write_data(Usb_read_byte()); 01107 Spi_write_data(Usb_read_byte()); 01108 Spi_write_data(Usb_read_byte()); 01109 Spi_write_data(Usb_read_byte()); 01110 Spi_write_data(Usb_read_byte()); 01111 Spi_write_data(Usb_read_byte()); 01112 Spi_write_data(Usb_read_byte()); 01113 Spi_write_data(Usb_read_byte()); 01114 Spi_write_data(Usb_read_byte()); 01115 Spi_write_data(Usb_read_byte()); 01116 Spi_write_data(Usb_read_byte()); 01117 Spi_write_data(Usb_read_byte()); 01118 Spi_write_data(Usb_read_byte()); 01119 Spi_write_data(Usb_read_byte()); 01120 Spi_write_data(Usb_read_byte()); 01121 Spi_write_data(Usb_read_byte()); 01122 Spi_write_data(Usb_read_byte()); 01123 Spi_write_data(Usb_read_byte()); 01124 Spi_write_data(Usb_read_byte()); 01125 Spi_write_data(Usb_read_byte()); 01126 Spi_write_data(Usb_read_byte()); 01127 Spi_write_data(Usb_read_byte()); 01128 Spi_write_data(Usb_read_byte()); 01129 Spi_write_data(Usb_read_byte()); 01130 Spi_write_data(Usb_read_byte()); 01131 Spi_write_data(Usb_read_byte()); 01132 Spi_write_data(Usb_read_byte()); 01133 Spi_write_data(Usb_read_byte()); 01134 Spi_write_data(Usb_read_byte()); 01135 Spi_write_data(Usb_read_byte()); 01136 Spi_write_data(Usb_read_byte()); 01137 Spi_write_data(Usb_read_byte()); 01138 Spi_write_data(Usb_read_byte()); 01139 Spi_write_data(Usb_read_byte()); 01140 Spi_write_data(Usb_read_byte()); 01141 Spi_write_data(Usb_read_byte()); 01142 Spi_write_data(Usb_read_byte()); 01143 Spi_write_data(Usb_read_byte()); 01144 Spi_write_data(Usb_read_byte()); 01145 Spi_write_data(Usb_read_byte()); 01146 Spi_write_data(Usb_read_byte()); 01147 Spi_write_data(Usb_read_byte()); 01148 Spi_write_data(Usb_read_byte()); 01149 Spi_write_data(Usb_read_byte()); 01150 Spi_write_data(Usb_read_byte()); 01151 Spi_write_data(Usb_read_byte()); 01152 Spi_write_data(Usb_read_byte()); 01153 Spi_write_data(Usb_read_byte()); 01154 Spi_write_data(Usb_read_byte()); 01155 Spi_write_data(Usb_read_byte()); 01156 Spi_write_data(Usb_read_byte()); 01157 Spi_write_data(Usb_read_byte()); 01158 Spi_write_data(Usb_read_byte()); 01159 Spi_write_data(Usb_read_byte()); 01160 Spi_write_data(Usb_read_byte()); 01161 Spi_write_data(Usb_read_byte()); 01162 Spi_write_data(Usb_read_byte()); 01163 Spi_write_data(Usb_read_byte()); 01164 Spi_write_data(Usb_read_byte()); 01165 Spi_write_data(Usb_read_byte()); 01166 Spi_write_data(Usb_read_byte()); 01167 Spi_write_data(Usb_read_byte()); 01168 Spi_write_data(Usb_read_byte()); 01169 Spi_write_data(Usb_read_byte()); 01170 Spi_ack_write(); // Final step to clear the SPIF bit. 01171 01172 Usb_ack_receive_out(); // USB EPOUT read acknowledgement. 01173 01174 Enable_interrupt(); // Global re-enable. 01175 } // for (i = 8; i != 0; i--) 01176 01177 Spi_write_data(0xFF); // send dummy CRC 01178 Spi_write_data(0xFF); 01179 01180 // read data response token 01181 Spi_write_data(0xFF); 01182 r1 = Spi_read_data(); 01183 if( (r1&MMC_DR_MASK) != MMC_DR_ACCEPT) 01184 { 01185 Mmc_sd_unselect(); // unselect MMC_SD 01186 return r1; 01187 } 01188 01189 // send dummy byte 01190 Spi_write_data(0xFF); 01191 01192 // release chip select 01193 Mmc_sd_unselect(); // unselect MMC_SD 01194 gl_ptr_mem += 512; // Update the memory pointer. 01195 nb_sector--; // 1 more sector written 01196 } 01197 while (nb_sector != 0); 01198 01199 // wait card not busy after last programming operation 01200 i=0; 01201 while (KO == mmc_sd_wait_not_busy()) 01202 { 01203 i++; 01204 if (i == 10) 01205 return KO; 01206 } 01207 01208 return OK; // Write done 01209 }
| bit mmc_sd_read_sector | ( | U16 | nb_sector | ) |
This function is optimized and writes nb-sector * 512 Bytes from DataFlash memory to USB controller DATA FLOW is: MMC_SD => USB NOTE:
| nb_sector | number of contiguous sectors to read [IN] | |
| gl_ptr_mem | memory ptr on MMC_SD [global][IN/OUT] |
Definition at line 894 of file mmc_sd.c.
References FALSE, gl_ptr_mem, i, Is_usb_endpoint_enabled, Is_usb_write_enabled, KO, MMC_READ_SINGLE_BLOCK, mmc_sd_command(), Mmc_sd_select, mmc_sd_send_and_read(), Mmc_sd_unselect, MMC_STARTBLOCK_READ, OK, r1, Spi_read_data, Spi_write_data, Usb_send_in, and Usb_write_byte.
00895 { 00896 Byte i; 00897 U16 read_time_out; 00898 00899 do 00900 { 00901 Mmc_sd_select(); // select MMC_SD 00902 // issue command 00903 r1 = mmc_sd_command(MMC_READ_SINGLE_BLOCK, gl_ptr_mem); 00904 // check for valid response 00905 if(r1 != 0x00) 00906 { 00907 Mmc_sd_unselect(); // unselect MMC_SD 00908 return KO; 00909 } 00910 00911 // wait for token (may be a datablock start token OR a data error token !) 00912 read_time_out = 30000; 00913 while((r1 = mmc_sd_send_and_read(0xFF)) == 0xFF) 00914 { 00915 read_time_out--; 00916 if (read_time_out == 0) // TIME-OUT 00917 { 00918 Mmc_sd_unselect(); // unselect MMC_SD 00919 return KO; 00920 } 00921 } 00922 00923 // check token 00924 if (r1 != MMC_STARTBLOCK_READ) 00925 { 00926 Spi_write_data(0xFF); 00927 Mmc_sd_unselect(); // unselect MMC_SD 00928 return KO; 00929 } 00930 00931 //# 00932 //# Read 8x64b = 512b, put them in the USB FIFO IN. 00933 //# 00934 for (i = 8; i != 0; i--) 00935 { 00936 Disable_interrupt(); // Global disable. 00937 00938 // Principle: send any Byte to get a Byte. 00939 // Spi_write_data(0): send any Byte + 1st step to clear the SPIF bit. 00940 // Spi_read_data(): get the Byte + final step to clear the SPIF bit. 00941 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00942 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00943 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00944 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00945 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00946 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00947 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00948 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00949 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00950 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00951 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00952 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00953 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00954 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00955 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00956 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00957 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00958 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00959 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00960 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00961 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00962 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00963 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00964 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00965 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00966 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00967 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00968 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00969 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00970 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00971 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00972 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00973 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00974 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00975 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00976 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00977 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00978 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00979 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00980 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00981 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00982 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00983 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00984 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00985 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00986 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00987 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00988 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00989 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00990 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00991 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00992 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00993 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00994 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00995 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00996 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00997 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00998 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 00999 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 01000 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 01001 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 01002 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 01003 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 01004 Spi_write_data(0xFF); Usb_write_byte(Spi_read_data()); 01005 Enable_interrupt(); // Global re-enable. 01006 01007 //# 01008 //# Send the USB FIFO IN content to the USB Host. 01009 //# 01010 Usb_send_in(); // Send the FIFO IN content to the USB Host. 01011 // Wait until the tx is done so that we may write to the FIFO IN again. 01012 while(Is_usb_write_enabled()==FALSE) 01013 { 01014 if(!Is_usb_endpoint_enabled()) 01015 return KO; // USB Reset 01016 } 01017 } // for (i = 8; i != 0; i--) 01018 01019 gl_ptr_mem += 512; // Update the memory pointer. 01020 nb_sector--; // 1 more sector read 01021 // read 16-bit CRC 01022 Spi_write_data(0xFF); 01023 Spi_write_data(0xFF); 01024 // dummy bytes 01025 Spi_write_data(0xFF); 01026 Spi_write_data(0xFF); 01027 // release chip select 01028 Mmc_sd_unselect(); // unselect MMC_SD 01029 } 01030 while (nb_sector != 0); 01031 01032 return OK; // Read done. 01033 }
| bit mmc_sd_read_sector_to_ram | ( | U8 * | ram | ) |
Functions to read/write one sector (512btes) with ram buffer pointer.
This function read one MMC sector and load it into a ram buffer DATA FLOW is: MMC/SD => RAM NOTE:
| *ram | pointer to ram buffer |
Definition at line 1363 of file mmc_sd.c.
References gl_ptr_mem, i, KO, MMC_READ_SINGLE_BLOCK, mmc_sd_command(), Mmc_sd_select, mmc_sd_send_and_read(), Mmc_sd_unselect, mmc_sd_wait_not_busy(), MMC_SECTOR_SIZE, MMC_STARTBLOCK_READ, OK, r1, Spi_read_data, and Spi_write_data.
01364 { 01365 U16 i; 01366 U16 read_time_out; 01367 01368 // wait for MMC not busy 01369 if (KO == mmc_sd_wait_not_busy()) 01370 return KO; 01371 01372 Mmc_sd_select(); // select MMC_SD 01373 // issue command 01374 r1 = mmc_sd_command(MMC_READ_SINGLE_BLOCK, gl_ptr_mem); 01375 01376 // check for valid response 01377 if (r1 != 0x00) 01378 { 01379 Mmc_sd_unselect(); // unselect MMC_SD 01380 return KO; 01381 } 01382 01383 // wait for token (may be a datablock start token OR a data error token !) 01384 read_time_out = 30000; 01385 while((r1 = mmc_sd_send_and_read(0xFF)) == 0xFF) 01386 { 01387 read_time_out--; 01388 if (read_time_out == 0) // TIME-OUT 01389 { 01390 Mmc_sd_unselect(); // unselect MMC_SD 01391 return KO; 01392 } 01393 } 01394 01395 // check token 01396 if (r1 != MMC_STARTBLOCK_READ) 01397 { 01398 Spi_write_data(0xFF); 01399 Mmc_sd_unselect(); // unselect MMC_SD 01400 return KO; 01401 } 01402 01403 // store datablock 01404 Disable_interrupt(); // Global disable. 01405 for(i=0;i<MMC_SECTOR_SIZE;i++) 01406 { 01407 Spi_write_data(0xFF); 01408 *ram=Spi_read_data(); 01409 ram++; 01410 } 01411 Enable_interrupt(); // Global re-enable. 01412 gl_ptr_mem += 512; // Update the memory pointer. 01413 01414 // load 16-bit CRC (ignored) 01415 Spi_write_data(0xFF); 01416 Spi_write_data(0xFF); 01417 01418 // continue delivering some clock cycles 01419 Spi_write_data(0xFF); 01420 Spi_write_data(0xFF); 01421 01422 // release chip select 01423 Mmc_sd_unselect(); // unselect MMC_SD 01424 01425 return OK; // Read done. 01426 }
| bit mmc_sd_write_sector_from_ram | ( | U8 * | ram | ) |
This function write one MMC sector from a ram buffer DATA FLOW is: RAM => MMC/SD NOTE (please read) :
| *ram | pointer to ram buffer |
Definition at line 1446 of file mmc_sd.c.
References gl_ptr_mem, i, KO, MMC_DR_ACCEPT, MMC_DR_MASK, mmc_sd_command(), Mmc_sd_select, mmc_sd_send_and_read(), Mmc_sd_unselect, mmc_sd_wait_not_busy(), MMC_SECTOR_SIZE, MMC_STARTBLOCK_WRITE, MMC_WRITE_BLOCK, OK, r1, and Spi_write_data.
01447 { 01448 U16 i; 01449 01450 // wait for MMC not busy 01451 if (KO == mmc_sd_wait_not_busy()) 01452 return KO; 01453 01454 Mmc_sd_select(); // select MMC_SD 01455 // issue command 01456 r1 = mmc_sd_command(MMC_WRITE_BLOCK, gl_ptr_mem); 01457 // check for valid response 01458 if(r1 != 0x00) 01459 { 01460 Mmc_sd_unselect(); 01461 return KO; 01462 } 01463 // send dummy 01464 Spi_write_data(0xFF); // give clock again to end transaction 01465 01466 // send data start token 01467 Spi_write_data(MMC_STARTBLOCK_WRITE); 01468 // write data 01469 for(i=0;i<MMC_SECTOR_SIZE;i++) 01470 { 01471 Spi_write_data(*ram); 01472 ram++; 01473 } 01474 01475 Spi_write_data(0xFF); // send CRC (field required but value ignored) 01476 Spi_write_data(0xFF); 01477 01478 // read data response token 01479 r1 = mmc_sd_send_and_read(0xFF); 01480 if( (r1&MMC_DR_MASK) != MMC_DR_ACCEPT) 01481 { 01482 Spi_write_data(0xFF); // send dummy bytes 01483 Spi_write_data(0xFF); 01484 Mmc_sd_unselect(); 01485 return KO; 01486 // return r1; // return ERROR byte 01487 } 01488 01489 Spi_write_data(0xFF); // send dummy bytes 01490 Spi_write_data(0xFF); 01491 01492 // release chip select 01493 Mmc_sd_unselect(); // unselect MMC_SD 01494 gl_ptr_mem += 512; // Update the memory pointer. 01495 01496 // wait card not busy after last programming operation 01497 i=0; 01498 while (KO == mmc_sd_wait_not_busy()) 01499 { 01500 i++; 01501 if (i == 10) 01502 return KO; 01503 } 01504 01505 return OK; // Write done 01506 }
This function erase a group of sectors NOTE : Erasing operation concerns only groups of sectors and not one sector only The global variable "erase_group_size" (extracted from CSD) contains the sector group size boundary User specifies the addresses of the first group and the last group to erase (several contiguous groups can be selected for erase) An misaligned address will not generate an error since the memory card ignore the LSbs of the address Some examples (with "erase_group_size" = 0x20 = group boundary) :
| U32 | adr_start address of 1st group (sector address, not byte address) U32 adr_end address of last group (sector address, not byte address) |
Definition at line 1298 of file mmc_sd.c.
References card_type, KO, MMC_CARD, MMC_ERASE, mmc_sd_command(), Mmc_sd_select, Mmc_sd_unselect, mmc_sd_wait_not_busy(), MMC_TAG_ERASE_GROUP_END, MMC_TAG_ERASE_GROUP_START, OK, r1, SD_TAG_WR_ERASE_GROUP_END, SD_TAG_WR_ERASE_GROUP_START, and Spi_write_data.
01299 { 01300 U8 cmd; 01301 01302 // wait for MMC not busy 01303 if (KO == mmc_sd_wait_not_busy()) 01304 return KO; 01305 01306 Mmc_sd_select(); // select MMC_SD 01307 01308 // send address of 1st group 01309 if (card_type == MMC_CARD) 01310 { cmd = MMC_TAG_ERASE_GROUP_START; } 01311 else 01312 { cmd = SD_TAG_WR_ERASE_GROUP_START; } 01313 if ((r1 = mmc_sd_command(cmd,(adr_start << 9))) != 0) 01314 { 01315 Mmc_sd_unselect(); 01316 return KO; 01317 } 01318 Spi_write_data(0xFF); 01319 01320 // send address of last group 01321 if (card_type == MMC_CARD) 01322 { cmd = MMC_TAG_ERASE_GROUP_END; } 01323 else 01324 { cmd = SD_TAG_WR_ERASE_GROUP_END; } 01325 if ((r1 = mmc_sd_command(cmd,(adr_end << 9))) != 0) 01326 { 01327 Mmc_sd_unselect(); 01328 return KO; 01329 } 01330 Spi_write_data(0xFF); 01331 01332 // send erase command 01333 if ((r1 = mmc_sd_command(MMC_ERASE,0)) != 0) 01334 { 01335 Mmc_sd_unselect(); 01336 return KO; 01337 } 01338 Spi_write_data(0xFF); 01339 01340 Mmc_sd_unselect(); 01341 01342 return OK; 01343 }
| volatile U32 mmc_sd_last_block_address |
| bit mmc_sd_init_done |
1.5.3