#include "conf/conf_access.h"#include "modules/control_access/ctrl_status.h"#include "conf/conf_usb.h"
Go to the source code of this file.
Functions | |
| void | host_mem_init (void) |
| This fonction must be call only once at the program startup to initialize the USB driver MS. | |
| Bool | host_mem_install (void) |
| This fonction must be call when a device is connected. | |
| void | host_mem_uninstall (void) |
| This fonction must be call when a device is disconnected. | |
| U8 | host_mem_get_lun (void) |
| This fonction returns the number of LUN of the devices mass storage connected to the host. | |
| Ctrl_status | host_mem_test_unit_ready (U8 lun) |
| This fonction test the state of memory, and start the initialisation of the memory. | |
| Ctrl_status | host_mem_read_capacity (U8 lun, U32 _MEM_TYPE_SLOW_ *u32_nb_sector) |
| This fonction returns the address of the last valid sector. | |
| U8 | host_mem_read_sector_size (U8 lun) |
| Bool | host_mem_wr_protect_cache (U8 lun) |
| Bool | host_mem_wr_protect (U8 lun) |
| Bool | host_mem_removal (void) |
| This fonction inform about the memory type. | |
| Ctrl_status | host_mem_read_format_capacity (U8 lun) |
| Ctrl_status | host_mem_inquiry (U8 lun) |
| Ctrl_status | host_mem_mem_2_ram (U8 lun, U32 addr, U8 *ram) |
| Ctrl_status | host_mem_mem_2_ram_stop (void) |
| This function terminates the tranfer of a physical sector from memory. | |
| Ctrl_status | host_mem_ram_2_mem (U8 lun, U32 addr, U8 *ram) |
| Ctrl_status | host_mem_mem_2_ram_ext (U8 lun, U32 addr, U8 *ram, U8 u8_nb_sector) |
| Ctrl_status | host_mem_ram_2_mem_ext (U8 lun, U32 addr, U8 *ram, U8 u8_nb_sector) |
This file contains the C51 RAM called CRAM management routines which are used for Mass storage when doing ISP This file calls routines of the cram_mem.c file
Definition in file host_mem.h.
| void host_mem_init | ( | void | ) |
This fonction must be call only once at the program startup to initialize the USB driver MS.
Definition at line 173 of file host_mem.c.
References S_dms_device::device_index, g_ms_nb_connected, i, and USB_MAX_DMS_NUMBER.
00174 { 00175 U8 i; 00176 // Reset Device MS struct 00177 for(i=0; i<USB_MAX_DMS_NUMBER; i++) 00178 { 00179 g_ms_devices[i].device_index=0xFF; 00180 } 00181 g_ms_nb_connected=0; 00182 }
| Bool host_mem_install | ( | void | ) |
This fonction must be call when a device is connected.
Definition at line 187 of file host_mem.c.
References S_lun_info::b_first_unitready, S_lun_info::b_protected, capacity, CONTROL_GOOD, data_stage, S_usb_tree::device, S_dms_device::device_index, S_usb_interface::ep, FALSE, g_ms_nb_connected, g_ms_sel_dms, Get_class, Get_ep_addr, Get_nb_device, Get_nb_supported_interface, host_mem_inquiry(), host_mem_read_capacity(), host_ms_get_max_lun, Host_select_device, i, S_usb_device::interface, Is_ep_addr_in, LOG_STR_CODE, S_dms_device::lun_info, MS_CLASS, S_dms_device::nb_lun, S_dms_device::pipe_in, S_usb_endpoint::pipe_number, S_dms_device::pipe_out, TRUE, USB_MAX_DMS_NUMBER, USB_MAX_LUN_PER_DMS, and usb_tree.
00188 { 00189 U32 capacity; 00190 U8 device_num; 00191 U8 interface_num; 00192 U8 lun_offset; 00193 U8 i; 00194 00195 // Check all devices connected 00196 for( device_num=0; device_num<Get_nb_device(); device_num++) 00197 { 00198 Host_select_device(device_num); 00199 00200 // Check all interfaces of device 00201 for( interface_num=0; interface_num < Get_nb_supported_interface(); interface_num++ ) 00202 { 00203 if( Get_class(interface_num)!= MS_CLASS ) 00204 continue; // It is not a MS interface 00205 00206 LOG_STR_CODE(log_ms_connect); 00207 00208 // If it is not the first MS device 00209 if( g_ms_nb_connected != 0 ) 00210 { 00211 // Check if already installed 00212 for( i=0; i<g_ms_nb_connected; i++ ) 00213 { 00214 if( g_ms_devices[i].device_index == device_num ) 00215 break; 00216 } 00217 if( i!=g_ms_nb_connected ) 00218 break; // Device already installed 00219 // Check struct space free 00220 if( USB_MAX_DMS_NUMBER == g_ms_nb_connected ) 00221 break; // Too many MS device connected 00222 } 00223 00224 //** Start install 00225 g_ms_devices[g_ms_nb_connected].device_index = device_num; 00226 00227 // Get correct physical pipes associated to IN/OUT Mass Storage Endpoints 00228 if(Is_ep_addr_in(Get_ep_addr(interface_num,0))) 00229 { //Yes associate it to the MassStorage IN pipe 00230 g_ms_devices[g_ms_nb_connected].pipe_in=usb_tree.device[device_num].interface[interface_num].ep[0].pipe_number; 00231 g_ms_devices[g_ms_nb_connected].pipe_out=usb_tree.device[device_num].interface[interface_num].ep[1].pipe_number; 00232 } 00233 else 00234 { //No, invert... 00235 g_ms_devices[g_ms_nb_connected].pipe_in=usb_tree.device[device_num].interface[interface_num].ep[1].pipe_number; 00236 g_ms_devices[g_ms_nb_connected].pipe_out=usb_tree.device[device_num].interface[interface_num].ep[0].pipe_number; 00237 } 00238 00239 // Get last LUN number on the device mass storage connected 00240 if( CONTROL_GOOD != host_ms_get_max_lun() ) 00241 data_stage[0] = 0; // If STALL request then last LUN number = 0 00242 g_ms_devices[g_ms_nb_connected].nb_lun = data_stage[0]+1; // Save number of LUN = last LUN number + 1 00243 00244 if( USB_MAX_LUN_PER_DMS < g_ms_devices[g_ms_nb_connected].nb_lun ) 00245 g_ms_devices[g_ms_nb_connected].nb_lun = USB_MAX_LUN_PER_DMS; // Limitation on the number of LUN 00246 00247 // Compute LUN offset of this new device 00248 lun_offset = 0; 00249 for( i=0; i<g_ms_nb_connected; i++) 00250 { 00251 lun_offset +=g_ms_devices[i].nb_lun; 00252 } 00253 00254 // Add the new MS device in MS strut 00255 g_ms_sel_dms = g_ms_nb_connected; 00256 g_ms_nb_connected++; 00257 00258 // Initialize all LUN from the new MS device 00259 for( i=0; i<g_ms_devices[g_ms_sel_dms].nb_lun; i++ ) 00260 { 00261 // Init struct of LUN 00262 g_ms_devices[g_ms_sel_dms].lun_info[i].b_first_unitready = FALSE; 00263 g_ms_devices[g_ms_sel_dms].lun_info[i].b_protected = TRUE; 00264 // Init MS corresponding at LUN 00265 host_mem_inquiry( lun_offset+i ); 00266 host_mem_read_capacity( lun_offset+i, &capacity ); 00267 } 00268 return TRUE; // Install interface/device done 00269 } 00270 } 00271 return FALSE; // No MSC install 00272 }
| void host_mem_uninstall | ( | void | ) |
This fonction must be call when a device is disconnected.
Definition at line 277 of file host_mem.c.
References S_usb_tree::device, S_usb_device::device_address, S_dms_device::device_index, FALSE, g_ms_nb_connected, i, TRUE, and usb_tree.
00278 { 00279 U8 device_num; 00280 U8 i; 00281 Bool b_last_ms_conected = TRUE; 00282 00283 for( i=g_ms_nb_connected; i!=0; i--) 00284 { 00285 device_num = g_ms_devices[i-1].device_index; 00286 if( 0xFF == device_num ) 00287 { 00288 // Device already remove but struct no updated 00289 // it may be possible in case of many MS on USB HUB 00290 g_ms_nb_connected--; 00291 continue; 00292 } 00293 if( 0 == usb_tree.device[device_num].device_address ) 00294 { 00295 g_ms_devices[i-1].device_index = 0xFF; 00296 if( b_last_ms_conected ) 00297 g_ms_nb_connected--; 00298 }else{ 00299 b_last_ms_conected = FALSE; 00300 } 00301 } 00302 }
| U8 host_mem_get_lun | ( | void | ) |
This fonction returns the number of LUN of the devices mass storage connected to the host.
Definition at line 309 of file host_mem.c.
References g_ms_nb_connected, i, Is_host_ms_configured, and S_dms_device::nb_lun.
00310 { 00311 U8 i; 00312 U8 host_ms_max_lun = 0; 00313 00314 if(!Is_host_ms_configured()) 00315 return 0; 00316 00317 for( i=0; i<g_ms_nb_connected; i++ ) 00318 { 00319 host_ms_max_lun += g_ms_devices[i].nb_lun; 00320 } 00321 return host_ms_max_lun; 00322 }
| Ctrl_status host_mem_test_unit_ready | ( | U8 | lun | ) |
This fonction test the state of memory, and start the initialisation of the memory.
Definition at line 337 of file host_mem.c.
References S_lun_info::b_first_unitready, S_lun_info::b_protected, S_cbw::cmd, CTRL_BUSY, CTRL_FAIL, CTRL_GOOD, CTRL_NO_PRESENT, S_cbw::dir, FALSE, g_ms_sel_dms, g_ms_sel_lun, g_readctx_b_run, host_mem_cbw_init(), host_mem_cbw_send(), host_mem_csw_read(), host_mem_mem_2_ram_stop(), host_mem_read_capacity(), host_mem_select_lun(), host_mem_wr_protect(), S_cbw::lgt, S_dms_device::lun_info, SBC_CMD_DIR_OUT, SBC_CMD_TEST_UNIT_READY, and TRUE.
00338 { 00339 Ctrl_status status; 00340 U32 u32_nb_sector; 00341 00342 if( !host_mem_select_lun(lun) ) 00343 return CTRL_NO_PRESENT; 00344 if (g_readctx_b_run) 00345 { 00346 host_mem_mem_2_ram_stop(); 00347 host_mem_select_lun(lun); 00348 } 00349 00350 // Send CBW 00351 host_mem_cbw_init(); 00352 // g_ms_cbw.lgt_lsb0 = 0; 00353 g_ms_cbw.dir = SBC_CMD_DIR_OUT; 00354 g_ms_cbw.lgt = 0x06; 00355 g_ms_cbw.cmd = SBC_CMD_TEST_UNIT_READY; 00356 if( !host_mem_cbw_send() ) 00357 return CTRL_FAIL; 00358 00359 // Read CSW status 00360 status = host_mem_csw_read(); 00361 if( status == CTRL_GOOD ) 00362 { 00363 if( FALSE == g_ms_devices[g_ms_sel_dms].lun_info[g_ms_sel_lun].b_first_unitready ) 00364 { 00365 // Signal the new diskl 00366 status = CTRL_BUSY; 00367 // U-Disk valid then update info LUN 00368 if( CTRL_GOOD == host_mem_read_capacity( lun , &u32_nb_sector ) ) 00369 { 00370 g_ms_devices[g_ms_sel_dms].lun_info[g_ms_sel_lun].b_protected = host_mem_wr_protect( lun ); 00371 g_ms_devices[g_ms_sel_dms].lun_info[g_ms_sel_lun].b_first_unitready = TRUE; 00372 } 00373 } 00374 } 00375 else 00376 { 00377 g_ms_devices[g_ms_sel_dms].lun_info[g_ms_sel_lun].b_first_unitready = FALSE; 00378 } 00379 return status; 00380 }
| Ctrl_status host_mem_read_capacity | ( | U8 | lun, | |
| U32 _MEM_TYPE_SLOW_ * | u32_nb_sector | |||
| ) |
This fonction returns the address of the last valid sector.
Ctrl_status It is ready -> CTRL_GOOD Memory unplug -> CTRL_NO_PRESENT Not initialize or change -> CTRL_BUSY A error occur -> CTRL_FAIL
Definition at line 392 of file host_mem.c.
References S_cbw::cmd, CTRL_FAIL, CTRL_NO_PRESENT, S_cbw::dir, DMS_pipe_in, g_ms_sel_dms, g_ms_sel_lun, g_readctx_b_run, host_get_data(), host_mem_cbw_init(), host_mem_cbw_send(), host_mem_csw_read(), host_mem_mem_2_ram_stop(), host_mem_select_lun(), host_mem_stall_management(), S_cbw::lgt, S_cbw::lgt_lsb0, S_dms_device::lun_info, MSB0, MSB1, MSB2, MSB3, PIPE_GOOD, PIPE_STALL, SBC_CMD_DIR_IN, SBC_CMD_READ_CAPACITY, and S_lun_info::u8_block_size.
00393 { 00394 U16 nb; 00395 U8 datas[8], status; 00396 00397 if( !host_mem_select_lun(lun) ) 00398 return CTRL_NO_PRESENT; 00399 if (g_readctx_b_run) 00400 { 00401 host_mem_mem_2_ram_stop(); 00402 host_mem_select_lun(lun); 00403 } 00404 00405 // Send CBW 00406 host_mem_cbw_init(); 00407 g_ms_cbw.lgt_lsb0 = 0x08; 00408 g_ms_cbw.dir = SBC_CMD_DIR_IN; 00409 g_ms_cbw.lgt = 0x0A; 00410 g_ms_cbw.cmd = SBC_CMD_READ_CAPACITY; 00411 if( !host_mem_cbw_send() ) 00412 return CTRL_FAIL; 00413 00414 // Receiv the capacity data 00415 nb=8; 00416 status = host_get_data(DMS_pipe_in(),&nb,datas); 00417 if( PIPE_GOOD != status ) 00418 { 00419 if( PIPE_STALL == status ) 00420 host_mem_stall_management(); 00421 host_mem_csw_read(); 00422 return CTRL_FAIL; 00423 } 00424 00425 // Get last sector address 00426 MSB0(*u32_nb_sector) = datas[0]; 00427 MSB1(*u32_nb_sector) = datas[1]; 00428 MSB2(*u32_nb_sector) = datas[2]; 00429 MSB3(*u32_nb_sector) = datas[3]; 00430 // Get block size (unit 512B) 00431 g_ms_devices[ g_ms_sel_dms ].lun_info[ g_ms_sel_lun ].u8_block_size = datas[6]/2; // Block size MSB 00432 00433 // Read CSW status 00434 return host_mem_csw_read(); 00435 }
Returns the physical sector of the memory
| lun,global | lun selected (global!=lun of specific USB device) |
Definition at line 444 of file host_mem.c.
References g_ms_sel_dms, g_ms_sel_lun, host_mem_select_lun(), host_mem_test_unit_ready(), S_dms_device::lun_info, and S_lun_info::u8_block_size.
00445 { 00446 host_mem_test_unit_ready( lun ); 00447 if( !host_mem_select_lun(lun) ) 00448 return 1; 00449 return g_ms_devices[g_ms_sel_dms].lun_info[g_ms_sel_lun].u8_block_size; 00450 }
Return the write protected mode (cache used) This information is in a cache to speed up command
| lun,global | lun selected (global!=lun of specific USB device) |
Definition at line 460 of file host_mem.c.
References S_lun_info::b_protected, g_ms_sel_dms, g_ms_sel_lun, host_mem_select_lun(), S_dms_device::lun_info, and TRUE.
00461 { 00462 if( !host_mem_select_lun(lun) ) 00463 return TRUE; // no present 00464 00465 return g_ms_devices[g_ms_sel_dms].lun_info[g_ms_sel_lun].b_protected; 00466 }
Return the write protected mode (no cache)
| lun,global | lun selected (global!=lun of specific USB device) |
Definition at line 475 of file host_mem.c.
References S_cbw::cmd, S_cbw::dir, DMS_pipe_in, g_ms_sel_dms, g_ms_sel_lun, g_readctx_b_run, host_get_data(), host_mem_cbw_init(), host_mem_cbw_send(), host_mem_csw_read(), host_mem_mem_2_ram_stop(), host_mem_select_lun(), host_mem_stall_management(), S_cbw::lgt, S_cbw::lgt_lsb0, PIPE_GOOD, PIPE_STALL, SBC_CMD_DIR_IN, SBC_CMD_MODE_SENSE_6, TRUE, S_cbw::u8_data, and USB_SUPPORT_MS_SECTOR_WR_MAX.
00476 { 00477 U16 nb; 00478 U8 write_code[0x0C], status; 00479 00480 if( !host_mem_select_lun(lun) ) 00481 return TRUE; 00482 00483 if( USB_SUPPORT_MS_SECTOR_WR_MAX < g_ms_devices[ g_ms_sel_dms ].lun_info[ g_ms_sel_lun ].u8_block_size ) 00484 return TRUE; // No supported this lun in write mode, because sector size != 512B 00485 00486 if (g_readctx_b_run) 00487 { 00488 host_mem_mem_2_ram_stop(); 00489 host_mem_select_lun(lun); 00490 } 00491 00492 // Send CBW 00493 host_mem_cbw_init(); 00494 g_ms_cbw.dir = SBC_CMD_DIR_IN; 00495 g_ms_cbw.lgt = 0x06; 00496 g_ms_cbw.cmd = SBC_CMD_MODE_SENSE_6; 00497 g_ms_cbw.lgt_lsb0 = 0x0C; 00498 //g_ms_cbw.u8_data[16-16] = 0x00; // 16 - CBWCB1 - Option 00499 g_ms_cbw.u8_data[17-16] = 0x3F; // 17 - CBWCB2 - Page Code 3F = return all mode pages 00500 //g_ms_cbw.u8_data[18-16] = 0x00; // 18 - CBWCB3 - reserved 00501 g_ms_cbw.u8_data[19-16] = 0x0C; // 19 - CBWCB4 - Allocation Length 00502 //g_ms_cbw.u8_data[20-16] = 0x00; // 20 - CBWCB5 - Control 00503 if( !host_mem_cbw_send() ) 00504 return TRUE; 00505 00506 // Receiv 00507 nb=0x0C; 00508 status = host_get_data(DMS_pipe_in(),&nb,write_code); 00509 if( PIPE_GOOD != status ) 00510 { 00511 if( PIPE_STALL == status ) 00512 host_mem_stall_management(); 00513 write_code[2] = 0x00; // error then no write protected by defaut 00514 } 00515 00516 // Read CSW status 00517 host_mem_csw_read(); // ignore error on CSW (in case of specific Udisk) 00518 00519 return (write_code[2] == 0x80); 00520 }
| Bool host_mem_removal | ( | void | ) |
This fonction inform about the memory type.
Definition at line 527 of file host_mem.c.
References TRUE.
00528 { 00529 return TRUE; 00530 }
| Ctrl_status host_mem_read_format_capacity | ( | U8 | lun | ) |
| Ctrl_status host_mem_inquiry | ( | U8 | lun | ) |
Read inquiry datas
| lun,global | lun selected (global!=lun of specific USB device) |
Definition at line 600 of file host_mem.c.
References S_cbw::cmd, CTRL_FAIL, CTRL_NO_PRESENT, S_cbw::dir, DMS_pipe_in, g_readctx_b_run, host_get_data(), host_mem_cbw_init(), host_mem_cbw_send(), host_mem_csw_read(), host_mem_mem_2_ram_stop(), host_mem_select_lun(), host_mem_stall_management(), S_cbw::lgt, S_cbw::lgt_lsb0, PIPE_STALL, SBC_CMD_DIR_IN, SBC_CMD_INQUIRY, and S_cbw::u8_data.
00601 { 00602 U16 nb; 00603 U8 datas[31], status; 00604 00605 if( !host_mem_select_lun(lun) ) 00606 return CTRL_NO_PRESENT; 00607 if (g_readctx_b_run) 00608 { 00609 host_mem_mem_2_ram_stop(); 00610 host_mem_select_lun(lun); 00611 } 00612 00613 host_mem_cbw_init(); 00614 g_ms_cbw.lgt_lsb0 = 0x24; 00615 g_ms_cbw.dir = SBC_CMD_DIR_IN; 00616 g_ms_cbw.lgt = 0x06; 00617 g_ms_cbw.cmd = SBC_CMD_INQUIRY; 00618 //g_ms_cbw.u8_data[16-16] = 0x00; // 16 - CBWCB1 - Option 00619 //g_ms_cbw.u8_data[17-16] = 0x00; // 17 - CBWCB2 - Page or operation code 00620 //g_ms_cbw.u8_data[18-16] = 0x00; // 18 - CBWCB3 - reserved 00621 g_ms_cbw.u8_data[19-16] = 0x24; // 19 - CBWCB4 - Allocation Length 00622 //g_ms_cbw.u8_data[20-16] = 0x00; // 20 - CBWCB5 - Control 00623 if( !host_mem_cbw_send() ) 00624 return CTRL_FAIL; 00625 00626 // Receiv Inquiry data 00627 // Transfer data ... 00628 nb=31; 00629 status = host_get_data(DMS_pipe_in(),&nb,datas); 00630 // Ignore inquiry data 00631 if( PIPE_STALL == status ) 00632 host_mem_stall_management(); 00633 00634 // Read CSW status 00635 return host_mem_csw_read(); 00636 }
| Ctrl_status host_mem_mem_2_ram | ( | U8 | lun, | |
| U32 | addr, | |||
| U8 * | ram | |||
| ) |
Read sectors on lun
| lun,global | lun selected (global!=lun of specific USB device) | |
| addr | Sector address to start read (unit 512B) | |
| *ram | buffer 512B to store the sector readed |
Definition at line 750 of file host_mem.c.
References S_cbw::cmd, CTRL_FAIL, CTRL_GOOD, S_dms_device::device_index, S_cbw::dir, DMS_pipe_in, FALSE, g_ms_sel_dms, g_ms_sel_lun, g_readctx_b_run, g_readctx_u16_sector, g_readctx_u32_addr, g_readctx_u8_device, g_readctx_u8_lun, host_get_data(), host_mem_cbw_init(), host_mem_cbw_send(), host_mem_csw_read(), host_mem_mem_2_ram_stop(), host_mem_select_lun(), host_mem_stall_management(), HOST_MS_CBW_DATA_POS, HOST_SECTOR_SIZE, S_cbw::lgt, S_cbw::lgt_lsb0, S_cbw::lgt_lsb1, S_cbw::lgt_lsb2, S_cbw::lgt_lsb3, S_dms_device::lun_info, MSB0, MSB1, MSB2, MSB3, NULL, PIPE_GOOD, PIPE_STALL, SBC_CMD_DIR_IN, SBC_CMD_READ_10, TRUE, S_lun_info::u8_block_size, and S_cbw::u8_data.
00751 { 00752 U8 status; 00753 U16 nb; 00754 U8 u8_nb_sec_ignore_at_beg, u8_sector_size; 00755 U32 u32_address; 00756 00757 if( !host_mem_select_lun(lun) ) 00758 return CTRL_FAIL; // no present 00759 00760 u8_nb_sec_ignore_at_beg = 0; 00761 00762 if( g_readctx_b_run ) 00763 { 00764 // Check if the sector requested is the following of previous read command 00765 if( ( g_ms_devices[g_ms_sel_dms].device_index != g_readctx_u8_device) 00766 || ( g_readctx_u8_lun != g_ms_sel_lun) 00767 || ( g_readctx_u32_addr > addr) 00768 || ( (g_readctx_u32_addr+g_readctx_u16_sector) <= addr ) ) 00769 { 00770 host_mem_mem_2_ram_stop(); 00771 host_mem_select_lun(lun); 00772 }else{ 00773 u8_nb_sec_ignore_at_beg = addr-g_readctx_u32_addr; 00774 } 00775 } 00776 00777 if( !g_readctx_b_run ) 00778 { 00779 u8_sector_size = g_ms_devices[ g_ms_sel_dms ].lun_info[ g_ms_sel_lun ].u8_block_size; 00780 00781 // Compute the address in physical sector units 00782 u32_address = addr / u8_sector_size; 00783 // Compute the number of sector to ignore from the beginning of the physical sector 00784 u8_nb_sec_ignore_at_beg = addr % u8_sector_size; 00785 // Update context 00786 g_readctx_u16_sector = u8_sector_size; 00787 g_readctx_u32_addr = addr - u8_nb_sec_ignore_at_beg; 00788 00789 // Send CBW 00790 host_mem_cbw_init(); 00791 g_ms_cbw.lgt_lsb0 = 0x00; 00792 g_ms_cbw.lgt_lsb1 = u8_sector_size * (512/256); 00793 g_ms_cbw.lgt_lsb2 = 0x00; 00794 g_ms_cbw.lgt_lsb3 = 0x00; 00795 g_ms_cbw.dir = SBC_CMD_DIR_IN; 00796 g_ms_cbw.lgt = 0x0A; 00797 g_ms_cbw.cmd = SBC_CMD_READ_10; 00798 //g_ms_cbw.u8_data[16-HOST_MS_CBW_DATA_POS] = 0x00; // 16 - CBWCB1 - Option 00799 g_ms_cbw.u8_data[17-HOST_MS_CBW_DATA_POS] = MSB0(u32_address); // 17 - CBWCB2 - MSB3(Logical Block Address) 00800 g_ms_cbw.u8_data[18-HOST_MS_CBW_DATA_POS] = MSB1(u32_address); // 18 - CBWCB3 - MSB2(Logical Block Address) 00801 g_ms_cbw.u8_data[19-HOST_MS_CBW_DATA_POS] = MSB2(u32_address); // 19 - CBWCB4 - MSB1(Logical Block Address) 00802 g_ms_cbw.u8_data[20-HOST_MS_CBW_DATA_POS] = MSB3(u32_address); // 20 - CBWCB5 - MSB0(Logical Block Address) 00803 //g_ms_cbw.u8_data[21-HOST_MS_CBW_DATA_POS] = 0x00; // 21 - CBWCB6 - reserved 00804 //g_ms_cbw.u8_data[22-HOST_MS_CBW_DATA_POS] = 0x00; // 22 - CBWCB7 - MSB1(Transfer Length) 00805 g_ms_cbw.u8_data[23-HOST_MS_CBW_DATA_POS] = 0x01; // 23 - CBWCB8 - MSB0(Transfer Length) 00806 //g_ms_cbw.u8_data[24-HOST_MS_CBW_DATA_POS] = 0x00; // 24 - CBWCB9 - Control 00807 if( !host_mem_cbw_send() ) 00808 return CTRL_FAIL; 00809 } 00810 00811 if( 0 != u8_nb_sec_ignore_at_beg ) 00812 { 00813 // Ignore eventualy first sector of command (in case of device with sector >512B) 00814 // Update sector remaining 00815 g_readctx_u16_sector -= u8_nb_sec_ignore_at_beg; 00816 g_readctx_u32_addr += u8_nb_sec_ignore_at_beg; 00817 while( 0 != u8_nb_sec_ignore_at_beg ) 00818 { 00819 // Read one sector 00820 nb=HOST_SECTOR_SIZE; 00821 status = host_get_data(DMS_pipe_in(),&nb,NULL); 00822 if(PIPE_GOOD != status) 00823 { 00824 if(PIPE_STALL==status) 00825 host_mem_stall_management(); 00826 host_mem_csw_read(); 00827 return CTRL_FAIL; 00828 } 00829 u8_nb_sec_ignore_at_beg--; 00830 } 00831 } 00832 00833 // Transfer data ... 00834 g_readctx_u16_sector--; 00835 g_readctx_u32_addr++; 00836 nb=HOST_SECTOR_SIZE; 00837 status = host_get_data(DMS_pipe_in(),&nb,ram); 00838 if(PIPE_GOOD != status) 00839 { 00840 if(PIPE_STALL==status) 00841 host_mem_stall_management(); 00842 host_mem_csw_read(); 00843 return CTRL_FAIL; 00844 } 00845 00846 if( 0 != g_readctx_u16_sector ) 00847 { 00848 // Update context 00849 g_readctx_u8_device = g_ms_devices[g_ms_sel_dms].device_index; 00850 g_readctx_u8_lun = g_ms_sel_lun; 00851 g_readctx_b_run = TRUE; 00852 return CTRL_GOOD; 00853 } 00854 00855 // Read CSW status 00856 g_readctx_b_run = FALSE; 00857 return host_mem_csw_read(); 00858 }
| Ctrl_status host_mem_mem_2_ram_stop | ( | void | ) |
This function terminates the tranfer of a physical sector from memory.
Definition at line 869 of file host_mem.c.
References CTRL_FAIL, DMS_pipe_in, FALSE, g_ms_sel_dms, g_ms_sel_lun, g_readctx_b_run, g_readctx_u16_sector, g_readctx_u8_device, g_readctx_u8_lun, host_get_data(), host_mem_csw_read(), host_mem_stall_management(), HOST_SECTOR_SIZE, Host_select_device, NULL, PIPE_GOOD, and PIPE_STALL.
00870 { 00871 U16 nb; 00872 U8 status; 00873 00874 g_readctx_b_run = FALSE; 00875 00876 g_ms_sel_lun = g_readctx_u8_lun; 00877 g_ms_sel_dms = g_readctx_u8_device; 00878 Host_select_device( g_ms_devices[g_ms_sel_dms].device_index ); 00879 00880 while( 0 != g_readctx_u16_sector ) 00881 { 00882 // Read one sector 00883 nb=HOST_SECTOR_SIZE; 00884 status = host_get_data(DMS_pipe_in(),&nb,NULL); 00885 if(PIPE_GOOD != status) 00886 { 00887 if(PIPE_STALL==status) 00888 host_mem_stall_management(); 00889 host_mem_csw_read(); 00890 return CTRL_FAIL; 00891 } 00892 g_readctx_u16_sector--; 00893 } 00894 00895 // Read CSW status 00896 return host_mem_csw_read(); 00897 }
| Ctrl_status host_mem_ram_2_mem | ( | U8 | lun, | |
| U32 | addr, | |||
| U8 * | ram | |||
| ) |
Write a sectors
| lun,global | lun selected (global!=lun of specific USB device) | |
| addr | Sector address to start write (unit 512B) | |
| *ram | buffer 512B with the data to store in the sector writed |
Definition at line 912 of file host_mem.c.
References S_cbw::cmd, CTRL_FAIL, CTRL_GOOD, S_cbw::dir, DMS_pipe_out, g_ms_sel_dms, g_ms_sel_lun, g_readctx_b_run, host_mem_cbw_init(), host_mem_cbw_send(), host_mem_csw_read(), host_mem_mem_2_ram(), host_mem_mem_2_ram_stop(), host_mem_select_lun(), host_mem_stall_management(), HOST_MS_CBW_DATA_POS, HOST_SECTOR_SIZE, host_send_data(), S_cbw::lgt, S_cbw::lgt_lsb1, S_dms_device::lun_info, MSB0, MSB1, MSB2, MSB3, PIPE_STALL, SBC_CMD_DIR_OUT, SBC_CMD_WRITE_10, S_lun_info::u8_block_size, S_cbw::u8_data, and USB_SUPPORT_MS_SECTOR_WR_MAX.
00913 { 00914 U8 status; 00915 U16 nb, u16_sector; 00916 U8 u8_nb_sec_ignore_at_beg, u8_sector_size; 00917 U32 u32_address; 00918 #if (USB_SUPPORT_MS_SECTOR_WR_MAX != 1) 00919 Ctrl_status read_status; 00920 U8 u8_i,u8_j; 00921 U32 u32_addr; 00922 #endif 00923 00924 if( !host_mem_select_lun(lun) ) 00925 return CTRL_FAIL; // no present 00926 00927 u8_sector_size = g_ms_devices[ g_ms_sel_dms ].lun_info[ g_ms_sel_lun ].u8_block_size; 00928 00929 if( USB_SUPPORT_MS_SECTOR_WR_MAX < u8_sector_size ) 00930 return CTRL_FAIL; // No supported this lun in write mode, because sector size != 512B 00931 00932 00933 // Compute the address in physical sector units 00934 u32_address = addr / u8_sector_size; 00935 // Compute the number of sector to ignore from the beginning of the physical sector 00936 u8_nb_sec_ignore_at_beg = addr % u8_sector_size; 00937 // Update context 00938 u16_sector = u8_sector_size; 00939 00940 #if (USB_SUPPORT_MS_SECTOR_WR_MAX != 1) 00941 // If the sector size > 512B then read sector and store it in a buffer 00942 if( 1 != u8_sector_size ) 00943 { 00944 u32_addr = addr - u8_nb_sec_ignore_at_beg; 00945 for( u8_i=0,u8_j=0 ; u8_i<u8_sector_size; u8_i++,u32_addr++ ) 00946 { 00947 if( u8_i == u8_nb_sec_ignore_at_beg ) 00948 continue; 00949 read_status = host_mem_mem_2_ram( lun, u32_addr, &g_ms_cache[u8_j*512] ); 00950 if( CTRL_GOOD != read_status ) 00951 return CTRL_GOOD; 00952 u8_j++; 00953 } 00954 } 00955 #endif 00956 00957 if (g_readctx_b_run) 00958 { 00959 host_mem_mem_2_ram_stop(); 00960 host_mem_select_lun(lun); 00961 } 00962 00963 // Send CBW 00964 host_mem_cbw_init(); 00965 //g_ms_cbw.lgt_lsb0 = 0x00; 00966 g_ms_cbw.lgt_lsb1 = u8_sector_size * (512/256); 00967 //g_ms_cbw.lgt_lsb2 = 0x00; 00968 //g_ms_cbw.lgt_lsb3 = 0x00; 00969 g_ms_cbw.dir = SBC_CMD_DIR_OUT; 00970 g_ms_cbw.lgt = 0x0A; 00971 g_ms_cbw.cmd = SBC_CMD_WRITE_10; 00972 //g_ms_cbw.u8_data[16-HOST_MS_CBW_DATA_POS] = 0x00; // 16 - CBWCB1 - Option 00973 g_ms_cbw.u8_data[17-HOST_MS_CBW_DATA_POS] = MSB0(u32_address); // 17 - CBWCB2 - MSB3(Logical Block Address) 00974 g_ms_cbw.u8_data[18-HOST_MS_CBW_DATA_POS] = MSB1(u32_address); // 18 - CBWCB3 - MSB2(Logical Block Address) 00975 g_ms_cbw.u8_data[19-HOST_MS_CBW_DATA_POS] = MSB2(u32_address); // 19 - CBWCB4 - MSB1(Logical Block Address) 00976 g_ms_cbw.u8_data[20-HOST_MS_CBW_DATA_POS] = MSB3(u32_address); // 20 - CBWCB5 - MSB0(Logical Block Address) 00977 //g_ms_cbw.u8_data[21-HOST_MS_CBW_DATA_POS] = 0x00; // 21 - CBWCB6 - reserved 00978 //g_ms_cbw.u8_data[22-HOST_MS_CBW_DATA_POS] = 0x00; // 22 - CBWCB7 - MSB1(Transfer Length) 00979 g_ms_cbw.u8_data[23-HOST_MS_CBW_DATA_POS] = 0x01; // 23 - CBWCB8 - MSB0(Transfer Length) 00980 //g_ms_cbw.u8_data[24-HOST_MS_CBW_DATA_POS] = 0x00; // 24 - CBWCB9 - Control 00981 if( !host_mem_cbw_send() ) 00982 return CTRL_FAIL; 00983 00984 #if (USB_SUPPORT_MS_SECTOR_WR_MAX != 1) 00985 if( 0 != u8_nb_sec_ignore_at_beg ) 00986 { 00987 // Ignore eventualy first sector of command (in case of device with sector >512B) 00988 // Update sector remaining 00989 u16_sector -= u8_nb_sec_ignore_at_beg; 00990 for( u8_i=0; u8_i < u8_nb_sec_ignore_at_beg; u8_i++ ) 00991 { 00992 // Transfer data ... 00993 nb=HOST_SECTOR_SIZE; 00994 status = host_send_data(DMS_pipe_out(),nb,&g_ms_cache[u8_i*512]); 00995 if(status==PIPE_STALL) 00996 { 00997 host_mem_stall_management(); 00998 host_mem_csw_read(); 00999 return CTRL_FAIL; 01000 } 01001 } 01002 } 01003 #endif 01004 01005 // Transfer data ... 01006 u16_sector--; 01007 nb=HOST_SECTOR_SIZE; 01008 status = host_send_data(DMS_pipe_out(),nb,ram); 01009 if(status==PIPE_STALL) 01010 { 01011 host_mem_stall_management(); 01012 host_mem_csw_read(); 01013 return CTRL_FAIL; 01014 } 01015 01016 #if (USB_SUPPORT_MS_SECTOR_WR_MAX != 1) 01017 while( 0 != u16_sector ) 01018 { 01019 // Transfer data ... 01020 nb=HOST_SECTOR_SIZE; 01021 status = host_send_data(DMS_pipe_out(),nb,&g_ms_cache[u8_nb_sec_ignore_at_beg*512]); 01022 if(status==PIPE_STALL) 01023 { 01024 host_mem_stall_management(); 01025 host_mem_csw_read(); 01026 return CTRL_FAIL; 01027 } 01028 u8_nb_sec_ignore_at_beg++; 01029 u16_sector--; 01030 } 01031 #endif 01032 01033 // Read CSW status 01034 return host_mem_csw_read(); 01035 }
| Ctrl_status host_mem_mem_2_ram_ext | ( | U8 | lun, | |
| U32 | addr, | |||
| U8 * | ram, | |||
| U8 | u8_nb_sector | |||
| ) |
Read sectors on lun
| lun,global | lun selected (global!=lun of specific USB device) | |
| addr | Sector address to start read (unit 512B) | |
| *ram | buffer 512B to store the sector readed |
Definition at line 1051 of file host_mem.c.
References S_cbw::cmd, CTRL_FAIL, CTRL_GOOD, S_cbw::dir, DMS_pipe_in, FALSE, g_ms_sel_dms, g_ms_sel_lun, g_readctx_b_run, host_get_data(), host_mem_cbw_init(), host_mem_cbw_send(), host_mem_csw_read(), host_mem_mem_2_ram(), host_mem_mem_2_ram_stop(), host_mem_select_lun(), host_mem_stall_management(), HOST_MS_CBW_DATA_POS, HOST_SECTOR_SIZE, S_cbw::lgt, S_cbw::lgt_lsb0, S_cbw::lgt_lsb1, S_cbw::lgt_lsb2, S_cbw::lgt_lsb3, LSB0, LSB1, LSB2, LSB3, S_dms_device::lun_info, MSB0, MSB1, MSB2, MSB3, PIPE_GOOD, PIPE_STALL, SBC_CMD_DIR_IN, SBC_CMD_READ_10, S_lun_info::u8_block_size, and S_cbw::u8_data.
01052 { 01053 Ctrl_status status; 01054 U8 u8_status; 01055 U8 u8_sector_size; 01056 U16 nb; 01057 U32 dCBWDataTransferLength; 01058 01059 if( !host_mem_select_lun(lun) ) 01060 return CTRL_FAIL; // no present 01061 01062 u8_sector_size = g_ms_devices[ g_ms_sel_dms ].lun_info[ g_ms_sel_lun ].u8_block_size; 01063 01064 if( 1 < u8_sector_size ) 01065 { 01066 // For U-Disk with large block then use standard routine 01067 while( u8_nb_sector != 0 ) { 01068 status = host_mem_mem_2_ram(lun, addr, ram); 01069 if (status != CTRL_GOOD) return status; 01070 u8_nb_sector--; 01071 addr++; 01072 ram = (U8*)ram + HOST_SECTOR_SIZE; 01073 } 01074 return CTRL_GOOD; 01075 } 01076 01077 if (g_readctx_b_run) 01078 { 01079 host_mem_mem_2_ram_stop(); 01080 host_mem_select_lun(lun); 01081 } 01082 01083 dCBWDataTransferLength = (U32)u8_nb_sector * 512; 01084 01085 // Send CBW 01086 host_mem_cbw_init(); 01087 g_ms_cbw.lgt_lsb0 = LSB0(dCBWDataTransferLength); // 8 - LSB0W(dCBWDataTransferLength) 01088 g_ms_cbw.lgt_lsb1 = LSB1(dCBWDataTransferLength); // 9 - LSB1W(dCBWDataTransferLength) 01089 g_ms_cbw.lgt_lsb2 = LSB2(dCBWDataTransferLength); // 10 - LSB2W(dCBWDataTransferLength) 01090 g_ms_cbw.lgt_lsb3 = LSB3(dCBWDataTransferLength); // 11 - LSB3W(dCBWDataTransferLength) 01091 g_ms_cbw.dir = SBC_CMD_DIR_IN; 01092 g_ms_cbw.lgt = 0x0A; 01093 g_ms_cbw.cmd = SBC_CMD_READ_10; 01094 //g_ms_cbw.u8_data[16-HOST_MS_CBW_DATA_POS] = 0x00; // 16 - CBWCB1 - Option 01095 g_ms_cbw.u8_data[17-HOST_MS_CBW_DATA_POS] = MSB0(addr); // 17 - CBWCB2 - MSB3(Logical Block Address) 01096 g_ms_cbw.u8_data[18-HOST_MS_CBW_DATA_POS] = MSB1(addr); // 18 - CBWCB3 - MSB2(Logical Block Address) 01097 g_ms_cbw.u8_data[19-HOST_MS_CBW_DATA_POS] = MSB2(addr); // 19 - CBWCB4 - MSB1(Logical Block Address) 01098 g_ms_cbw.u8_data[20-HOST_MS_CBW_DATA_POS] = MSB3(addr); // 20 - CBWCB5 - MSB0(Logical Block Address) 01099 //g_ms_cbw.u8_data[21-HOST_MS_CBW_DATA_POS] = 0x00; // 21 - CBWCB6 - reserved 01100 //g_ms_cbw.u8_data[22-HOST_MS_CBW_DATA_POS] = 0x00; // 22 - CBWCB7 - MSB1(Transfer Length) 01101 g_ms_cbw.u8_data[23-HOST_MS_CBW_DATA_POS] = u8_nb_sector; // 23 - CBWCB8 - MSB0(Transfer Length) 01102 //g_ms_cbw.u8_data[24-HOST_MS_CBW_DATA_POS] = 0x00; // 24 - CBWCB9 - Control 01103 if( !host_mem_cbw_send() ) 01104 return CTRL_FAIL; 01105 01106 // Transfer data ... 01107 nb=HOST_SECTOR_SIZE; 01108 while( u8_nb_sector!= 0 ) 01109 { 01110 u8_status = host_get_data(DMS_pipe_in(),&nb,ram); 01111 if(PIPE_GOOD != u8_status) 01112 { 01113 if(PIPE_STALL==u8_status) 01114 host_mem_stall_management(); 01115 host_mem_csw_read(); 01116 return CTRL_FAIL; 01117 } 01118 u8_nb_sector--; 01119 ram = (U8*)ram + HOST_SECTOR_SIZE; 01120 } 01121 01122 // Read CSW status 01123 g_readctx_b_run = FALSE; 01124 return host_mem_csw_read(); 01125 }
| Ctrl_status host_mem_ram_2_mem_ext | ( | U8 | lun, | |
| U32 | addr, | |||
| U8 * | ram, | |||
| U8 | u8_nb_sector | |||
| ) |
Write a sectors
| lun,global | lun selected (global!=lun of specific USB device) | |
| addr | Sector address to start write (unit 512B) | |
| u8_nb_sector | Number of sector to write | |
| *ram | buffer with the data to store in the sector writed |
Definition at line 1142 of file host_mem.c.
References S_cbw::cmd, CTRL_FAIL, S_cbw::dir, DMS_pipe_out, g_ms_sel_dms, g_ms_sel_lun, g_readctx_b_run, host_mem_cbw_init(), host_mem_cbw_send(), host_mem_csw_read(), host_mem_mem_2_ram_stop(), host_mem_select_lun(), host_mem_stall_management(), HOST_MS_CBW_DATA_POS, HOST_SECTOR_SIZE, host_send_data(), S_cbw::lgt, S_cbw::lgt_lsb0, S_cbw::lgt_lsb1, S_cbw::lgt_lsb2, S_cbw::lgt_lsb3, LSB0, LSB1, LSB2, LSB3, S_dms_device::lun_info, MSB0, MSB1, MSB2, MSB3, PIPE_STALL, SBC_CMD_DIR_OUT, SBC_CMD_WRITE_10, S_lun_info::u8_block_size, and S_cbw::u8_data.
01143 { 01144 U8 status; 01145 U16 nb; 01146 U8 u8_sector_size; 01147 U32 dCBWDataTransferLength; 01148 01149 if( !host_mem_select_lun(lun) ) 01150 return CTRL_FAIL; // no present 01151 01152 u8_sector_size = g_ms_devices[ g_ms_sel_dms ].lun_info[ g_ms_sel_lun ].u8_block_size; 01153 01154 if( 1 < u8_sector_size ) 01155 return CTRL_FAIL; // No supported this lun in write mode, because sector size != 512B 01156 01157 01158 if (g_readctx_b_run) 01159 { 01160 host_mem_mem_2_ram_stop(); 01161 host_mem_select_lun(lun); 01162 } 01163 01164 dCBWDataTransferLength = (U32)u8_nb_sector * 512; 01165 01166 // Send CBW 01167 host_mem_cbw_init(); 01168 g_ms_cbw.lgt_lsb0 = LSB0(dCBWDataTransferLength); // 8 - LSB0W(dCBWDataTransferLength) 01169 g_ms_cbw.lgt_lsb1 = LSB1(dCBWDataTransferLength); // 9 - LSB1W(dCBWDataTransferLength) 01170 g_ms_cbw.lgt_lsb2 = LSB2(dCBWDataTransferLength); // 10 - LSB2W(dCBWDataTransferLength) 01171 g_ms_cbw.lgt_lsb3 = LSB3(dCBWDataTransferLength); // 11 - LSB3W(dCBWDataTransferLength) 01172 g_ms_cbw.dir = SBC_CMD_DIR_OUT; 01173 g_ms_cbw.lgt = 0x0A; 01174 g_ms_cbw.cmd = SBC_CMD_WRITE_10; 01175 //g_ms_cbw.u8_data[16-HOST_MS_CBW_DATA_POS] = 0x00; // 16 - CBWCB1 - Option 01176 g_ms_cbw.u8_data[17-HOST_MS_CBW_DATA_POS] = MSB0(addr); // 17 - CBWCB2 - MSB3(Logical Block Address) 01177 g_ms_cbw.u8_data[18-HOST_MS_CBW_DATA_POS] = MSB1(addr); // 18 - CBWCB3 - MSB2(Logical Block Address) 01178 g_ms_cbw.u8_data[19-HOST_MS_CBW_DATA_POS] = MSB2(addr); // 19 - CBWCB4 - MSB1(Logical Block Address) 01179 g_ms_cbw.u8_data[20-HOST_MS_CBW_DATA_POS] = MSB3(addr); // 20 - CBWCB5 - MSB0(Logical Block Address) 01180 //g_ms_cbw.u8_data[21-HOST_MS_CBW_DATA_POS] = 0x00; // 21 - CBWCB6 - reserved 01181 //g_ms_cbw.u8_data[22-HOST_MS_CBW_DATA_POS] = 0x00; // 22 - CBWCB7 - MSB1(Transfer Length) 01182 g_ms_cbw.u8_data[23-HOST_MS_CBW_DATA_POS] = u8_nb_sector;// 23 - CBWCB8 - MSB0(Transfer Length) 01183 //g_ms_cbw.u8_data[24-HOST_MS_CBW_DATA_POS] = 0x00; // 24 - CBWCB9 - Control 01184 if( !host_mem_cbw_send() ) 01185 return CTRL_FAIL; 01186 01187 // Transfer data ... 01188 nb=HOST_SECTOR_SIZE; 01189 while( u8_nb_sector!= 0 ) 01190 { 01191 status = host_send_data(DMS_pipe_out(),nb,ram); 01192 if(status==PIPE_STALL) 01193 { 01194 host_mem_stall_management(); 01195 host_mem_csw_read(); 01196 return CTRL_FAIL; 01197 } 01198 u8_nb_sector--; 01199 ram = (U8*)ram + HOST_SECTOR_SIZE; 01200 } 01201 01202 // Read CSW status 01203 return host_mem_csw_read(); 01204 }
1.5.3