#include "conf_explorer.h"
Go to the source code of this file.
Data Structures | |
| struct | Fs_index |
Defines | |
| #define | _GLOBEXT_ extern |
| Used to have a clear code with only one segment to define a variable in project. | |
Modes of file name control functions | |
| #define | FS_NAME_GET TRUE |
| #define | FS_NAME_CHECK FALSE |
Modes of disk serial number function | |
| #define | FS_SN_READ TRUE |
| #define | FS_SN_WRITE FALSE |
Modes of disk label function | |
| #define | FS_LABEL_READ TRUE |
| #define | FS_LABEL_WRITE FALSE |
Status returned by paste file function | |
| #define | COPY_BUSY 0x00 |
| #define | COPY_FAIL 0x01 |
| #define | COPY_FINISH 0x02 |
Date field managed by date control functions | |
| #define | FS_DATE_CREATION TRUE |
| #define | FS_DATE_LAST_WRITE FALSE |
File entry types used by many functions | |
| #define | FS_FILE TRUE |
| #define | FS_DIR FALSE |
Directory identifier, which corresponding at the first cluster of directory cluster list | |
| #define | FS_ID_DIR_EMPTY 0xFFFFFFFF |
| #define | FS_ID_DIR_ROOT 0 |
File entry attributes | |
| #define | FS_ATTR_FILE ((Byte)0x00) |
| #define | FS_ATTR_READ_ONLY ((Byte)0x01) |
| #define | FS_ATTR_HIDDEN ((Byte)0x02) |
| #define | FS_ATTR_SYSTEM ((Byte)0x04) |
| #define | FS_ATTR_VOLUME_ID ((Byte)0x08) |
| #define | FS_ATTR_DIRECTORY ((Byte)0x10) |
| #define | FS_ATTR_ARCHIVE ((Byte)0x20) |
| #define | FS_ATTR_LFN_ENTRY ((Byte)0x0F) |
| #define | Fat_is_not_a_file ((FS_ATTR_DIRECTORY & fs_g_nav_entry.u8_attr) || (FS_ATTR_VOLUME_ID & fs_g_nav_entry.u8_attr)) |
File open modes | |
| #define | FOPEN_READ_ACCESS 0x01 |
| #define | FOPEN_WRITE_ACCESS 0x02 |
| #define | FOPEN_CLEAR_SIZE 0x04 |
| #define | FOPEN_CLEAR_PTR 0x08 |
| #define | FOPEN_MODE_R (FOPEN_READ_ACCESS|FOPEN_CLEAR_PTR) |
| R access, flux pointer = 0, size not modify. | |
| #define | FOPEN_MODE_R_PLUS (FOPEN_READ_ACCESS|FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR) |
| R/W access, flux pointer = 0, size not modify. | |
| #define | FOPEN_MODE_W (FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR|FOPEN_CLEAR_SIZE) |
| W access, flux pointer = 0, size = 0. | |
| #define | FOPEN_MODE_W_PLUS (FOPEN_READ_ACCESS|FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR|FOPEN_CLEAR_SIZE) |
| R/W access, flux pointer = 0, size = 0. | |
| #define | FOPEN_MODE_APPEND (FOPEN_WRITE_ACCESS) |
| W access, flux pointer = at the end, size not modify. | |
Value to signal the end of file after a file_getc() call | |
| #define | FS_EOF 0xFFFF |
Options of format function | |
| #define | FS_FORMAT_DEFAULT 0x01 |
| The format routine chooses the better FAT for the device. | |
| #define | FS_FORMAT_FAT 0x02 |
| Force FAT12 or FAT16 format. | |
| #define | FS_FORMAT_FAT32 0x03 |
| Force FAT32 format. | |
| #define | FS_FORMAT_NOMBR_FLAG 0x80 |
| MBR is mandatory for USB device on MacOS, and no MBR is mandatory for CD-ROM USB device on Windows. | |
| #define | FS_FORMAT_DEFAULT_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_DEFAULT) |
| #define | FS_FORMAT_FAT_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_FAT) |
| #define | FS_FORMAT_FAT32_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_FAT32) |
File System errors list | |
| #define | FS_ERR_HW (FAIL+0) |
| Hardware driver error. | |
| #define | FS_ERR_NO_FORMAT (FAIL+1) |
| The selected drive isn't formated. | |
| #define | FS_ERR_NO_PART (FAIL+2) |
| The selected partition doesn't existed. | |
| #define | FS_ERR_NO_SUPPORT_PART (FAIL+3) |
| The selected partition isn't supported. | |
| #define | FS_ERR_TOO_FILE_OPEN (FAIL+4) |
| The navigation have already opened a file. | |
| #define | FS_ERR_END_OF_DRIVE (FAIL+5) |
| There are not other driver. | |
| #define | FS_ERR_BAD_POS (FAIL+6) |
| The position is over the file. | |
| #define | FS_ERR_FS (FAIL+7) |
| File system error. | |
| #define | FS_ERR_NO_FIND (FAIL+8) |
| File no found. | |
| #define | FS_ERR_ENTRY_EMPTY (FAIL+9) |
| File entry empty. | |
| #define | FS_ERR_ENTRY_BAD (FAIL+10) |
| File entry bad. | |
| #define | FS_ERR_ENTRY_BADTYPE (FAIL+11) |
| File entry type don't corresponding. | |
| #define | FS_ERR_NO_DIR (FAIL+12) |
| The selected file isn't a directory. | |
| #define | FS_ERR_NO_MOUNT (FAIL+13) |
| The partition isn't mounted. | |
| #define | FS_ERR_NO_FILE_SEL (FAIL+14) |
| There are no selected file. | |
| #define | FS_NO_LAST_LFN_ENTRY (FAIL+15) |
| The file entry isn't the last long file entry. | |
| #define | FS_ERR_ID_FILE (FAIL+17) |
| The file identifier is bad. | |
| #define | FS_ERR_NO_FILE (FAIL+18) |
| The selected file entry isn't a file. | |
| #define | FS_LUN_WP (FAIL+19) |
| Drive is in read only mode. | |
| #define | FS_ERR_READ_ONLY (FAIL+20) |
| File is on read access only. | |
| #define | FS_ERR_NAME_INCORRECT (FAIL+21) |
| The name don't corresponding at the filter name. | |
| #define | FS_ERR_FILE_NO_OPEN (FAIL+22) |
| No file is opened. | |
| #define | FS_ERR_HW_NO_PRESENT (FAIL+23) |
| Device is not present. | |
| #define | FS_ERR_IS_ROOT (FAIL+24) |
| There aren't parent because the current directory is a root directory. | |
| #define | FS_ERR_OUT_LIST (FAIL+25) |
| The position is outside the cluster list. | |
| #define | FS_ERR_NO_FREE_SPACE (FAIL+26) |
| No free cluster found in FAT. | |
| #define | FS_ERR_INCORRECT_NAME (FAIL+27) |
| Incorrect name, this one cannot contain any of the following characters \/:*?"<>|. | |
| #define | FS_ERR_DIR_NOT_EMPTY (FAIL+28) |
| This function erases only file and empty directory. | |
| #define | FS_ERR_WRITE_ONLY (FAIL+29) |
| File is on write access only. | |
| #define | FS_ERR_MODE_NOAVIALABLE (FAIL+30) |
| This open mode isn't available. | |
| #define | FS_ERR_EOF (FAIL+31) |
| End of file. | |
| #define | FS_ERR_BAD_SIZE_FAT (FAIL+32) |
| The disk size is not supported by selected FAT format. | |
| #define | FS_ERR_COMMAND (FAIL+33) |
| This command is not supported. | |
| #define | FS_ERR_BUFFER_FULL (FAIL+34) |
| Buffer is too small. | |
| #define | FS_ERR_COPY_DIR (FAIL+35) |
| Directory copy is not supported. | |
| #define | FS_ERR_COPY_RUNNING (FAIL+36) |
| A copy action is always running. | |
| #define | FS_ERR_COPY_IMPOSSIBLE (FAIL+37) |
| The copy is impossible. | |
| #define | FS_ERR_BAD_NAV (FAIL+38) |
| The navigator identifier doesn't existed. | |
| #define | FS_ERR_FILE_OPEN (FAIL+39) |
| The file is already opened. | |
| #define | FS_ERR_FILE_OPEN_WR (FAIL+40) |
| The file is already opened in write mode. | |
| #define | FS_ERR_FILE_EXIST (FAIL+41) |
| The file is already existed. | |
| #define | FS_ERR_NAME_TOO_LARGE (FAIL+42) |
| The file name is too large (>260 characters). | |
| #define | FS_ERR_DEVICE_TOO_SMALL (FAIL+43) |
| The disk size is too small for format routine. | |
| #define | FS_ERR_PL_NOT_OPEN (FAIL+50) |
| The play list isn't opened. | |
| #define | FS_ERR_PL_ALREADY_OPEN (FAIL+51) |
| The play list is already opened. | |
| #define | FS_ERR_PL_LST_END (FAIL+52) |
| You are at the end of play list. | |
| #define | FS_ERR_PL_LST_BEG (FAIL+53) |
| You are at the beginning of play list. | |
| #define | FS_ERR_PL_OUT_LST (FAIL+54) |
| You are outside of the play list. | |
| #define | FS_ERR_PL_READ_ONLY (FAIL+55) |
| Impossible to modify the play list. | |
Compilation feature levels | |
| #define | FSFEATURE_READ 0x00 |
| All read functions. | |
| #define | FSFEATURE_WRITE 0x02 |
| nav_file_copy(), nav_file_paste(), nav_file_del(), file_create(), file_open(MODE_WRITE), file_write(), file_putc() | |
| #define | FSFEATURE_WRITE_COMPLET 0x06 |
| FSFEATURE_WRITE + nav_drive_format(), nav_dir_make(), nav_file_rename(), nav_file_dateset(), nav_file_attributset(). | |
| #define | FSFEATURE_ALL 0xFF |
| All file system module. | |
Typedefs | |
String types depend of ASCII and UNICODE options | |
| typedef U16 | UNICODE |
| typedef char _MEM_TYPE_SLOW_ * | FS_STRING |
| typedef UNICODE _MEM_TYPE_SLOW_ * | FS_STR_UNICODE |
Status type for the file system | |
| typedef U8 | Fs_status |
Variables | |
Global status of file system module (used to return error number) | |
| _MEM_TYPE_SLOW_ Fs_status | fs_g_status |
This file provides a set of definitions for FAT module interface.
Definition in file fs_com.h.
| #define _GLOBEXT_ extern |
| #define FS_NAME_GET TRUE |
Definition at line 84 of file fs_com.h.
Referenced by copy_dir(), fat_entry_longname(), fat_entry_shortname(), nav_dir_name(), nav_file_getname(), nav_file_name(), nav_getcwd(), ushell_cmd_copy(), ushell_cmd_ls(), and ushell_cmd_sync().
| #define FS_NAME_CHECK FALSE |
| #define FS_LABEL_READ TRUE |
| #define FS_LABEL_WRITE FALSE |
| #define COPY_BUSY 0x00 |
Definition at line 102 of file fs_com.h.
Referenced by copy_dir(), ushell_cmd_copy(), and ushell_cmd_sync().
| #define COPY_FAIL 0x01 |
| #define COPY_FINISH 0x02 |
| #define FS_DATE_LAST_WRITE FALSE |
| #define FS_FILE TRUE |
Definition at line 115 of file fs_com.h.
Referenced by fat_entry_check(), nav_dir_name(), nav_filelist_nb(), and nav_filelist_set().
| #define FS_DIR FALSE |
Definition at line 116 of file fs_com.h.
Referenced by fat_clear_entry_info_and_ptr(), fat_entry_check(), nav_dir_gotoparent(), nav_filelist_eol(), and nav_filelist_set().
| #define FS_ATTR_READ_ONLY ((Byte)0x01) |
| #define FS_ATTR_VOLUME_ID ((Byte)0x08) |
| #define FS_ATTR_DIRECTORY ((Byte)0x10) |
| #define FS_ATTR_LFN_ENTRY ((Byte)0x0F) |
| #define Fat_is_not_a_file ((FS_ATTR_DIRECTORY & fs_g_nav_entry.u8_attr) || (FS_ATTR_VOLUME_ID & fs_g_nav_entry.u8_attr)) |
| #define FOPEN_READ_ACCESS 0x01 |
Definition at line 140 of file fs_com.h.
Referenced by file_getc(), file_read(), and file_read_buf().
| #define FOPEN_WRITE_ACCESS 0x02 |
| #define FOPEN_CLEAR_SIZE 0x04 |
| #define FOPEN_CLEAR_PTR 0x08 |
| #define FOPEN_MODE_R (FOPEN_READ_ACCESS|FOPEN_CLEAR_PTR) |
R access, flux pointer = 0, size not modify.
Definition at line 144 of file fs_com.h.
Referenced by ushell_cmd_cat().
| #define FOPEN_MODE_R_PLUS (FOPEN_READ_ACCESS|FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR) |
| #define FOPEN_MODE_W (FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR|FOPEN_CLEAR_SIZE) |
W access, flux pointer = 0, size = 0.
Definition at line 146 of file fs_com.h.
Referenced by ushell_cmd_perform_alloc().
| #define FOPEN_MODE_W_PLUS (FOPEN_READ_ACCESS|FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR|FOPEN_CLEAR_SIZE) |
| #define FOPEN_MODE_APPEND (FOPEN_WRITE_ACCESS) |
W access, flux pointer = at the end, size not modify.
Definition at line 148 of file fs_com.h.
Referenced by ushell_cmd_append_file().
| #define FS_EOF 0xFFFF |
| #define FS_FORMAT_DEFAULT 0x01 |
The format routine chooses the better FAT for the device.
Definition at line 156 of file fs_com.h.
Referenced by ushell_cmd_format().
| #define FS_FORMAT_NOMBR_FLAG 0x80 |
| #define FS_FORMAT_DEFAULT_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_DEFAULT) |
| #define FS_FORMAT_FAT_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_FAT) |
| #define FS_FORMAT_FAT32_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_FAT32) |
| #define FS_ERR_HW (FAIL+0) |
Hardware driver error.
Definition at line 190 of file fs_com.h.
Referenced by fat_cache_flush(), fat_cache_read_sector(), fat_check_device(), and file_read_buf().
| #define FS_ERR_NO_FORMAT (FAIL+1) |
The selected drive isn't formated.
Definition at line 191 of file fs_com.h.
Referenced by fat_mount().
| #define FS_ERR_NO_PART (FAIL+2) |
The selected partition doesn't existed.
Definition at line 192 of file fs_com.h.
Referenced by fat_mount().
| #define FS_ERR_NO_SUPPORT_PART (FAIL+3) |
The selected partition isn't supported.
Definition at line 193 of file fs_com.h.
Referenced by fat_mount().
| #define FS_ERR_TOO_FILE_OPEN (FAIL+4) |
The navigation have already opened a file.
Definition at line 194 of file fs_com.h.
Referenced by fat_check_noopen().
| #define FS_ERR_END_OF_DRIVE (FAIL+5) |
| #define FS_ERR_BAD_POS (FAIL+6) |
| #define FS_ERR_FS (FAIL+7) |
File system error.
Definition at line 197 of file fs_com.h.
Referenced by fat_cluster_list(), nav_dir_gotoparent(), and nav_filelist_set().
| #define FS_ERR_NO_FIND (FAIL+8) |
File no found.
Definition at line 198 of file fs_com.h.
Referenced by nav_filelist_first(), nav_filelist_last(), and nav_filelist_set().
| #define FS_ERR_ENTRY_EMPTY (FAIL+9) |
File entry empty.
Definition at line 199 of file fs_com.h.
Referenced by fat_entry_check(), nav_filelist_set(), and nav_partition_label().
| #define FS_ERR_ENTRY_BAD (FAIL+10) |
File entry bad.
Definition at line 200 of file fs_com.h.
Referenced by fat_entry_check(), fat_entry_longname(), and nav_file_name().
| #define FS_ERR_ENTRY_BADTYPE (FAIL+11) |
| #define FS_ERR_NO_DIR (FAIL+12) |
The selected file isn't a directory.
Definition at line 202 of file fs_com.h.
Referenced by copy_dir(), fat_entry_is_dir(), and ushell_cmd_sync().
| #define FS_ERR_NO_MOUNT (FAIL+13) |
The partition isn't mounted.
Definition at line 203 of file fs_com.h.
Referenced by fat_check_mount().
| #define FS_ERR_NO_FILE_SEL (FAIL+14) |
There are no selected file.
Definition at line 204 of file fs_com.h.
Referenced by fat_check_select().
| #define FS_NO_LAST_LFN_ENTRY (FAIL+15) |
The file entry isn't the last long file entry.
Definition at line 205 of file fs_com.h.
Referenced by fat_entry_longname(), and nav_file_name().
| #define FS_ERR_ID_FILE (FAIL+17) |
| #define FS_ERR_NO_FILE (FAIL+18) |
The selected file entry isn't a file.
Definition at line 208 of file fs_com.h.
Referenced by fat_check_is_file().
| #define FS_LUN_WP (FAIL+19) |
Drive is in read only mode.
Definition at line 209 of file fs_com.h.
Referenced by fat_cache_flush(), and file_open().
| #define FS_ERR_READ_ONLY (FAIL+20) |
| #define FS_ERR_NAME_INCORRECT (FAIL+21) |
The name don't corresponding at the filter name.
Definition at line 211 of file fs_com.h.
Referenced by fat_entry_longname(), and fat_entry_shortname().
| #define FS_ERR_FILE_NO_OPEN (FAIL+22) |
| #define FS_ERR_HW_NO_PRESENT (FAIL+23) |
| #define FS_ERR_IS_ROOT (FAIL+24) |
There aren't parent because the current directory is a root directory.
Definition at line 214 of file fs_com.h.
Referenced by nav_dir_gotoparent(), and nav_getcwd().
| #define FS_ERR_OUT_LIST (FAIL+25) |
The position is outside the cluster list.
Definition at line 215 of file fs_com.h.
Referenced by fat_cluster_list(), fat_read_file(), file_getc(), file_read(), file_read_buf(), and nav_filelist_set().
| #define FS_ERR_NO_FREE_SPACE (FAIL+26) |
| #define FS_ERR_INCORRECT_NAME (FAIL+27) |
| #define FS_ERR_DIR_NOT_EMPTY (FAIL+28) |
| #define FS_ERR_WRITE_ONLY (FAIL+29) |
File is on write access only.
Definition at line 219 of file fs_com.h.
Referenced by file_getc(), file_read(), and file_read_buf().
| #define FS_ERR_MODE_NOAVIALABLE (FAIL+30) |
| #define FS_ERR_EOF (FAIL+31) |
End of file.
Definition at line 221 of file fs_com.h.
Referenced by file_getc(), file_read(), and file_read_buf().
| #define FS_ERR_BAD_SIZE_FAT (FAIL+32) |
| #define FS_ERR_COMMAND (FAIL+33) |
This command is not supported.
Definition at line 223 of file fs_com.h.
Referenced by fat_cluster_val().
| #define FS_ERR_BUFFER_FULL (FAIL+34) |
| #define FS_ERR_COPY_DIR (FAIL+35) |
| #define FS_ERR_COPY_RUNNING (FAIL+36) |
| #define FS_ERR_COPY_IMPOSSIBLE (FAIL+37) |
| #define FS_ERR_BAD_NAV (FAIL+38) |
The navigator identifier doesn't existed.
Definition at line 228 of file fs_com.h.
Referenced by nav_select().
| #define FS_ERR_FILE_OPEN (FAIL+39) |
| #define FS_ERR_FILE_OPEN_WR (FAIL+40) |
| #define FS_ERR_FILE_EXIST (FAIL+41) |
The file is already existed.
Definition at line 231 of file fs_com.h.
Referenced by copy_dir(), ushell_cmd_perform_alloc(), and ushell_cmd_sync().
| #define FS_ERR_NAME_TOO_LARGE (FAIL+42) |
| #define FS_ERR_DEVICE_TOO_SMALL (FAIL+43) |
| #define FS_ERR_PL_NOT_OPEN (FAIL+50) |
| #define FS_ERR_PL_ALREADY_OPEN (FAIL+51) |
| #define FS_ERR_PL_LST_END (FAIL+52) |
| #define FS_ERR_PL_LST_BEG (FAIL+53) |
| #define FS_ERR_PL_OUT_LST (FAIL+54) |
| #define FS_ERR_PL_READ_ONLY (FAIL+55) |
| #define FSFEATURE_WRITE 0x02 |
nav_file_copy(), nav_file_paste(), nav_file_del(), file_create(), file_open(MODE_WRITE), file_write(), file_putc()
| #define FSFEATURE_WRITE_COMPLET 0x06 |
FSFEATURE_WRITE + nav_drive_format(), nav_dir_make(), nav_file_rename(), nav_file_dateset(), nav_file_attributset().
| typedef UNICODE _MEM_TYPE_SLOW_* FS_STR_UNICODE |
| _MEM_TYPE_SLOW_ Fs_status fs_g_status |
Referenced by copy_dir(), fat_cache_flush(), fat_cache_read_sector(), fat_check_device(), fat_check_is_file(), fat_check_mount(), fat_check_noopen(), fat_check_open(), fat_check_select(), fat_cluster_list(), fat_cluster_val(), fat_entry_check(), fat_entry_is_dir(), fat_entry_longname(), fat_entry_shortname(), fat_mount(), fat_read_file(), file_getc(), file_open(), file_read(), file_read_buf(), file_seek(), nav_dir_gotoparent(), nav_drive_set(), nav_file_name(), nav_filelist_first(), nav_filelist_last(), nav_filelist_set(), nav_getcwd(), nav_partition_label(), nav_select(), ushell_cmd_perform_alloc(), and ushell_cmd_sync().
1.5.3