#include "conf_explorer.h"
#include "file.h"
#include "navigation.h"
#include <LIB_MEM>
#include <LIB_CTRLACCESS>
Go to the source code of this file.
Functions | |
| static void | file_load_segment_value (Fs_file_segment _MEM_TYPE_SLOW_ *segment) |
| This function stores the global segment variable in other variable. | |
| Bool | file_ispresent (void) |
| This function checks if a file is selected. | |
| Bool | file_open (U8 fopen_mode) |
| This function opens the selected file. | |
| Bool | file_read (Fs_file_segment _MEM_TYPE_SLOW_ *segment) |
| This function returns a segment (position & size) in a physical memory corresponding at the file. | |
| U16 | file_read_buf (U8 _MEM_TYPE_SLOW_ *buffer, U16 u16_buf_size) |
| This function copys in a buffer the file data corresponding at the current position. | |
| U16 | file_getc (void) |
| This function returns the next byte of file. | |
| U32 | file_getpos (void) |
| This function returns the position in the file. | |
| Bool | file_seek (U32 u32_pos, U8 u8_whence) |
| This function changes the position in the file. | |
| U8 | file_bof (void) |
| This function checks the beginning of file. | |
| U8 | file_eof (void) |
| This function checks the end of file. | |
| void | file_flush (void) |
| This function flushs the internal cache (file datas and file information). | |
| void | file_close (void) |
| This function closes the file. | |
Variables | |
| _MEM_TYPE_SLOW_ U8 | fs_g_sector [512] |
| Use "FAT sector cache" to store a sector from a file (see file_putc(), file_getc(), file_read_buf(), file_write_buf()). | |
This file defines a useful set of functions for the file accesses on AVR32 devices.
Definition in file file.c.
| static void file_load_segment_value | ( | Fs_file_segment _MEM_TYPE_SLOW_ * | segment | ) | [static] |
This function stores the global segment variable in other variable.
| segment | Pointer on the variable to fill |
Definition at line 147 of file file.c.
References fs_g_nav, fs_g_seg, Fs_segment::u32_addr, Fs_segment::u32_size_or_pos, and Fs_management::u8_lun.
Referenced by file_read().
00148 { 00149 segment->u8_lun = fs_g_nav.u8_lun; 00150 segment->u32_addr = fs_g_seg.u32_addr; 00151 segment->u16_size = fs_g_seg.u32_size_or_pos; 00152 }
| Bool file_ispresent | ( | void | ) |
This function checks if a file is selected.
FALSE, otherwise
Definition at line 72 of file file.c.
00073 { 00074 if( !fat_check_mount_select() ) 00075 return FALSE; 00076 return fat_check_is_file(); 00077 }
This function opens the selected file.
| fopen_mode | option to open the file : FOPEN_MODE_R R access, flux pointer = 0, size not modify FOPEN_MODE_R_PLUS R/W access, flux pointer = 0, size not modify FOPEN_MODE_W W access, flux pointer = 0, size = 0 FOPEN_MODE_W_PLUS R/W access, flux pointer = 0, size = 0 FOPEN_MODE_APPEND W access, flux pointer = at the end, size not modify |
TRUE otherwise
Definition at line 92 of file file.c.
Referenced by ushell_cmd_append_file(), ushell_cmd_cat(), and ushell_cmd_perform_alloc().
00093 { 00094 if( !fat_check_mount_select_noopen()) 00095 return FALSE; 00096 00097 if( !fat_check_is_file()) 00098 return FALSE; 00099 00100 if(FOPEN_WRITE_ACCESS & fopen_mode) 00101 { 00102 if( !fat_check_nav_access_file( TRUE ) ) 00103 return FALSE; 00104 #if (FSFEATURE_WRITE == (FS_LEVEL_FEATURES & FSFEATURE_WRITE)) 00105 if (FS_ATTR_READ_ONLY & fs_g_nav_entry.u8_attr) 00106 { 00107 fs_g_status = FS_ERR_READ_ONLY; // File is read only 00108 return FALSE; 00109 } 00110 if( mem_wr_protect( fs_g_nav.u8_lun )) 00111 { 00112 fs_g_status = FS_LUN_WP; // Disk read only 00113 return FALSE; 00114 } 00115 #else 00116 fs_g_status = FS_ERR_MODE_NOAVIALABLE; 00117 return FALSE; 00118 #endif // FS_LEVEL_FEATURES 00119 } 00120 else 00121 { 00122 if( !fat_check_nav_access_file( FALSE ) ) 00123 return FALSE; 00124 } 00125 00126 if(FOPEN_CLEAR_SIZE & fopen_mode) 00127 { 00128 fs_g_nav_entry.u32_size = 0; // The size is null 00129 } 00130 if(FOPEN_CLEAR_PTR & fopen_mode) 00131 { 00132 fs_g_nav_entry.u32_pos_in_file = 0; 00133 } 00134 else 00135 { // Go to at the end of file 00136 fs_g_nav_entry.u32_pos_in_file = fs_g_nav_entry.u32_size; 00137 } 00138 fs_g_nav_entry.u8_open_mode = fopen_mode; 00139 return TRUE; 00140 }
| Bool file_read | ( | Fs_file_segment _MEM_TYPE_SLOW_ * | segment | ) |
This function returns a segment (position & size) in a physical memory corresponding at the file.
| segment | Pointer on the segment structure: ->u32_size_or_pos IN, shall contains maximum number of sector to read in file (0 = unlimited) ->u32_size_or_pos OUT, containt the segment size (unit sector) ->other IN, ignored ->other OUT, contains the segment position |
TRUE otherwise
//! This routine is interesting to read a file via a DMA and avoid the file system decode //! because this routine returns a physical memory segment without File System information. //! Note: the file can be fragmented and you must call file_read() for each fragments. //!
Definition at line 172 of file file.c.
00173 { 00174 U8 u8_nb_sector_truncated; 00175 00176 if( !fat_check_mount_select_open()) 00177 return FALSE; 00178 00179 if(!(FOPEN_READ_ACCESS & fs_g_nav_entry.u8_open_mode)) 00180 { 00181 fs_g_status = FS_ERR_WRITE_ONLY; 00182 return FALSE; 00183 } 00184 00185 if ( file_eof() ) 00186 { 00187 // End of the file 00188 fs_g_status = FS_ERR_EOF; 00189 return FALSE; 00190 } 00191 00192 if( !fat_read_file(FS_CLUST_ACT_SEG)) 00193 { 00194 if( FS_ERR_OUT_LIST == fs_g_status ) 00195 fs_g_status = FS_ERR_EOF; // translate the error 00196 return FALSE; 00197 } 00198 // If the segment is too large then truncate it 00199 if( (segment->u16_size != 0) // if no limit then no truncate 00200 && (segment->u16_size < fs_g_seg.u32_size_or_pos) ) 00201 { 00202 u8_nb_sector_truncated = fs_g_seg.u32_size_or_pos - segment->u16_size; 00203 fs_g_seg.u32_size_or_pos = segment->u16_size ; 00204 }else{ 00205 u8_nb_sector_truncated = 0; 00206 } 00207 00208 // Update file position 00209 fs_g_nav_entry.u32_pos_in_file += (U32)fs_g_seg.u32_size_or_pos * FS_512B; 00210 if( fs_g_nav_entry.u32_size < fs_g_nav_entry.u32_pos_in_file ) 00211 { 00212 // The segment is more larger then file 00213 // case possible: if the file don't use all cluster space 00214 // then compute sectors not used in last cluster of file cluster list 00215 U8 u8_nb_sector_not_used; 00216 00217 // Compute the number of sector used in last cluster 00218 // remark: also the two first bytes of size is used, because the cluster size can't be more larger then 64KB 00219 u8_nb_sector_not_used = LSB1( fs_g_nav_entry.u32_size ) >> (FS_512B_SHIFT_BIT-8); 00220 if( 0 != (fs_g_nav_entry.u32_size & FS_512B_MASK) ) 00221 { // last sector of file isn't full, but it must been read 00222 u8_nb_sector_not_used++; 00223 } 00224 00225 // Compute the number of sector not used in last cluster 00226 u8_nb_sector_not_used = fs_g_nav.u8_BPB_SecPerClus - (u8_nb_sector_not_used % fs_g_nav.u8_BPB_SecPerClus); 00227 // if all space of cluster isn't used, then it is wrong 00228 if( u8_nb_sector_not_used == fs_g_nav.u8_BPB_SecPerClus ) 00229 u8_nb_sector_not_used = 0; // The file uses all last cluster space 00230 00231 // Subtract this value a the file position and segment size 00232 u8_nb_sector_not_used -= u8_nb_sector_truncated; 00233 fs_g_seg.u32_size_or_pos -= u8_nb_sector_not_used; // unit sector 00234 fs_g_nav_entry.u32_pos_in_file -= ((U16)u8_nb_sector_not_used) << FS_512B_SHIFT_BIT; // unit byte 00235 } 00236 file_load_segment_value( segment ); 00237 return TRUE; 00238 }
This function copys in a buffer the file data corresponding at the current position.
| buffer | buffer to fill | |
| u16_buf_size | buffer size |
0, in case of error
Definition at line 249 of file file.c.
00250 { 00251 _MEM_TYPE_FAST_ U16 u16_nb_read_tmp; 00252 _MEM_TYPE_FAST_ U16 u16_nb_read; 00253 _MEM_TYPE_FAST_ U16 u16_pos_in_sector; 00254 _MEM_TYPE_FAST_ U32 u32_byte_remaining; 00255 00256 if( !fat_check_mount_select_open()) 00257 return FALSE; 00258 00259 if(!(FOPEN_READ_ACCESS & fs_g_nav_entry.u8_open_mode)) 00260 { 00261 fs_g_status = FS_ERR_WRITE_ONLY; 00262 return FALSE; 00263 } 00264 00265 u16_nb_read = 0; 00266 00267 while( 0 != u16_buf_size ) 00268 { 00269 if ( file_eof() ) 00270 { 00271 fs_g_status = FS_ERR_EOF; 00272 return u16_nb_read; // End of the file 00273 } 00274 u32_byte_remaining = fs_g_nav_entry.u32_size-fs_g_nav_entry.u32_pos_in_file; 00275 u16_pos_in_sector = fs_g_nav_entry.u32_pos_in_file % FS_512B; 00276 00277 if( (0== u16_pos_in_sector) 00278 && (FS_512B <= u32_byte_remaining) 00279 && (FS_512B <= u16_buf_size) 00280 #if __GNUC__ && __AVR32__ || __ICCAVR32__ 00281 && (Test_align((U32)buffer, sizeof(U32))) 00282 #endif 00283 ) 00284 { 00285 // The file data sector can been directly transfer from memory to buffer (don't use internal cache) 00286 if( u16_buf_size <= u32_byte_remaining) 00287 { 00288 u16_nb_read_tmp = u16_buf_size; 00289 }else{ 00290 u16_nb_read_tmp = u32_byte_remaining; 00291 } 00292 u16_nb_read_tmp = u16_nb_read_tmp / FS_512B; // read a modulo sector size 00293 00294 // Get following sector segment of file 00295 if( !fat_read_file(FS_CLUST_ACT_SEG)) 00296 { 00297 if( FS_ERR_OUT_LIST == fs_g_status ) 00298 fs_g_status = FS_ERR_EOF; // translate the error 00299 return u16_nb_read; 00300 } 00301 // Truncate the segment size found if more larger than asked size 00302 if( u16_nb_read_tmp > fs_g_seg.u32_size_or_pos ) 00303 { 00304 u16_nb_read_tmp = fs_g_seg.u32_size_or_pos; 00305 }else{ 00306 fs_g_seg.u32_size_or_pos = u16_nb_read_tmp; 00307 } 00308 00309 // Directly data tranfert from memory to buffer 00310 while( 0 != fs_g_seg.u32_size_or_pos ) 00311 { 00312 if( CTRL_GOOD != memory_2_ram( fs_g_nav.u8_lun , fs_g_seg.u32_addr, buffer)) 00313 { 00314 fs_g_status = FS_ERR_HW; 00315 return u16_nb_read; 00316 } 00317 fs_g_seg.u32_size_or_pos--; 00318 fs_g_seg.u32_addr++; 00319 buffer += FS_512B; 00320 } 00321 // Translate from sector unit to byte unit 00322 u16_nb_read_tmp *= FS_512B; 00323 } 00324 else 00325 { 00326 // The file data can't been directly transfer from memory to buffer, the internal cache must be used 00327 00328 // Tranfer data from memory to internal cache 00329 if( !fat_read_file( FS_CLUST_ACT_ONE )) 00330 { 00331 if( FS_ERR_OUT_LIST == fs_g_status ) 00332 { // Translate the error 00333 fs_g_status = FS_ERR_EOF; // End of file 00334 } 00335 return u16_nb_read; 00336 } 00337 00338 // Compute the number of data to transfer 00339 u16_nb_read_tmp = FS_512B - u16_pos_in_sector; // The number is limited at sector size 00340 if( u16_nb_read_tmp > u32_byte_remaining ) 00341 u16_nb_read_tmp = u32_byte_remaining; 00342 if( u16_nb_read_tmp > u16_buf_size ) 00343 u16_nb_read_tmp = u16_buf_size; 00344 00345 // Tranfer data from internal cache to buffer 00346 memcpy_ram2ram( buffer , &fs_g_sector[ u16_pos_in_sector ], u16_nb_read_tmp ); 00347 buffer += u16_nb_read_tmp; 00348 } 00349 // Update positions 00350 fs_g_nav_entry.u32_pos_in_file += u16_nb_read_tmp; 00351 u16_nb_read += u16_nb_read_tmp; 00352 u16_buf_size -= u16_nb_read_tmp; 00353 } 00354 return u16_nb_read; // Buffer is full 00355 }
| U16 file_getc | ( | void | ) |
This function returns the next byte of file.
EOF, in case of error or end of file
Definition at line 363 of file file.c.
Referenced by ushell_cmd_cat().
00364 { 00365 U16 u16_byte; 00366 00367 while(1) 00368 { 00369 if(!(FOPEN_READ_ACCESS & fs_g_nav_entry.u8_open_mode)) 00370 { 00371 fs_g_status = FS_ERR_WRITE_ONLY; 00372 break; 00373 } 00374 if( fs_g_nav_entry.u32_size <= fs_g_nav_entry.u32_pos_in_file ) 00375 { 00376 fs_g_status = FS_ERR_EOF; 00377 break; 00378 } 00379 00380 if( !fat_read_file( FS_CLUST_ACT_ONE )) 00381 { 00382 if( FS_ERR_OUT_LIST == fs_g_status ) 00383 { // Translate the error 00384 fs_g_status = FS_ERR_EOF; // End of file 00385 } 00386 break; 00387 } 00388 00389 u16_byte = fs_g_sector[ fs_g_nav_entry.u32_pos_in_file & FS_512B_MASK ]; 00390 fs_g_nav_entry.u32_pos_in_file++; 00391 return u16_byte; 00392 } 00393 return FS_EOF; // No data readed 00394 }
| U32 file_getpos | ( | void | ) |
This function returns the position in the file.
Definition at line 632 of file file.c.
00633 { 00634 if( !fat_check_mount_select_open() ) 00635 return 0; 00636 00637 return fs_g_nav_entry.u32_pos_in_file; 00638 }
This function changes the position in the file.
| u32_pos | number of byte to seek | |
| u8_whence | direction of seek FS_SEEK_SET , start at the beginning and foward FS_SEEK_END , start at the end of file and rewind FS_SEEK_CUR_RE, start at the current position and rewind FS_SEEK_CUR_FW, start at the current position and foward |
TRUE otherwise
Definition at line 653 of file file.c.
00654 { 00655 if( !fat_check_mount_select_open()) 00656 return FALSE; 00657 00658 switch(u8_whence) 00659 { 00660 case FS_SEEK_CUR_RE: 00661 if( fs_g_nav_entry.u32_pos_in_file < u32_pos ) 00662 { // Out of the limit 00663 fs_g_status = FS_ERR_BAD_POS; 00664 return FALSE; 00665 } 00666 // update the position 00667 fs_g_nav_entry.u32_pos_in_file -= u32_pos; 00668 break; 00669 00670 case FS_SEEK_SET: 00671 if( fs_g_nav_entry.u32_size < u32_pos ) 00672 { // Out of the limit 00673 fs_g_status = FS_ERR_BAD_POS; 00674 return FALSE; 00675 } 00676 // update the position 00677 fs_g_nav_entry.u32_pos_in_file = u32_pos; 00678 break; 00679 00680 case FS_SEEK_END: 00681 if( fs_g_nav_entry.u32_size < u32_pos ) 00682 { // Out of the limit 00683 fs_g_status = FS_ERR_BAD_POS; 00684 return FALSE; 00685 } 00686 // update the position 00687 fs_g_nav_entry.u32_pos_in_file = fs_g_nav_entry.u32_size - u32_pos; 00688 break; 00689 00690 case FS_SEEK_CUR_FW: 00691 u32_pos += fs_g_nav_entry.u32_pos_in_file; 00692 if( fs_g_nav_entry.u32_size < u32_pos ) 00693 { // Out of the limit 00694 fs_g_status = FS_ERR_BAD_POS; 00695 return FALSE; 00696 } 00697 // update the position 00698 fs_g_nav_entry.u32_pos_in_file = u32_pos; 00699 break; 00700 } 00701 return TRUE; 00702 }
| U8 file_bof | ( | void | ) |
This function checks the beginning of file.
0 the position isn't at the beginning of file
FFh error
Definition at line 711 of file file.c.
00712 { 00713 if( !fat_check_mount_select_open() ) 00714 return 0xFF; 00715 00716 return (0 == fs_g_nav_entry.u32_pos_in_file ); 00717 }
| U8 file_eof | ( | void | ) |
This function checks the end of file.
0 the position isn't at the end of file
FFh error
Definition at line 726 of file file.c.
Referenced by file_read(), file_read_buf(), and ushell_cmd_cat().
00727 { 00728 if( !fat_check_mount_select_open() ) 00729 return 0xFF; 00730 return (fs_g_nav_entry.u32_size <= fs_g_nav_entry.u32_pos_in_file ); 00731 }
| void file_flush | ( | void | ) |
This function flushs the internal cache (file datas and file information).
Definition at line 736 of file file.c.
00737 { 00738 U8 save_open_mode; 00739 save_open_mode = fs_g_nav_entry.u8_open_mode; 00740 file_close(); 00741 fs_g_nav_entry.u8_open_mode = save_open_mode; 00742 }
| void file_close | ( | void | ) |
This function closes the file.
Definition at line 747 of file file.c.
Referenced by file_flush(), nav_exit(), ushell_cmd_append_file(), ushell_cmd_cat(), ushell_cmd_perform(), and ushell_cmd_perform_alloc().
00748 { 00749 // If a file is opened, then close this one 00750 if( fat_check_mount_select_open() ) 00751 { 00752 00753 #if (FSFEATURE_WRITE == (FS_LEVEL_FEATURES & FSFEATURE_WRITE)) 00754 if( FOPEN_WRITE_ACCESS & fs_g_nav_entry.u8_open_mode ) 00755 { 00756 // Write file information 00757 if( !fat_read_dir() ) 00758 return; // error 00759 fat_write_entry_file(); 00760 fat_cache_flush(); // In case of error during writing data, flush the data before exit function 00761 } 00762 #endif // FS_LEVEL_FEATURES 00763 Fat_file_close(); 00764 } 00765 }
| _MEM_TYPE_SLOW_ U8 fs_g_sector[512] |
Use "FAT sector cache" to store a sector from a file (see file_putc(), file_getc(), file_read_buf(), file_write_buf()).
1.5.3