Collaboration diagram for USB task entry point module:
|
Modules | |
| USB software Events Management | |
| Macros to manage USB events detected under interrupt. | |
Defines | |
| #define | USB_MODE_UNDEFINED 0x00 |
| #define | USB_MODE_HOST 0x01 |
| #define | USB_MODE_DEVICE 0x02 |
Functions | |
| void | usb_task_init (void) |
| This function initializes the USB proces. | |
| void | usb_task (void) |
| Entry point of the USB mamnagement. | |
Variables | |
| volatile U16 | g_usb_event |
| Public : U16 g_usb_event usb_connected is used to store USB events detected upon USB general interrupt subroutine Its value is managed by the following macros (See usb_task.h file) Usb_send_event(x) Usb_ack_event(x) Usb_clear_all_event() Is_usb_event(x) Is_not_usb_event(x). | |
| volatile U8 | private_sof_counter |
| Private : (U8) private_sof_counter Incremented by host SOF interrupt subroutime This counter is used to detect timeout in host requests. | |
|
|
Definition at line 51 of file usb_task.h. Referenced by usb_task(), and usb_task_init(). |
|
|
Definition at line 52 of file usb_task.h. Referenced by usb_task(), and usb_task_init(). |
|
|
Definition at line 53 of file usb_task.h. Referenced by usb_task(), and usb_task_init(). |
|
|
This function initializes the USB proces. Depending on the mode supported (HOST/DEVICE/DUAL_ROLE) the function calls the coresponding usb mode initialization function
Definition at line 128 of file usb_task.c. References g_old_usb_mode, g_usb_mode, Is_usb_id_device, PORTA, Usb_ack_id_transition, usb_device_task_init(), Usb_enable_id_interrupt, Usb_enable_regulator, Usb_enable_uid_pin, Usb_force_device_mode, Usb_force_host_mode, USB_MODE_DEVICE, USB_MODE_HOST, and USB_MODE_UNDEFINED. 00129 { 00130 #if (USB_HOST_FEATURE == ENABLED) 00131 U8 delay; 00132 #endif 00133 00134 #if (USE_USB_PADS_REGULATOR==ENABLE) // Otherwise assume USB PADs regulator is not used 00135 Usb_enable_regulator(); 00136 #endif 00137 00138 // ---- DUAL ROLE DEVICE USB MODE --------------------------------------------- 00139 #if ((USB_DEVICE_FEATURE == ENABLED)&& (USB_HOST_FEATURE == ENABLED)) 00140 Usb_enable_uid_pin(); 00141 delay=PORTA; 00142 g_usb_mode=USB_MODE_UNDEFINED; 00143 if(Is_usb_id_device()) 00144 { 00145 g_usb_mode=USB_MODE_DEVICE; 00146 usb_device_task_init(); 00147 } 00148 else 00149 { 00150 g_usb_mode=USB_MODE_HOST; 00151 Usb_ack_id_transition(); // REQUIRED !!! Startup with ID=0, Ack ID pin transistion (default hwd start up is device mode) 00152 Usb_enable_id_interrupt(); 00153 Enable_interrupt(); 00154 usb_host_task_init(); 00155 } 00156 g_old_usb_mode=g_usb_mode; // Store current usb mode, for mode change detection 00157 // ----------------------------------------------------------------------------- 00158 00159 // ---- DEVICE ONLY USB MODE --------------------------------------------------- 00160 #elif ((USB_DEVICE_FEATURE == ENABLED)&& (USB_HOST_FEATURE == DISABLE)) 00161 Usb_force_device_mode(); 00162 usb_device_task_init(); 00163 // ----------------------------------------------------------------------------- 00164 00165 // ---- REDUCED HOST ONLY USB MODE --------------------------------------------- 00166 #elif ((USB_DEVICE_FEATURE == DISABLE)&& (USB_HOST_FEATURE == ENABLED)) 00167 Usb_force_host_mode(); 00168 usb_host_task_init(); 00169 #elif ((USB_DEVICE_FEATURE == DISABLE)&& (USB_HOST_FEATURE == DISABLE)) 00170 #error at least one of USB_DEVICE_FEATURE or USB_HOST_FEATURE should be enabled 00171 #endif 00172 // ----------------------------------------------------------------------------- 00173 00174 00175 }
Here is the call graph for this function: ![]() |
|
|
Entry point of the USB mamnagement. Depending on the USB mode supported (HOST/DEVICE/DUAL_ROLE) the function calls the coresponding usb management function.
Definition at line 187 of file usb_task.c. References g_old_usb_mode, g_usb_mode, Is_usb_id_device, usb_device_task(), USB_MODE_DEVICE, USB_MODE_HOST, USB_MODE_UNDEFINED, and Wdt_change_16ms. 00188 { 00189 // ---- DUAL ROLE DEVICE USB MODE --------------------------------------------- 00190 #if ((USB_DEVICE_FEATURE == ENABLED)&& (USB_HOST_FEATURE == ENABLED)) 00191 if(Is_usb_id_device()) 00192 { g_usb_mode=USB_MODE_DEVICE;} 00193 else 00194 { g_usb_mode=USB_MODE_HOST;} 00195 // TODO !!! ID pin hot state change 00196 // Preliminary management: HARDWARE RESET !!! 00197 #if ( ID_PIN_CHANGE_GENERATE_RESET == ENABLE) 00198 // Hot ID transition generates wdt reset 00199 if((g_old_usb_mode!=g_usb_mode)) 00200 {Wdt_change_16ms(); while(1);} 00201 #endif 00202 // Depending on current usb mode, launch the correct usb task (device or host) 00203 switch(g_usb_mode) 00204 { 00205 case USB_MODE_DEVICE: 00206 usb_device_task(); 00207 break; 00208 case USB_MODE_HOST: 00209 usb_host_task(); 00210 break; 00211 case USB_MODE_UNDEFINED: // No break ! 00212 default: 00213 break; 00214 } 00215 // ----------------------------------------------------------------------------- 00216 00217 // ---- DEVICE ONLY USB MODE --------------------------------------------------- 00218 #elif ((USB_DEVICE_FEATURE == ENABLED)&& (USB_HOST_FEATURE == DISABLE)) 00219 usb_device_task(); 00220 // ----------------------------------------------------------------------------- 00221 00222 // ---- REDUCED HOST ONLY USB MODE --------------------------------------------- 00223 #elif ((USB_DEVICE_FEATURE == DISABLE)&& (USB_HOST_FEATURE == ENABLED)) 00224 usb_host_task(); 00225 // ----------------------------------------------------------------------------- 00226 00228 #elif ((USB_DEVICE_FEATURE == DISABLE)&& (USB_HOST_FEATURE == DISABLE)) 00229 #error at least one of USB_DEVICE_FEATURE or USB_HOST_FEATURE should be enabled 00230 #error otherwise the usb task has nothiing to do ... 00231 #endif 00232 // ----------------------------------------------------------------------------- 00233 00234 }
Here is the call graph for this function: ![]() |
|
|
Public : U16 g_usb_event usb_connected is used to store USB events detected upon USB general interrupt subroutine Its value is managed by the following macros (See usb_task.h file) Usb_send_event(x) Usb_ack_event(x) Usb_clear_all_event() Is_usb_event(x) Is_not_usb_event(x).
Definition at line 70 of file usb_task.c. |
|
|
Private : (U8) private_sof_counter Incremented by host SOF interrupt subroutime This counter is used to detect timeout in host requests. It must not be modified by the user application tasks. / Definition at line 99 of file usb_task.c. Referenced by usb_general_interrupt(). |
1.4.6-NO