Collaboration diagram for USB device standard requests decoding module:
|
Modules | |
| Standard requests defines | |
Defines | |
| #define | ATTACHED 0 |
| #define | POWERED 1 |
| #define | DEFAULT 2 |
| #define | ADDRESSED 3 |
| #define | CONFIGURED 4 |
| #define | SUSPENDED 5 |
| #define | USB_CONFIG_ATTRIBUTES_RESERVED 0x80 |
| #define | USB_CONFIG_BUSPOWERED (USB_CONFIG_ATTRIBUTES_RESERVED | 0x00) |
| #define | USB_CONFIG_SELFPOWERED (USB_CONFIG_ATTRIBUTES_RESERVED | 0x40) |
| #define | USB_CONFIG_REMOTEWAKEUP (USB_CONFIG_ATTRIBUTES_RESERVED | 0x20) |
| #define | Is_device_enumerated() ((usb_configuration_nb!=0) ? TRUE : FALSE) |
| Returns true when device connected and correctly enumerated with an host. | |
| #define | Is_device_not_enumerated() ((usb_configuration_nb!=0) ? FALSE : TRUE) |
Functions | |
| void | usb_var_init (void) |
| void | usb_process_request (void) |
| This function reads the SETUP request sent to the default control endpoint and calls the appropriate function. | |
Variables | |
| U8 | usb_configuration_nb |
| Public : (U8) usb_configuration_nb Store the number of the USB configuration used by the USB device when its value is different from zero, it means the device mode is enumerated Used with USB_DEVICE_FEATURE == ENABLED only /. | |
|
|
Definition at line 92 of file usb_standard_request.h. |
|
|
Definition at line 93 of file usb_standard_request.h. |
|
|
Definition at line 94 of file usb_standard_request.h. |
|
|
Definition at line 95 of file usb_standard_request.h. |
|
|
Definition at line 96 of file usb_standard_request.h. |
|
|
Definition at line 97 of file usb_standard_request.h. |
|
|
Definition at line 99 of file usb_standard_request.h. |
|
|
Definition at line 100 of file usb_standard_request.h. |
|
|
Definition at line 101 of file usb_standard_request.h. |
|
|
Definition at line 102 of file usb_standard_request.h. |
|
|
Returns true when device connected and correctly enumerated with an host. The device high level application should tests this before performing any applicative requests Definition at line 108 of file usb_standard_request.h. Referenced by hid_task(). |
|
|
Definition at line 109 of file usb_standard_request.h. |
|
|
|
|
|
This function reads the SETUP request sent to the default control endpoint and calls the appropriate function.
Definition at line 119 of file usb_standard_request.c. References bmRequestType, CLEAR_FEATURE, FALSE, GET_CONFIGURATION, GET_DESCRIPTOR, GET_INTERFACE, GET_STATUS, SET_ADDRESS, SET_CONFIGURATION, SET_DESCRIPTOR, SET_FEATURE, SET_INTERFACE, SYNCH_FRAME, Usb_ack_receive_setup, usb_clear_feature(), Usb_enable_stall_handshake, usb_get_configuration(), usb_get_descriptor(), usb_get_interface(), usb_get_status(), Usb_read_byte, usb_set_address(), usb_set_configuration(), usb_set_feature(), usb_set_interface(), and usb_user_read_request(). Referenced by usb_device_task(). 00120 { 00121 U8 bmRequest; 00122 00123 bmRequestType = Usb_read_byte(); 00124 bmRequest = Usb_read_byte(); 00125 00126 switch (bmRequest) 00127 { 00128 case GET_DESCRIPTOR: 00129 if (0x80 == bmRequestType) { usb_get_descriptor(); } 00130 else { usb_user_read_request(bmRequestType, bmRequest); } 00131 break; 00132 00133 case GET_CONFIGURATION: 00134 if (0x80 == bmRequestType) { usb_get_configuration(); } 00135 else { usb_user_read_request(bmRequestType, bmRequest); } 00136 break; 00137 00138 case SET_ADDRESS: 00139 if (0x00 == bmRequestType) { usb_set_address(); } 00140 else { usb_user_read_request(bmRequestType, bmRequest); } 00141 break; 00142 00143 case SET_CONFIGURATION: 00144 if (0x00 == bmRequestType) { usb_set_configuration(); } 00145 else { usb_user_read_request(bmRequestType, bmRequest); } 00146 break; 00147 00148 case CLEAR_FEATURE: 00149 if (0x02 >= bmRequestType) { usb_clear_feature(); } 00150 else { usb_user_read_request(bmRequestType, bmRequest); } 00151 break; 00152 00153 case SET_FEATURE: 00154 if (0x02 >= bmRequestType) { usb_set_feature(); } 00155 else { usb_user_read_request(bmRequestType, bmRequest); } 00156 break; 00157 00158 case GET_STATUS: 00159 if ((0x7F < bmRequestType) & (0x82 >= bmRequestType)) 00160 { usb_get_status(); } 00161 else { usb_user_read_request(bmRequestType, bmRequest); } 00162 break; 00163 00164 case GET_INTERFACE: 00165 if (bmRequestType == 0x81) { usb_get_interface(); } 00166 else { usb_user_read_request(bmRequestType, bmRequest); } 00167 break; 00168 00169 00170 case SET_INTERFACE: 00171 if (bmRequestType == 0x01) {usb_set_interface();} 00172 break; 00173 00174 case SET_DESCRIPTOR: 00175 case SYNCH_FRAME: 00176 default: 00177 if(usb_user_read_request(bmRequestType, bmRequest) == FALSE) 00178 { 00179 Usb_enable_stall_handshake(); 00180 Usb_ack_receive_setup(); 00181 return; 00182 } 00183 break; 00184 } 00185 }
Here is the call graph for this function: ![]() |
|
|
Public : (U8) usb_configuration_nb Store the number of the USB configuration used by the USB device when its value is different from zero, it means the device mode is enumerated Used with USB_DEVICE_FEATURE == ENABLED only /.
Definition at line 70 of file usb_standard_request.c. |
1.4.6-NO