Collaboration diagram for USB device controller drivers:
|
Defines | |
| #define | Usb_initiate_remote_wake_up() (UDCON |= (1<<RMWKUP)) |
| initiates a remote wake-up | |
| #define | Usb_detach() (UDCON |= (1<<DETACH)) |
| detaches from USB bus | |
| #define | Usb_attach() (UDCON &= ~(1<<DETACH)) |
| attaches to USB bus | |
| #define | Is_usb_pending_remote_wake_up() ((UDCON & (1<<RMWKUP)) ? TRUE : FALSE) |
| test if remote wake-up still running | |
| #define | Is_usb_detached() ((UDCON & (1<<DETACH)) ? TRUE : FALSE) |
| test if the device is detached | |
| #define | Usb_get_device_interrupt() (UDINT & (1<<UDIEN)) |
| returns the USB device interrupts (interrupt enabled) | |
| #define | Usb_ack_all_device_interrupt() (UDINT = ~(1<<UDIEN)) |
| acks the USB device interrupts (interrupt enabled) | |
| #define | Usb_enable_remote_wake_up_interrupt() (UDIEN |= (1<<UPRSME)) |
| enables remote wake-up interrupt | |
| #define | Usb_disable_remote_wake_up_interrupt() (UDIEN &= ~(1<<UPRSME)) |
| disables remote wake-up interrupt | |
| #define | Is_remote_wake_up_interrupt_enabled() ((UDIEN & (1<<UPRSME)) ? TRUE : FALSE) |
| #define | Usb_ack_remote_wake_up_start() (UDINT = ~(1<<UPRSMI)) |
| acks remote wake-up | |
| #define | Is_usb_remote_wake_up_start() ((UDINT & (1<<UPRSMI)) ? TRUE : FALSE) |
| tests if remote wake-up still running | |
| #define | Usb_enable_resume_interrupt() (UDIEN |= (1<<EORSME)) |
| enables resume interrupt | |
| #define | Usb_disable_resume_interrupt() (UDIEN &= ~(1<<EORSME)) |
| disables resume interrupt | |
| #define | Is_resume_interrupt_enabled() ((UDIEN & (1<<EORSME)) ? TRUE : FALSE) |
| #define | Usb_ack_resume() (UDINT = ~(1<<EORSMI)) |
| acks resume | |
| #define | Is_usb_resume() ((UDINT & (1<<EORSMI)) ? TRUE : FALSE) |
| tests if resume occurs | |
| #define | Usb_enable_wake_up_interrupt() (UDIEN |= (1<<WAKEUPE)) |
| enables wake-up interrupt | |
| #define | Usb_disable_wake_up_interrupt() (UDIEN &= ~(1<<WAKEUPE)) |
| disables wake-up interrupt | |
| #define | Is_swake_up_interrupt_enabled() ((UDIEN & (1<<WAKEUPE)) ? TRUE : FALSE) |
| #define | Usb_ack_wake_up() (UDINT = ~(1<<WAKEUPI)) |
| acks wake-up | |
| #define | Is_usb_wake_up() ((UDINT & (1<<WAKEUPI)) ? TRUE : FALSE) |
| tests if wake-up occurs | |
| #define | Usb_enable_reset_interrupt() (UDIEN |= (1<<EORSTE)) |
| enables USB reset interrupt | |
| #define | Usb_disable_reset_interrupt() (UDIEN &= ~(1<<EORSTE)) |
| disables USB reset interrupt | |
| #define | Is_reset_interrupt_enabled() ((UDIEN & (1<<EORSTE)) ? TRUE : FALSE) |
| #define | Usb_ack_reset() (UDINT = ~(1<<EORSTI)) |
| acks USB reset | |
| #define | Is_usb_reset() ((UDINT & (1<<EORSTI)) ? TRUE : FALSE) |
| tests if USB reset occurs | |
| #define | Usb_enable_sof_interrupt() (UDIEN |= (1<<SOFE)) |
| enables Start Of Frame Interrupt | |
| #define | Usb_disable_sof_interrupt() (UDIEN &= ~(1<<SOFE)) |
| disables Start Of Frame Interrupt | |
| #define | Is_sof_interrupt_enabled() ((UDIEN & (1<<SOFE)) ? TRUE : FALSE) |
| #define | Usb_ack_sof() (UDINT = ~(1<<SOFI)) |
| acks Start Of Frame | |
| #define | Is_usb_sof() ((UDINT & (1<<SOFI)) ? TRUE : FALSE) |
| tests if Start Of Frame occurs | |
| #define | Usb_enable_suspend_interrupt() (UDIEN |= (1<<SUSPE)) |
| enables suspend state interrupt | |
| #define | Usb_disable_suspend_interrupt() (UDIEN &= ~(1<<SUSPE)) |
| disables suspend state interrupt | |
| #define | Is_suspend_interrupt_enabled() ((UDIEN & (1<<SUSPE)) ? TRUE : FALSE) |
| #define | Usb_ack_suspend() (UDINT = ~(1<<SUSPI)) |
| acks Suspend | |
| #define | Is_usb_suspend() ((UDINT & (1<<SUSPI)) ? TRUE : FALSE) |
| tests if Suspend state detected | |
| #define | Usb_enable_address() (UDADDR |= (1<<ADDEN)) |
| enables USB device address | |
| #define | Usb_disable_address() (UDADDR &= ~(1<<ADDEN)) |
| disables USB device address | |
| #define | Usb_configure_address(addr) (UDADDR = (UDADDR & (1<<ADDEN)) | ((U8)addr & MSK_UADD)) |
| sets the USB device address | |
| #define | Usb_frame_number() ((U16)((((U16)UDFNUMH) << 8) | ((U16)UDFNUML))) |
| returns the last frame number | |
| #define | Is_usb_frame_number_crc_error() ((UDMFN & (1<<FNCERR)) ? TRUE : FALSE) |
| tests if a crc error occurs in frame number | |
|
|
initiates a remote wake-up
|
|
|
detaches from USB bus
Definition at line 333 of file usb_drv.h. Referenced by hid_task(). |
|
|
attaches to USB bus
Definition at line 335 of file usb_drv.h. Referenced by usb_device_task(), usb_general_interrupt(), and usb_start_device(). |
|
|
test if remote wake-up still running
|
|
|
test if the device is detached
|
|
|
returns the USB device interrupts (interrupt enabled)
|
|
|
acks the USB device interrupts (interrupt enabled)
|
|
|
enables remote wake-up interrupt
|
|
|
disables remote wake-up interrupt
|
|
|
|
|
|
acks remote wake-up
|
|
|
tests if remote wake-up still running
|
|
|
enables resume interrupt
|
|
|
disables resume interrupt
Definition at line 359 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
Definition at line 360 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
acks resume
Definition at line 362 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
tests if resume occurs
Definition at line 364 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
enables wake-up interrupt
Definition at line 367 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
disables wake-up interrupt
Definition at line 369 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
Definition at line 370 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
acks wake-up
Definition at line 372 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
tests if wake-up occurs
Definition at line 374 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
enables USB reset interrupt
Definition at line 377 of file usb_drv.h. Referenced by usb_device_task(), usb_general_interrupt(), and usb_start_device(). |
|
|
disables USB reset interrupt
|
|
|
Definition at line 380 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
acks USB reset
Definition at line 382 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
tests if USB reset occurs
Definition at line 384 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
enables Start Of Frame Interrupt
|
|
|
disables Start Of Frame Interrupt
|
|
|
Definition at line 390 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
acks Start Of Frame
Definition at line 392 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
tests if Start Of Frame occurs
Definition at line 394 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
enables suspend state interrupt
Definition at line 397 of file usb_drv.h. Referenced by usb_start_device(). |
|
|
disables suspend state interrupt
|
|
|
Definition at line 400 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
acks Suspend
Definition at line 402 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
tests if Suspend state detected
Definition at line 404 of file usb_drv.h. Referenced by usb_general_interrupt(). |
|
|
enables USB device address
Definition at line 407 of file usb_drv.h. Referenced by usb_set_address(). |
|
|
disables USB device address
|
|
|
sets the USB device address
Definition at line 411 of file usb_drv.h. Referenced by usb_set_address(). |
|
|
returns the last frame number
|
|
|
tests if a crc error occurs in frame number
|
1.4.6-NO