This graph shows which files directly or indirectly include this file:

Go to the source code of this file.
Defines | |
| #define | USB_HOST_FEATURE DISABLED |
| ENABLE to activate the host software library support. | |
| #define | USB_DEVICE_FEATURE ENABLED |
| ENABLE to activate the device software library support. | |
| #define | USE_USB_PADS_REGULATOR ENABLE |
| Enable the internal regulator for USB pads. | |
| #define | HID_CLASS 0x03 |
| #define | MS_CLASS 0x08 |
| #define | VID_PID_TABLE |
| VID/PID supported table list. | |
| #define | CLASS_SUBCLASS_PROTOCOL |
| CLASS/SUBCLASS_PROTOCOL supported table list. | |
| #define | SIZEOF_DATA_STAGE 250 |
| The size of RAM buffer reserved of descriptors manipulation. | |
| #define | DEVICE_ADDRESS 0x05 |
| The address that will be assigned to the connected device. | |
| #define | HOST_STRICT_VID_PID_TABLE DISABLE |
| The host controller will be limited to the strict VID/PID list. | |
| #define | HOST_AUTO_CFG_ENDPOINT ENABLE |
| Try to configure the host pipe according to the device descriptors received. | |
| #define | HOST_CONTINUOUS_SOF_INTERRUPT DISABLE |
| Host start of frame interrupt always enable. | |
| #define | HOST_ERROR_RESTART ENABLE |
| When Host error state detected, goto unattached state. | |
| #define | ID_PIN_CHANGE_GENERATE_RESET DISABLE |
| Force WDT reset upon ID pin change. | |
| #define | NAK_TIMEOUT_DELAY 1 |
| NAK handshake in 1/4sec (250ms) before timeout. | |
| #define | User_configure_endpoint() |
| If no auto configuration of EP, map here user function. | |
| #define | Usb_id_transition_action() |
| #define | Host_device_disconnection_action() |
| #define | Host_device_connection_action() |
| #define | Host_sof_action() |
| #define | Host_suspend_action() host_suspend_action(); |
| #define | Host_hwup_action() |
| #define | Host_device_not_supported_action() |
| #define | Host_device_supported_action() |
| #define | Host_device_error_action() |
| #define | Usb_unicode(a) ((U16)(a)) |
| #define | NB_ENDPOINTS 2 |
| #define | EP_HID_IN 1 |
| #define | EP_HID_OUT 2 |
| #define | Usb_sof_action() sof_action(); |
| #define | Usb_wake_up_action() |
| #define | Usb_resume_action() |
| #define | Usb_suspend_action() |
| #define | Usb_reset_action() |
| #define | Usb_vbus_on_action() |
| #define | Usb_vbus_off_action() |
| #define | Usb_set_configuration_action() |
Functions | |
| void | host_suspend_action (void) |
| void | sof_action (void) |
| sof_action | |
Copyright (c) 2006 Atmel.
Please read file license.txt for copyright notice.
This file contains the possible external configuration of the USB
Definition in file conf_usb.h.
1.4.6-NO