Microcontroller Wireless Solutions


nwk_msg_code.h File Reference

This file defines all message constants. More...

Go to the source code of this file.

Defines

#define NLDE_DATA_REQ_LEN
#define NLME_AUTO_DISCOVERY_REQ_LEN
#define NLME_DISCOVERY_REQ_LEN
#define NLME_DISCOVERY_RESP_LEN
#define NLME_PAIR_REQ_LEN
#define NLME_PAIR_RESP_LEN
#define NLME_RESET_REQ_LEN
#define NLME_GET_REQ_LEN
#define NLME_RX_ENABLE_REQ_LEN
#define NLME_SET_REQ_LEN
#define NLME_START_REQ
#define NLME_UNPAIR_REQ_LEN
#define NLME_UNPAIR_RESP_LEN
#define NLME_UPDATE_KEY_REQ_LEN
#define NWK_CH_AGILITY_REQ_LEN
#define MAC_DATA_IND_LEN
#define NLDE_DATA_IND_LEN   8
#define NLDE_DATA_CONF_LEN   4
#define NLME_AUTO_DISCOVERY_CONF_LEN   10
#define NLME_COMM_STATUS_IND_LEN   14
#define NLME_DISCOVERY_IND_LEN   48
#define NLME_DISCOVERY_CONF_LEN   4
#define NLME_GET_CONF_LEN   5
#define NLME_PAIR_IND_LEN   50
#define NLME_PAIR_CONF_LEN   38
#define NLME_RESET_CONF_LEN   2
#define NLME_RX_ENABLE_CONF_LEN   2
#define NLME_SET_CONF_LEN   4
#define NLME_START_CONF_LEN   2
#define NLME_UNPAIR_IND_LEN   2
#define NLME_UNPAIR_CONF_LEN   3
#define NLME_UPDATE_KEY_CONF_LEN   3
#define NWK_CH_AGILITY_IND_LEN   2
#define NWK_CH_AGILITY_CONF_LEN   4
#define UNSUPPORTED_CMD_LEN   1

Typedefs

typedef enum nwk_msg_code_tag nwk_msg_code_t

Enumerations

enum  nwk_msg_code_tag {
  NLDE_DATA_REQUEST = 0x24,
  NLME_AUTO_DISCOVERY_REQUEST = 0x25,
  NLME_DISCOVERY_REQUEST = 0x26,
  NLME_DISCOVERY_RESPONSE = 0x27,
  NLME_PAIR_REQUEST = 0x28,
  NLME_PAIR_RESPONSE = 0x29,
  NLME_RESET_REQUEST = 0x2A,
  NLME_GET_REQUEST = 0x2B,
  NLME_RX_ENABLE_REQUEST = 0x2C,
  NLME_SET_REQUEST = 0x2D,
  NLME_START_REQUEST = 0x2E,
  NLME_UNPAIR_REQUEST = 0x2F,
  NLME_UNPAIR_RESPONSE = 0x30,
  NLME_UPDATE_KEY_REQUEST = 0x31,
  NWK_CH_AGILITY_REQUEST = 0x32,
  MAC_DATA_INDICATION = 0x33,
  NLDE_DATA_INDICATION = 0x34,
  NLDE_DATA_CONFIRM = 0x35,
  NLME_AUTO_DISCOVERY_CONFIRM = 0x36,
  NLME_COMM_STATUS_INDICATION = 0x37,
  NLME_DISCOVERY_INDICATION = 0x38,
  NLME_DISCOVERY_CONFIRM = 0x39,
  NLME_GET_CONFIRM = 0x3A,
  NLME_PAIR_INDICATION = 0x3B,
  NLME_PAIR_CONFIRM = 0x3C,
  NLME_RESET_CONFIRM = 0x3D,
  NLME_RX_ENABLE_CONFIRM = 0x3E,
  NLME_SET_CONFIRM = 0x3F,
  NLME_START_CONFIRM = 0x40,
  NLME_UNPAIR_INDICATION = 0x41,
  NLME_UNPAIR_CONFIRM = 0x42,
  NLME_UPDATE_KEY_CONFIRM = 0x43,
  NWK_CH_AGILITY_INDICATION = 0x44,
  NWK_CH_AGILITY_CONFIRM = 0x45
}

Detailed Description

This file defines all message constants.

Id:
nwk_msg_code.h 32147 2012-05-24 09:53:50Z agasthian.s
Author:
Atmel Corporation: http://www.atmel.com
Support email: avr@atmel.com

Definition in file nwk_msg_code.h.


Define Documentation

#define MAC_DATA_IND_LEN

Definition at line 122 of file nwk_msg_code.h.

#define NLDE_DATA_CONF_LEN   4

Definition at line 125 of file nwk_msg_code.h.

#define NLDE_DATA_IND_LEN   8

Definition at line 124 of file nwk_msg_code.h.

#define NLDE_DATA_REQ_LEN

The following defines describe the minimum length of a primitive message.

Definition at line 106 of file nwk_msg_code.h.

#define NLME_AUTO_DISCOVERY_CONF_LEN   10

Definition at line 126 of file nwk_msg_code.h.

#define NLME_AUTO_DISCOVERY_REQ_LEN

Definition at line 107 of file nwk_msg_code.h.

#define NLME_COMM_STATUS_IND_LEN   14

Definition at line 127 of file nwk_msg_code.h.

#define NLME_DISCOVERY_CONF_LEN   4

Definition at line 129 of file nwk_msg_code.h.

#define NLME_DISCOVERY_IND_LEN   48

Definition at line 128 of file nwk_msg_code.h.

#define NLME_DISCOVERY_REQ_LEN

Definition at line 108 of file nwk_msg_code.h.

#define NLME_DISCOVERY_RESP_LEN

Definition at line 109 of file nwk_msg_code.h.

#define NLME_GET_CONF_LEN   5

Definition at line 130 of file nwk_msg_code.h.

#define NLME_GET_REQ_LEN

Definition at line 113 of file nwk_msg_code.h.

#define NLME_PAIR_CONF_LEN   38

Definition at line 132 of file nwk_msg_code.h.

#define NLME_PAIR_IND_LEN   50

Definition at line 131 of file nwk_msg_code.h.

#define NLME_PAIR_REQ_LEN

Definition at line 110 of file nwk_msg_code.h.

#define NLME_PAIR_RESP_LEN

Definition at line 111 of file nwk_msg_code.h.

#define NLME_RESET_CONF_LEN   2

Definition at line 133 of file nwk_msg_code.h.

#define NLME_RESET_REQ_LEN

Definition at line 112 of file nwk_msg_code.h.

#define NLME_RX_ENABLE_CONF_LEN   2

Definition at line 134 of file nwk_msg_code.h.

#define NLME_RX_ENABLE_REQ_LEN

Definition at line 114 of file nwk_msg_code.h.

#define NLME_SET_CONF_LEN   4

Definition at line 135 of file nwk_msg_code.h.

#define NLME_SET_REQ_LEN

Definition at line 115 of file nwk_msg_code.h.

#define NLME_START_CONF_LEN   2

Definition at line 136 of file nwk_msg_code.h.

#define NLME_START_REQ

Definition at line 116 of file nwk_msg_code.h.

#define NLME_UNPAIR_CONF_LEN   3

Definition at line 138 of file nwk_msg_code.h.

#define NLME_UNPAIR_IND_LEN   2

Definition at line 137 of file nwk_msg_code.h.

#define NLME_UNPAIR_REQ_LEN

Definition at line 117 of file nwk_msg_code.h.

#define NLME_UNPAIR_RESP_LEN

Definition at line 118 of file nwk_msg_code.h.

#define NLME_UPDATE_KEY_CONF_LEN   3

Definition at line 139 of file nwk_msg_code.h.

#define NLME_UPDATE_KEY_REQ_LEN

Definition at line 119 of file nwk_msg_code.h.

#define NWK_CH_AGILITY_CONF_LEN   4

Definition at line 141 of file nwk_msg_code.h.

#define NWK_CH_AGILITY_IND_LEN   2

Definition at line 140 of file nwk_msg_code.h.

#define NWK_CH_AGILITY_REQ_LEN

Definition at line 120 of file nwk_msg_code.h.


Typedef Documentation

This type contains the service primitives of the Network-layer as well the command-interface primitives

DO NOT CHANGE ORDER OF ENUM!


Enumeration Type Documentation

This type contains the service primitives of the Network-layer as well the command-interface primitives

DO NOT CHANGE ORDER OF ENUM!

Enumerator:
NLDE_DATA_REQUEST 
NLME_AUTO_DISCOVERY_REQUEST 
NLME_DISCOVERY_REQUEST 
NLME_DISCOVERY_RESPONSE 
NLME_PAIR_REQUEST 
NLME_PAIR_RESPONSE 
NLME_RESET_REQUEST 
NLME_GET_REQUEST 
NLME_RX_ENABLE_REQUEST 
NLME_SET_REQUEST 
NLME_START_REQUEST 
NLME_UNPAIR_REQUEST 
NLME_UNPAIR_RESPONSE 
NLME_UPDATE_KEY_REQUEST 
NWK_CH_AGILITY_REQUEST 
MAC_DATA_INDICATION 
NLDE_DATA_INDICATION 
NLDE_DATA_CONFIRM 
NLME_AUTO_DISCOVERY_CONFIRM 
NLME_COMM_STATUS_INDICATION 
NLME_DISCOVERY_INDICATION 
NLME_DISCOVERY_CONFIRM 
NLME_GET_CONFIRM 
NLME_PAIR_INDICATION 
NLME_PAIR_CONFIRM 
NLME_RESET_CONFIRM 
NLME_RX_ENABLE_CONFIRM 
NLME_SET_CONFIRM 
NLME_START_CONFIRM 
NLME_UNPAIR_INDICATION 
NLME_UNPAIR_CONFIRM 
NLME_UPDATE_KEY_CONFIRM 
NWK_CH_AGILITY_INDICATION 
NWK_CH_AGILITY_CONFIRM 

Definition at line 34 of file nwk_msg_code.h.