usb_device_qualifier_descriptor Struct Reference
[USB Protocol Definitions]

Standard USB device qualifier descriptor. More...

#include <usb_protocol.h>


Detailed Description

Standard USB device qualifier descriptor.

This descriptor contains information about the device when running at the "other" speed (i.e. if the device is currently operating at high speed, this descriptor can be used to determine what would change if the device was operating at full speed.)

Definition at line 286 of file usb_protocol.h.


The documentation for this struct was generated from the following file:
Generated on Thu Apr 29 14:10:36 2010 for xplain-bc by  doxygen 1.6.3