scsi_mode_param_header6 Struct Reference

SCSI Mode Parameter Header used by MODE SELECT(6) and MODE SENSE(6). More...

#include <spc_protocol.h>

Data Fields

uint8_t mode_data_length
 Number of bytes after this.
uint8_t medium_type
 Medium Type.
uint8_t device_specific_parameter
 Defined by command set.
uint8_t block_descriptor_length
 Length of block descriptors.

Detailed Description

SCSI Mode Parameter Header used by MODE SELECT(6) and MODE SENSE(6).

Definition at line 213 of file spc_protocol.h.


Field Documentation

Length of block descriptors.

Definition at line 217 of file spc_protocol.h.

Defined by command set.

Definition at line 216 of file spc_protocol.h.

Medium Type.

Definition at line 215 of file spc_protocol.h.

Number of bytes after this.

Definition at line 214 of file spc_protocol.h.


The documentation for this struct was generated from the following file:
Generated on Thu Apr 29 14:10:36 2010 for xplain-bc by  doxygen 1.6.3