include/status_codes.h File Reference

Status code definitions. More...

Go to the source code of this file.

Enumerations

enum  status_code {
  STATUS_OK = 0, ERR_IO_ERROR = -1, ERR_FLUSHED = -2, ERR_TIMEOUT = -3,
  ERR_BAD_DATA = -4, ERR_PROTOCOL = -5, ERR_UNSUPPORTED_DEV = -6, ERR_NO_MEMORY = -7,
  ERR_INVALID_ARG = -8, ERR_BAD_ADDRESS = -9, ERR_BUSY = -10, ERR_BAD_FORMAT = -11,
  OPERATION_IN_PROGRESS = -128
}

Detailed Description

Status code definitions.

This file defines various status codes returned by functions, indicating success or failure as well as what kind of failure.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

Definition in file status_codes.h.


Enumeration Type Documentation

Status code that may be returned by shell commands and protocol implementations.

Note:
Any change to these status codes and the corresponding message strings is strictly forbidden. New codes can be added, however, but make sure that any message string tables are updated at the same time.
Enumerator:
STATUS_OK 

Success.

ERR_IO_ERROR 

I/O error.

ERR_FLUSHED 

Request flushed from queue.

ERR_TIMEOUT 

Operation timed out.

ERR_BAD_DATA 

Data integrity check failed.

ERR_PROTOCOL 

Protocol error.

ERR_UNSUPPORTED_DEV 

Unsupported device.

ERR_NO_MEMORY 

Insufficient memory.

ERR_INVALID_ARG 

Invalid argument.

ERR_BAD_ADDRESS 

Bad address.

ERR_BUSY 

Resource is busy.

ERR_BAD_FORMAT 

Data format not recognized.

OPERATION_IN_PROGRESS 

Operation in progress.

This status code is for driver-internal use when an operation is currently being performed.

Note:
Drivers should never return this status code to any callers. It is strictly for internal use.

Definition at line 53 of file status_codes.h.

Generated on Thu Apr 29 14:10:34 2010 for xplain-bc by  doxygen 1.6.3