include/scsi/spc_protocol.h File Reference

SCSI Primary Commands. More...

Go to the source code of this file.

Data Structures

struct  scsi_inquiry_data
 SCSI Standard Inquiry data structure. More...
struct  scsi_mode_param_header6
 SCSI Mode Parameter Header used by MODE SELECT(6) and MODE SENSE(6). More...
struct  scsi_mode_param_header10
 SCSI Mode Parameter Header used by MODE SELECT(10) and MODE SENSE(10). More...
struct  scsi_mode_page_0_header
 SCSI Page_0 Mode Page header (SPF not set). More...

Defines

#define SCSI_INQ_REQ_EVPD   0x01
 Enable Vital Product Data.
#define SCSI_INQ_PQ_CONNECTED   0x00
 Peripheral connected.
#define SCSI_INQ_PQ_NOT_CONN   0x20
 Peripheral not connected.
#define SCSI_INQ_PQ_NOT_SUPP   0x60
 Peripheral not supported.
#define SCSI_INQ_DT_DIR_ACCESS   0x00
 Direct Access (SBC).
#define SCSI_INQ_DT_SEQ_ACCESS   0x01
 Sequential Access.
#define SCSI_INQ_DT_PRINTER   0x02
 Printer.
#define SCSI_INQ_DT_PROCESSOR   0x03
 Processor device.
#define SCSI_INQ_DT_WRITE_ONCE   0x04
 Write-once device.
#define SCSI_INQ_DT_CD_DVD   0x05
 CD/DVD device.
#define SCSI_INQ_DT_OPTICAL   0x07
 Optical Memory.
#define SCSI_INQ_DT_MC   0x08
 Medium Changer.
#define SCSI_INQ_DT_ARRAY   0x0c
 Storage Array Controller.
#define SCSI_INQ_DT_ENCLOSURE   0x0d
 Enclosure Services.
#define SCSI_INQ_DT_RBC   0x0e
 Simplified Direct Access.
#define SCSI_INQ_DT_OCRW   0x0f
 Optical card reader/writer.
#define SCSI_INQ_DT_BCC   0x10
 Bridge Controller Commands.
#define SCSI_INQ_DT_OSD   0x11
 Object-based Storage.
#define SCSI_INQ_DT_NONE   0x1f
 No Peripheral.
#define SCSI_INQ_RMB   0x80
 Removable Medium.
#define SCSI_INQ_VER_NONE   0x00
 No standards conformance.
#define SCSI_INQ_VER_SPC   0x03
 SCSI Primary Commands.
#define SCSI_INQ_VER_SPC2   0x04
 SCSI Primary Commands - 2.
#define SCSI_INQ_VER_SPC3   0x05
 SCSI Primary Commands - 3.
#define SCSI_INQ_VER_SPC4   0x06
 SCSI Primary Commands - 4.
#define SCSI_INQ_NORMACA   0x20
 Normal ACA Supported.
#define SCSI_INQ_HISUP   0x10
 Hierarchial LUN addressing.
#define SCSI_INQ_RSP_SPC2   0x02
 SPC-2 / SPC-3 response format.
#define SCSI_INQ_ADDL_LEN(tot)   ((tot) - 5)
 Total length is tot.
#define SCSI_PAGE_CODE_PS   (1 << 7)
 Parameters Saveable.
#define SCSI_PAGE_CODE_SPF   (1 << 6)
 SubPage Format.

Detailed Description

SCSI Primary Commands.

This file contains definitions of some of the commands found in the SPC-2 standard.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

Definition in file spc_protocol.h.


Define Documentation

#define SCSI_INQ_ADDL_LEN ( tot   )     ((tot) - 5)

Total length is tot.

Definition at line 95 of file spc_protocol.h.

#define SCSI_INQ_DT_ARRAY   0x0c

Storage Array Controller.

Definition at line 75 of file spc_protocol.h.

#define SCSI_INQ_DT_BCC   0x10

Bridge Controller Commands.

Definition at line 79 of file spc_protocol.h.

#define SCSI_INQ_DT_CD_DVD   0x05

CD/DVD device.

Definition at line 72 of file spc_protocol.h.

#define SCSI_INQ_DT_DIR_ACCESS   0x00

Direct Access (SBC).

Definition at line 67 of file spc_protocol.h.

#define SCSI_INQ_DT_ENCLOSURE   0x0d

Enclosure Services.

Definition at line 76 of file spc_protocol.h.

#define SCSI_INQ_DT_MC   0x08

Medium Changer.

Definition at line 74 of file spc_protocol.h.

#define SCSI_INQ_DT_NONE   0x1f

No Peripheral.

Definition at line 81 of file spc_protocol.h.

#define SCSI_INQ_DT_OCRW   0x0f

Optical card reader/writer.

Definition at line 78 of file spc_protocol.h.

#define SCSI_INQ_DT_OPTICAL   0x07

Optical Memory.

Definition at line 73 of file spc_protocol.h.

#define SCSI_INQ_DT_OSD   0x11

Object-based Storage.

Definition at line 80 of file spc_protocol.h.

#define SCSI_INQ_DT_PRINTER   0x02

Printer.

Definition at line 69 of file spc_protocol.h.

#define SCSI_INQ_DT_PROCESSOR   0x03

Processor device.

Definition at line 70 of file spc_protocol.h.

#define SCSI_INQ_DT_RBC   0x0e

Simplified Direct Access.

Definition at line 77 of file spc_protocol.h.

#define SCSI_INQ_DT_SEQ_ACCESS   0x01

Sequential Access.

Definition at line 68 of file spc_protocol.h.

#define SCSI_INQ_DT_WRITE_ONCE   0x04

Write-once device.

Definition at line 71 of file spc_protocol.h.

#define SCSI_INQ_HISUP   0x10

Hierarchial LUN addressing.

Definition at line 92 of file spc_protocol.h.

#define SCSI_INQ_NORMACA   0x20

Normal ACA Supported.

Definition at line 91 of file spc_protocol.h.

#define SCSI_INQ_PQ_CONNECTED   0x00

Peripheral connected.

Definition at line 64 of file spc_protocol.h.

#define SCSI_INQ_PQ_NOT_CONN   0x20

Peripheral not connected.

Definition at line 65 of file spc_protocol.h.

#define SCSI_INQ_PQ_NOT_SUPP   0x60

Peripheral not supported.

Definition at line 66 of file spc_protocol.h.

#define SCSI_INQ_REQ_EVPD   0x01

Enable Vital Product Data.

Definition at line 55 of file spc_protocol.h.

#define SCSI_INQ_RMB   0x80

Removable Medium.

Definition at line 83 of file spc_protocol.h.

#define SCSI_INQ_RSP_SPC2   0x02

SPC-2 / SPC-3 response format.

Definition at line 93 of file spc_protocol.h.

#define SCSI_INQ_VER_NONE   0x00

No standards conformance.

Definition at line 85 of file spc_protocol.h.

#define SCSI_INQ_VER_SPC   0x03

SCSI Primary Commands.

Definition at line 86 of file spc_protocol.h.

#define SCSI_INQ_VER_SPC2   0x04

SCSI Primary Commands - 2.

Definition at line 87 of file spc_protocol.h.

#define SCSI_INQ_VER_SPC3   0x05

SCSI Primary Commands - 3.

Definition at line 88 of file spc_protocol.h.

#define SCSI_INQ_VER_SPC4   0x06

SCSI Primary Commands - 4.

Definition at line 89 of file spc_protocol.h.

#define SCSI_PAGE_CODE_PS   (1 << 7)

Parameters Saveable.

Definition at line 238 of file spc_protocol.h.

#define SCSI_PAGE_CODE_SPF   (1 << 6)

SubPage Format.

Definition at line 239 of file spc_protocol.h.

Generated on Thu Apr 29 14:10:34 2010 for xplain-bc by  doxygen 1.6.3