Physical memory allocator implementation. More...
#include <physmem.h>#include <util.h>Go to the source code of this file.
Functions | |
| phys_addr_t | physmem_alloc (struct physmem_pool *pool, phys_size_t size, unsigned int align_order) |
| Allocate a region of physical memory. | |
| phys_addr_t | physmem_alloc_low (struct physmem_pool *pool, phys_size_t size, unsigned int align_order) |
| Allocate a low region of physical memory. | |
Physical memory allocator implementation.
This physical memory allocator implemention only supports allocating physical memory, not freeing it. This makes the allocator very lightweight, while still useful for initializing other allocators, and for expanding the malloc() pool.
Copyright (C) 2009 Atmel Corporation. All rights reserved.
Definition in file physmem.c.
| phys_addr_t physmem_alloc | ( | struct physmem_pool * | pool, | |
| phys_size_t | size, | |||
| unsigned int | align_order | |||
| ) |
Allocate a region of physical memory.
This function tries to allocate a block of physical memory from the given pool, at the highest possible address.
The following pools must be available on any CPU with internal SRAM (though they may refer to the same pool):
| pool | The physical memory pool to allocate from. | |
| size | The number of bytes to allocate. | |
| align_order | log2 of required alignment. |
Definition at line 66 of file physmem.c.
References physmem_pool::addr, PHYSMEM_ALLOC_ERR, and round_down.
Referenced by dma_pool_init_coherent_physmem().
| phys_addr_t physmem_alloc_low | ( | struct physmem_pool * | pool, | |
| phys_size_t | size, | |||
| unsigned int | align_order | |||
| ) |
Allocate a low region of physical memory.
This function tries to allocate a block of physical memory from the given pool, at the highest possible address.
| pool | The physical memory pool to allocate from. | |
| size | The number of bytes to allocate. | |
| align_order | log2 of required alignment. |
Definition at line 98 of file physmem.c.
References physmem_pool::addr, PHYSMEM_ALLOC_ERR, and round_up.
Referenced by malloc().
1.6.3