Generic SPI polled internals
[Serial Peripheral Interface (SPI)]

Collaboration diagram for Generic SPI polled internals:

Data Structures

struct  spi_master_polled
 Polled SPI master defintion. More...
struct  spi_device
 Polled SPI device defintion. More...

Modules

 Common ATmega and ATxmega SPI internals

Typedefs

typedef void(* spi_start_func_t )(struct spi_master *spim, uint8_t tx_byte)
 SPI start transfer function.

Enumerations

enum  spi_polled_op_flags { SPI_OP_WRITE, SPI_OP_READ, SPI_OP_BUFFER }
 

Flags for SPI polled operation.

More...

Functions

void spi_polled_start (struct spi_master *spim, uint8_t tx_byte, size_t residue)
 Start polled SPI transfer.
void spi_polled_write (struct spi_master *spim, const uint8_t *data, size_t len)
void spi_polled_read (struct spi_master *spim, uint8_t *data, size_t len)
void spi_polled_exchange (struct spi_master *spim, const uint8_t *write, uint8_t *read, size_t len)
void spi_polled_master_init (struct spi_master *spim, workqueue_func_t poll, spi_start_func_t start)
 Initialize polled SPI master struct.
void spi_polled_next_buffer (struct workqueue_task *task)
 Iterate to next buffer in SPI buffer list operation.
void spi_polled_write_buf_list (struct spi_master *spim, struct slist *buf_list)
void spi_polled_read_buf_list (struct spi_master *spim, struct slist *buf_list)
void spi_polled_exchange_buf_list (struct spi_master *spim, struct slist *write_buf_list, struct slist *read_buf_list)
static struct spi_master_polledspi_master_polled_of (struct spi_master *base)
 Return SPI master polled from SPI master.
static bool spi_polled_is_buffer_op (struct spi_master *spim)
 Test if polled SPI operation is using buffer list.
static void spi_polled_sched_poll (struct spi_master *spim)
 Schedule SPI poll operation.
static void spi_polled_sched_next_buffer (struct spi_master *spim)
 Schedule buffer list handling.
static void spi_polled_buf_list_init (struct spi_master *spim)
 Initialize polled SPI master.

Typedef Documentation

typedef void(* spi_start_func_t)(struct spi_master *spim, uint8_t tx_byte)

SPI start transfer function.

Parameters:
spim SPI master struct
tx_byte First byte to be written

Definition at line 64 of file spi_polled.h.


Enumeration Type Documentation

Flags for SPI polled operation.

Enumerator:
SPI_OP_WRITE 

Write operation.

SPI_OP_READ 

Read operation.

SPI_OP_BUFFER 

buffer list operation

Definition at line 52 of file spi_polled.h.


Function Documentation

static struct spi_master_polled* spi_master_polled_of ( struct spi_master base  )  [static, read]

Return SPI master polled from SPI master.

Parameters:
base SPI master struct
Returns:
SPI master polled struct

Definition at line 106 of file spi_polled.h.

References container_of.

Referenced by spi_polled_buf_list_init(), spi_polled_is_buffer_op(), spi_polled_sched_next_buffer(), and spi_polled_sched_poll().

static void spi_polled_buf_list_init ( struct spi_master spim  )  [inline, static]

Initialize polled SPI master.

Parameters:
spim SPI master struct

Definition at line 184 of file spi_polled.h.

References spi_master_polled_of(), spi_polled_next_buffer(), and workqueue_task_init().

void spi_polled_exchange ( struct spi_master spim,
const uint8_t write,
uint8_t read,
size_t  len 
)

For internal use only.

See also:
spi_exchange

Referenced by spi_exchange().

void spi_polled_exchange_buf_list ( struct spi_master spim,
struct slist write_buf_list,
struct slist read_buf_list 
)

For internal use only.

See also:
spi_exchange_buf_list

Referenced by spi_exchange_buf_list().

static bool spi_polled_is_buffer_op ( struct spi_master spim  )  [inline, static]

Test if polled SPI operation is using buffer list.

Parameters:
spim SPI master struct
Return values:
true Operation is buffer based
false Operation is not buffer based

Definition at line 123 of file spi_polled.h.

References spi_master_polled::op, spi_master_polled_of(), SPI_OP_BUFFER, and test_bit.

Referenced by spi_poll().

void spi_polled_master_init ( struct spi_master spim,
workqueue_func_t  poll,
spi_start_func_t  start 
)

Initialize polled SPI master struct.

Parameters:
spim SPI master struct
poll Poll function
start Start function
void spi_polled_next_buffer ( struct workqueue_task task  ) 

Iterate to next buffer in SPI buffer list operation.

Parameters:
task Task struct

Referenced by spi_polled_buf_list_init().

void spi_polled_read ( struct spi_master spim,
uint8_t data,
size_t  len 
)

For internal use only.

See also:
spi_read

Referenced by spi_read().

void spi_polled_read_buf_list ( struct spi_master spim,
struct slist buf_list 
)

For internal use only.

See also:
spi_read_buf_list

Referenced by spi_read_buf_list().

static void spi_polled_sched_next_buffer ( struct spi_master spim  )  [inline, static]

Schedule buffer list handling.

Parameters:
spim SPI master struct

Definition at line 153 of file spi_polled.h.

References main_workqueue, spi_master_polled_of(), and workqueue_add_task().

Referenced by spi_poll().

static void spi_polled_sched_poll ( struct spi_master spim  )  [inline, static]

Schedule SPI poll operation.

Parameters:
spim SPI master struct

Definition at line 139 of file spi_polled.h.

References main_workqueue, spi_master_polled::poll, spi_master_polled_of(), and workqueue_add_task().

Referenced by spi_poll().

void spi_polled_start ( struct spi_master spim,
uint8_t  tx_byte,
size_t  residue 
)

Start polled SPI transfer.

Parameters:
spim SPI master struct
tx_byte Initial byte to send
residue Length of remaining bytes
void spi_polled_write ( struct spi_master spim,
const uint8_t data,
size_t  len 
)

For internal use only.

See also:
spi_write

Referenced by spi_write().

void spi_polled_write_buf_list ( struct spi_master spim,
struct slist buf_list 
)

For internal use only.

See also:
spi_write_buf_list

Referenced by spi_write_buf_list().

Generated on Thu Apr 29 14:10:35 2010 for xplain-bc by  doxygen 1.6.3