chip/at90usb1287/include/chip/gpio.h File Reference

GPIO chip specific implementation. More...

#include <types.h>
#include <chip/regs.h>
#include <gpio/gpio_mega.h>

Go to the source code of this file.

Enumerations

enum  port_t
 

Ports on AT90USB1287.

More...

Detailed Description

GPIO chip specific implementation.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

Definition in file gpio.h.


Enumeration Type Documentation

enum port_t

Ports on AT90USB1287.

This device has 6 ports. Each port has a port number according to the representing letter. The first port A starts with number 0. Port B is 1, ... The numbering is continuous, that means even if a port is not available in the datasheet it is included in the port numbering.

Definition at line 48 of file gpio.h.

Generated on Thu Apr 29 14:10:34 2010 for xplain-bc by  doxygen 1.6.3