include/assembler/iar.h File Reference

Assembler abstraction layer: IAR Assembler specifics. More...

#include <arch/assembler-iar.h>

Go to the source code of this file.

Defines

Control Statements

#define REPEAT(count)   REPT count
 Repeat the following statements count times.
#define END_REPEAT()   ENDR
 Mark the end of the statements to be repeated.
#define SET_LOC(offset)   ORG offset
 Set the location counter to offset.
#define END_FILE()   END
 Mark the end of the file.
Data Objects

#define FILL_BYTES(count)   DS8 count
 Allocate space for count bytes.
Symbol Definition

#define L(name)   name
 Turn name into a local symbol, if possible.
#define EXTERN_SYMBOL(name)   EXTERN name
 Declare name as an external symbol referenced by this file.
#define FUNCTION(name)   iar_begin_func name, text_##name, 0, 0
 Define a file-local function called name.
#define PUBLIC_FUNCTION(name)   iar_begin_func name, text_##name, 1, 0
 Define a globally visible function called name.
#define WEAK_FUNCTION(name)   iar_begin_func name, text_##name, 1, 1
 Define a weak function called name.
#define WEAK_FUNCTION_ALIAS(name, strong_name)   iar_weak_alias name, strong_name
 Define name as a weak alias for the function strong_name.
#define END_FUNC(name)   ENDMOD
 Mark the end of the function called name.
Section Definition

#define TEXT_SECTION(name)   RSEG name:CODE:NOROOT
 Start a new section containing executable code.
#define RODATA_SECTION(name)   RSEG name:CONST:NOROOT
 Start a new section containing read-only data.
#define DATA_SECTION(name)   RSEG name:DATA:NOROOT
 Start a new section containing writeable initialized data.
#define BSS_SECTION(name)   RSEG name:DATA:NOROOT
 Start a new section containing writeable zero-initialized data.

Detailed Description

Assembler abstraction layer: IAR Assembler specifics.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

Definition in file iar.h.

Generated on Thu Apr 29 14:10:34 2010 for xplain-bc by  doxygen 1.6.3