Data Structures

Here are the data structures with brief descriptions:
app_usb_mode_taskApplication task struct with shared variables
at45_deviceAT45 DataFlash device
at90usb_controller
at90usb_host
at90usb_udc
at90usb_udc_ep
atomic_objectImplementation-specific structure holding an atomic object
block_deviceA block device
block_requestA block device request
board_spi_selectBoard SPI select struct
bufferA generic data buffer
dataflash_bdevDataFlash specific block device
dataflash_breqDataFlash specific block device request
dma_addr_tA physical/virtual address pair used for DMA
dma_poolDMA memory pool
mem_poolMemory pool
msc_interfaceA Mass Storage Class interface instance
nested_workqueueNested Work Queue
physmem_poolA region of available physical memory
ring_headRing buffer management data
sbc_caching_mode_pageSBC-2 Caching mode page
sbc_read_capacity10_dataSBC-2 READ CAPACITY (10) parameter data
sbc_slba_block_descSBC-2 Short LBA mode parameter block descriptor
scsi_inquiry_dataSCSI Standard Inquiry data structure
scsi_mode_page_0_headerSCSI Page_0 Mode Page header (SPF not set)
scsi_mode_param_header10SCSI Mode Parameter Header used by MODE SELECT(10) and MODE SENSE(10)
scsi_mode_param_header6SCSI Mode Parameter Header used by MODE SELECT(6) and MODE SENSE(6)
slistA singly linked list
slist_nodeA node in a singly linked list
softirq_descSoft interrupt descriptor
spi_devicePolled SPI device defintion
spi_device_privPrivate SPI device definition
spi_masterSPI master
spi_master_polledPolled SPI master defintion
udcA USB Device Controller
udc_fifoInternal state variables used by the FIFO accessors
udm_configA USB device configuration
udm_interfaceA USB device interface
usb_configuration_descriptorStandard USB configuration descriptor
usb_device_descriptorStandard USB device descriptor
usb_device_qualifier_descriptorStandard USB device qualifier descriptor
usb_endpoint_descriptorStandard USB endpoint descriptor
usb_interface_descriptorStandard USB interface descriptor
usb_msc_cbwA Command Block Wrapper (CBW)
usb_msc_cswA Command Status Wrapper (CSW)
usb_requestA USB request
usb_setup_reqA USB Device SETUP request
usb_string_descriptorA standard USB string descriptor
workqueueWork queue
workqueue_taskTask to be run from a work queue
Generated on Thu Apr 29 14:10:36 2010 for xplain-bc by  doxygen 1.6.3