chip/atxmega128a1/include/chip/nvm_regs.h File Reference

NVM register definitions. More...

#include <memory/flash/flash_xmega.h>
#include <memory/eeprom/eeprom_xmega.h>
#include <memory/fuses/fuses_xmega.h>
#include <memory/sram/sram_xmega.h>
#include <memory/lockbits/lockbits_xmega.h>
#include <memory/user-signature/user-signature_xmega.h>
#include <memory/common/memory_common_xmega.h>
#include <io.h>
#include <types.h>
#include <chip/memory-map.h>

Go to the source code of this file.

Defines

#define nvm_write_reg(reg, value)   mmio_write8((void *) (NVM_CONTROLLER_BASE + NVM_##reg), value)
 Write value to the 8-bit NVM register reg.
#define nvm_read_reg(reg)   mmio_read8((void *)(NVM_CONTROLLER_BASE + NVM_##reg))
 Read the 8-bit NVM register reg.

Detailed Description

NVM register definitions.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

Definition in file nvm_regs.h.


Define Documentation

#define nvm_read_reg ( reg   )     mmio_read8((void *)(NVM_CONTROLLER_BASE + NVM_##reg))

Read the 8-bit NVM register reg.

Definition at line 116 of file nvm_regs.h.

#define nvm_write_reg ( reg,
value   )     mmio_write8((void *) (NVM_CONTROLLER_BASE + NVM_##reg), value)

Write value to the 8-bit NVM register reg.

Definition at line 111 of file nvm_regs.h.

Generated on Thu Apr 29 14:09:42 2010 for uart-loopback by  doxygen 1.6.3