include/stdint.h File Reference

C99 integer type definitions. More...

#include <arch/stdint.h>

Go to the source code of this file.


Detailed Description

C99 integer type definitions.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

This file defines the standard C99 integer types like int8_t and friends. These are normally provided by the C library, but since this library is designed for running without one, we need to provide them ourselves.

Note that this file does not define all the types specified by the C99 standard.

Definition in file stdint.h.

Generated on Thu Apr 29 14:09:42 2010 for uart-loopback by  doxygen 1.6.3