include/generic/atomic.h File Reference

Atomic Operations: Generic implementation. More...

#include <compiler.h>
#include <interrupt.h>

Go to the source code of this file.

Data Structures

struct  atomic_object
 Implementation-specific structure holding an atomic object. More...

Typedefs

typedef struct atomic_object atomic_t
 An atomic object representing a value which is manipulated atomically.

Functions

static atomic_value_t atomic_read (atomic_t *ptr)
 Return the value of the atomic object at ptr.
static void atomic_write (atomic_t *ptr, atomic_value_t value)
 Write value to the atomic object at ptr.
static atomic_t atomic_add (atomic_t *ptr, atomic_value_t value)
 Atomically add value to the value stored at ptr.
static atomic_t atomic_sub (atomic_t *ptr, atomic_value_t value)
 Atomically subtract value from the value stored at ptr.

Detailed Description

Atomic Operations: Generic implementation.

Architectures which don't have any special mechanisms for atomic operations may include this file after defining the type atomic_value_t to something suitable for the architecture.

The generic implementation disables interrupts to achieve atomicity.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

Definition in file atomic.h.

Generated on Thu Apr 29 14:09:42 2010 for uart-loopback by  doxygen 1.6.3