Oscillator Management
[Clock Management]

Collaboration diagram for Oscillator Management:

Functions

static __always_inline void osc_enable_internal (uint8_t id)
 Enable internal oscillator id.
static void osc_enable_external (uint8_t id)
 Enable external oscillator id.

Oscillator Management



static __always_inline void osc_disable (uint8_t id)
 Disable oscillator id.
static bool osc_is_running (uint8_t id)
 Determine whether oscillator id is running.
static __always_inline void osc_enable (uint8_t id)
 Enable oscillator id.
static __always_inline uint32_t osc_get_rate (uint8_t id)
 Return the frequency of oscillator id in Hz.

Detailed Description

This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators.


Function Documentation

void osc_disable ( uint8_t  id  )  [static]

Disable oscillator id.

Definition at line 94 of file osc.h.

References osc_read_reg, and osc_write_reg.

Referenced by sysclk_init().

void osc_enable ( uint8_t  id  )  [static]

Enable oscillator id.

The startup time and mode value is automatically determined based on definitions in the board code.

Definition at line 48 of file osc.h.

References assert, osc_enable_external(), and osc_enable_internal().

Referenced by sysclk_init().

osc_enable_external ( uint8_t  id  )  [inline, static]

Enable external oscillator id.

For internal use only.

Do not call this function directly. Use osc_enable() instead. Also note that this function is only available if the board actually has an external oscillator crystal.

Definition at line 88 of file osc.h.

Referenced by osc_enable().

static __always_inline void osc_enable_internal ( uint8_t  id  )  [static]

Enable internal oscillator id.

For internal use only.

Do not call this function directly. Use osc_enable() instead.

Definition at line 59 of file osc.h.

References osc_read_reg, and osc_write_reg.

Referenced by osc_enable().

uint32_t osc_get_rate ( uint8_t  id  )  [static]

Return the frequency of oscillator id in Hz.

Definition at line 58 of file osc.h.

References unhandled_case.

Referenced by pll_config_init().

osc_is_running ( uint8_t  id  )  [inline, static]

Determine whether oscillator id is running.

Return values:
true Oscillator id is running
false Oscillator id is not running

Definition at line 103 of file osc.h.

References osc_read_reg.

Referenced by sysclk_init().

Generated on Thu Apr 29 14:09:43 2010 for uart-loopback by  doxygen 1.6.3