Frame widget implementation. More...
#include <stdint.h>#include <stdlib.h>#include <assert.h>#include <membag.h>#include <string.h>#include <gfx/wtk.h>Go to the source code of this file.
Data Structures | |
| struct | wtk_frame |
| Frame control struct. More... | |
|
| |
| enum | wtk_frame_state { WTK_FRAME_NORMAL, WTK_FRAME_AWAITING_MOVE, WTK_FRAME_MOVING, WTK_FRAME_AWAITING_RESIZE, WTK_FRAME_RESIZING } |
| static struct win_point | wtk_drag_origin |
| Drag origin position during drag operations. | |
| static gfx_color_t * | wtk_drag_origin_pixmap |
| Storage for saved screen beneath drag origin, NULL when not dragging. | |
| static gfx_color_t * | wtk_drag_target_pixmap |
| Storage for saved screen beneath drag target, NULL when not dragging. | |
| static struct gfx_bitmap | wtk_frame_background |
| Frame background bitmap. | |
| static bool | wtk_frame_handler (struct win_window *win, enum win_event_type type, void const *data) |
| static void | wtk_handle_frame_press (struct wtk_frame *frame, struct win_pointer_event const *event) |
| static void | wtk_handle_frame_move (struct wtk_frame *frame, struct win_pointer_event const *event) |
| static void | wtk_handle_frame_release (struct wtk_frame *frame, struct win_pointer_event const *event) |
| static void | wtk_handle_resize_press (struct wtk_frame *frame, struct win_pointer_event const *event) |
| static void | wtk_handle_resize_move (struct wtk_frame *frame, struct win_pointer_event const *event) |
| static void | wtk_handle_resize_release (struct wtk_frame *frame, struct win_pointer_event const *event) |
| static void | wtk_resize_frame (struct wtk_frame *frame, struct win_area const *contents_area) |
| static void | wtk_prepare_drag (struct win_point const *pos) |
| static bool | wtk_is_drag_threshold_exceeded (struct win_point const *pos) |
| static void | wtk_start_drag (struct win_point const *pos) |
| static void | wtk_continue_drag (struct win_point const *last_pos, struct win_point const *pos) |
| static void | wtk_stop_drag (struct win_point const *last_pos) |
| struct win_window * | wtk_frame_as_parent (struct wtk_frame *frame) |
| struct win_window * | wtk_frame_as_child (struct wtk_frame *frame) |
| void * | wtk_frame_get_custom_data (struct wtk_frame const *frame) |
| struct wtk_frame * | wtk_frame_create (struct win_window *parent, struct win_area const *area, char const *caption, bool allow_resize, wtk_frame_handler_t frame_handler, void *custom_data) |
Frame widget implementation.
Copyright (C) 2009 - 2010 Atmel Corporation. All rights reserved.
Definition in file wtk_frame.c.
| enum wtk_frame_state |
Valid states for frame, relevant to pointer and keyboard operations.
For internal use only.
Definition at line 109 of file wtk_frame.c.
| static void wtk_continue_drag | ( | struct win_point const * | last_pos, | |
| struct win_point const * | pos | |||
| ) | [static] |
This function updated the drag target handle graphics. Call this function from the MOVE event handler of the dragging widget. This function needs both the current position and the last used position. The last position will be either the position handed to wtk_start_drag() or the "pos" parameter of the last call to wtk_continue_drag(). The pointer event struct will keep this value for you. No need to store it yourself.
| last_pos | Last position. | |
| pos | Current position. |
Definition at line 575 of file wtk_frame.c.
References gfx_draw_filled_circle, gfx_get_height(), gfx_get_pixmap, gfx_get_width(), gfx_put_pixmap, gfx_set_clipping(), GFX_WHOLE, WTK_DRAG_HANDLE_RADIUS, wtk_drag_origin_pixmap, WTK_DRAG_PIXMAP_SIZE, WTK_DRAG_TARGET_COLOR, and wtk_drag_target_pixmap.
Referenced by wtk_handle_frame_move(), and wtk_handle_resize_move().
| static void wtk_handle_frame_move | ( | struct wtk_frame * | frame, | |
| struct win_pointer_event const * | event | |||
| ) | [static] |
This function is a helper function for the wtk_frame_handler() function. It is called when a pointer MOVE event is sent to the container window. This function either starts or continues a drag operation, depending on current state.
| frame | Frame the received the event. | |
| event | Pointer event information. |
Definition at line 227 of file wtk_frame.c.
References win_pointer_event::last_pos, win_pointer_event::pos, wtk_frame::state, wtk_continue_drag(), WTK_FRAME_AWAITING_MOVE, WTK_FRAME_MOVING, wtk_is_drag_threshold_exceeded(), and wtk_start_drag().
Referenced by wtk_frame_handler().
| static void wtk_handle_frame_press | ( | struct wtk_frame * | frame, | |
| struct win_pointer_event const * | event | |||
| ) | [static] |
This function is a helper function for the wtk_frame_handler() function. It is called when a pointer PRESS event is sent to the container window. This function prepares a drag operation.
| frame | Frame the received the event. | |
| event | Pointer event information. |
Definition at line 201 of file wtk_frame.c.
References wtk_frame::container, win_pointer_event::pos, wtk_frame::state, win_grab_pointer(), WTK_FRAME_AWAITING_MOVE, WTK_FRAME_NORMAL, and wtk_prepare_drag().
Referenced by wtk_frame_handler().
| static void wtk_handle_frame_release | ( | struct wtk_frame * | frame, | |
| struct win_pointer_event const * | event | |||
| ) | [static] |
This function is a helper function for the wtk_frame_handler() function. It is called when a pointer RELEASE event is sent to the container window. This function completes the move operation if the RELEASE event was inside the parent window's boundaries.
| frame | Frame the received the event. | |
| event | Pointer event information. |
Definition at line 260 of file wtk_frame.c.
References wtk_frame::container, win_pointer_event::last_pos, win_area::pos, win_pointer_event::pos, wtk_frame::state, WIN_ATTR_POSITION, win_get_area(), win_get_parent(), win_grab_pointer(), win_is_inside_window(), win_set_area(), wtk_drag_origin, WTK_FRAME_MOVING, WTK_FRAME_NORMAL, and wtk_stop_drag().
Referenced by wtk_frame_handler().
| static void wtk_handle_resize_move | ( | struct wtk_frame * | frame, | |
| struct win_pointer_event const * | event | |||
| ) | [static] |
This function is a helper function for the wtk_frame_handler() function. It is called when a pointer MOVE event is sent to the resize window. This function either starts or continues a drag operation, depending on current state.
| frame | Frame the received the event. | |
| event | Pointer event information. |
Definition at line 328 of file wtk_frame.c.
References win_pointer_event::last_pos, win_pointer_event::pos, wtk_frame::state, wtk_continue_drag(), WTK_FRAME_AWAITING_RESIZE, WTK_FRAME_RESIZING, wtk_is_drag_threshold_exceeded(), and wtk_start_drag().
Referenced by wtk_frame_handler().
| static void wtk_handle_resize_press | ( | struct wtk_frame * | frame, | |
| struct win_pointer_event const * | event | |||
| ) | [static] |
This function is a helper function for the wtk_frame_handler() function. It is called when a pointer PRESS event is sent to the resize window. This function prepares a drag operation.
| frame | Frame the received the event. | |
| event | Pointer event information. |
Definition at line 302 of file wtk_frame.c.
References win_pointer_event::pos, wtk_frame::resize, wtk_frame::state, win_grab_pointer(), WTK_FRAME_AWAITING_RESIZE, WTK_FRAME_NORMAL, and wtk_prepare_drag().
Referenced by wtk_frame_handler().
| static void wtk_handle_resize_release | ( | struct wtk_frame * | frame, | |
| struct win_pointer_event const * | event | |||
| ) | [static] |
This function is a helper function for the wtk_frame_handler() function. It is called when a pointer RELEASE event is sent to the resize window. This function completes the resize operation if the RELEASE event was inside the parent window's boundaries.
| frame | Frame the received the event. | |
| event | Pointer event information. |
Definition at line 361 of file wtk_frame.c.
References wtk_frame::contents, win_pointer_event::last_pos, win_pointer_event::pos, win_area::size, wtk_frame::state, win_get_area(), win_get_parent(), win_grab_pointer(), win_is_inside_window(), wtk_drag_origin, WTK_FRAME_NORMAL, WTK_FRAME_RESIZING, wtk_resize_frame(), and wtk_stop_drag().
Referenced by wtk_frame_handler().
| static bool wtk_is_drag_threshold_exceeded | ( | struct win_point const * | pos | ) | [static] |
This function compares a given position with the drag origin prepared by the wtk_prepare_drag() function. If either the X or Y distance exceeds the WTK_DRAG_THRESHOLD value, this function returns true. That is when the widget event handler should call wtk_start_drag().
| pos | Position to compare. |
Definition at line 489 of file wtk_frame.c.
References wtk_drag_origin, and WTK_DRAG_THRESHOLD.
Referenced by wtk_handle_frame_move(), and wtk_handle_resize_move().
| static void wtk_prepare_drag | ( | struct win_point const * | pos | ) | [static] |
This function prepares for a drag operation. No drag is started yet, but the drag origin is stored. To start a drag operation, one would repeatedly check if the drag threshold is exceeded, then call the wtk_start_drag() function.
| pos | Pointer position for drag origin. |
Definition at line 471 of file wtk_frame.c.
References wtk_drag_origin.
Referenced by wtk_handle_frame_press(), and wtk_handle_resize_press().
| static void wtk_resize_frame | ( | struct wtk_frame * | frame, | |
| struct win_area const * | contents_area | |||
| ) | [static] |
This function is a helper function used when creating a frame widget and when handling resize events. Given a new size for the contents window, it resizes and rearranges the windows composing the frame so that the frame decorations are properly sized and positioned.
| frame | Frame to resize. | |
| contents_area | New size for the contents window. |
Definition at line 407 of file wtk_frame.c.
References wtk_frame::container, wtk_frame::contents, win_area::pos, wtk_frame::resize, win_area::size, WIN_ATTR_POSITION, WIN_ATTR_SIZE, win_get_area(), win_set_area(), WTK_FRAME_BOTTOMBORDER, WTK_FRAME_MIN_HEIGHT, WTK_FRAME_MIN_WIDTH, WTK_FRAME_RESIZE_HEIGHT, WTK_FRAME_RESIZE_WIDTH, WTK_FRAME_RIGHTBORDER, WTK_FRAME_SHADESIZE, WTK_FRAME_TITLEBAR_HEIGHT, and WTK_FRAME_TOPBORDER.
Referenced by wtk_frame_create(), and wtk_handle_resize_release().
| static void wtk_start_drag | ( | struct win_point const * | pos | ) | [static] |
This function starts the drag operation. It will allocate memory to store the screen behind the drag handles and draw the handles themselves. Do not call this function unless wtk_prepare_drag() has been called first with the drag origin position. If there is not enough memory, this function will no draw anything, but it is still safe to call wtk_continue_drag() and wtk_stop_drag().
| pos | Current position of drag target. |
Definition at line 510 of file wtk_frame.c.
References gfx_draw_filled_circle, gfx_get_height(), gfx_get_pixmap, gfx_get_width(), gfx_set_clipping(), GFX_WHOLE, membag_alloc(), membag_free(), WTK_DRAG_HANDLE_RADIUS, wtk_drag_origin, WTK_DRAG_ORIGIN_COLOR, wtk_drag_origin_pixmap, WTK_DRAG_PIXMAP_SIZE, WTK_DRAG_TARGET_COLOR, and wtk_drag_target_pixmap.
Referenced by wtk_handle_frame_move(), and wtk_handle_resize_move().
| static void wtk_stop_drag | ( | struct win_point const * | last_pos | ) | [static] |
This function stops an ongoing drag operation. Do not call this unless dragging has been started with wtk_start_drag() first. This function erases the drag handles and frees any allocated memory.
| last_pos | Last position, as for wtk_continue_drag(). |
Definition at line 612 of file wtk_frame.c.
References gfx_get_height(), gfx_get_width(), gfx_put_pixmap, gfx_set_clipping(), membag_free(), WTK_DRAG_HANDLE_RADIUS, wtk_drag_origin, wtk_drag_origin_pixmap, WTK_DRAG_PIXMAP_SIZE, and wtk_drag_target_pixmap.
Referenced by wtk_handle_frame_release(), and wtk_handle_resize_release().
struct win_point wtk_drag_origin [static] |
Drag origin position during drag operations.
Definition at line 85 of file wtk_frame.c.
Referenced by wtk_handle_frame_release(), wtk_handle_resize_release(), wtk_is_drag_threshold_exceeded(), wtk_prepare_drag(), wtk_start_drag(), and wtk_stop_drag().
gfx_color_t* wtk_drag_origin_pixmap [static] |
Storage for saved screen beneath drag origin, NULL when not dragging.
Definition at line 88 of file wtk_frame.c.
Referenced by wtk_continue_drag(), wtk_start_drag(), and wtk_stop_drag().
gfx_color_t* wtk_drag_target_pixmap [static] |
Storage for saved screen beneath drag target, NULL when not dragging.
Definition at line 91 of file wtk_frame.c.
Referenced by wtk_continue_drag(), wtk_start_drag(), and wtk_stop_drag().
struct gfx_bitmap wtk_frame_background [static] |
{
.type = BITMAP_SOLID,
.data.color = WTK_FRAME_BACKGROUND_COLOR,
}
Frame background bitmap.
Definition at line 100 of file wtk_frame.c.
1.6.3