wtk_radio_group Struct Reference

Collaboration diagram for wtk_radio_group:
Collaboration graph
[legend]

Data Fields

wtk_radio_group_size_t num_references
 Number of members in this group.
struct wtk_radio_buttonselected
 Currently selected member.

Detailed Description

This is the radio button group control struct. It contains the necessary information about a radio button group, i.e. number of members in the group and the current selected one.

Note:
Structure fields are only internally accessible, only pointers to structure is needed externally.

Definition at line 69 of file wtk_radio_button.c.


Field Documentation

Number of members in this group.

Definition at line 71 of file wtk_radio_button.c.

Referenced by wtk_radio_button_create(), wtk_radio_button_handler(), and wtk_radio_group_create().


The documentation for this struct was generated from the following file:
Generated on Thu Apr 29 15:18:25 2010 for display-training by  doxygen 1.6.3