include/stream.h File Reference

Character stream interface. More...

#include <assert.h>
#include <ring.h>
#include <stdarg.h>
#include <types.h>

Go to the source code of this file.

Data Structures

struct  stream
 A generic byte stream. More...
struct  stream_ops
 Stream backend operations. More...

Functions

int stream_vprintf (struct stream *stream, const char *format, va_list ap)
 Formatted output conversion to a stream.
int stream_printf (struct stream *stream, const char *format,...)
 Formatted output conversion.
int stream_putstr (struct stream *stream, const char *str)
 Write a string to a stream.
int stream_putchar (struct stream *stream, int c)
 Write a single character to a stream.
static unsigned int stream_buf_size (struct stream *stream)
 Return the size of the buffer associated with stream.
static bool stream_buf_has_data (struct stream *stream)
 Return true if stream contains any data which can be extracted.
static bool stream_buf_is_full (struct stream *stream)
 Return true if stream currently cannot accept any more data.
static unsigned int stream_buf_unused (struct stream *stream)
 Return the number of bytes available for insertion into stream.
static unsigned int stream_buf_used (struct stream *stream)
 Return the number of bytes available for extraction from stream.
static unsigned int stream_buf_unused_before_end (struct stream *stream)
 Return the number of unused bytes before the buffer wraps around.
static unsigned int stream_buf_used_before_end (struct stream *stream)
 Return the number of bytes available for extraction from stream before the buffer wraps around.
static unsigned int stream_buf_head (struct stream *stream)
 Return the head index of stream, i.e. the index at which to insert the next byte.
static unsigned int stream_buf_tail (struct stream *stream)
 Return the tail index of stream, i.e. the index at which to extract the next byte.
static char stream_buf_insert_char (struct stream *stream, char c)
 Insert the character c at the head of stream.
static char stream_buf_extract_char (struct stream *stream)
 Extract one character from the tail of stream.

Detailed Description

Character stream interface.

Copyright (C) 2009 - 2010 Atmel Corporation. All rights reserved.

Definition in file stream.h.

Generated on Thu Apr 29 15:18:22 2010 for display-training by  doxygen 1.6.3