Physical memory allocation and mapping. More...
#include <cpu/physmem.h>#include <chip/memory-map.h>Go to the source code of this file.
Data Structures | |
| struct | physmem_pool |
| A region of available physical memory. More... | |
Functions | |
| phys_addr_t | physmem_alloc (struct physmem_pool *pool, phys_size_t size, unsigned int align_order) |
| Allocate a region of physical memory. | |
| phys_addr_t | physmem_alloc_low (struct physmem_pool *pool, phys_size_t size, unsigned int align_order) |
| Allocate a low region of physical memory. | |
Physical memory allocation and mapping.
Copyright (C) 2009 Atmel Corporation. All rights reserved.
Definition in file physmem.h.
| phys_addr_t physmem_alloc | ( | struct physmem_pool * | pool, | |
| phys_size_t | size, | |||
| unsigned int | align_order | |||
| ) |
Allocate a region of physical memory.
This function tries to allocate a block of physical memory from the given pool, at the highest possible address.
The following pools must be available on any CPU with internal SRAM (though they may refer to the same pool):
| pool | The physical memory pool to allocate from. | |
| size | The number of bytes to allocate. | |
| align_order | log2 of required alignment. |
Definition at line 66 of file physmem.c.
References physmem_pool::addr, PHYSMEM_ALLOC_ERR, and round_down.
Referenced by hugemem_alloc(), membag_pool_init_physmem(), and tsfs_init().
| phys_addr_t physmem_alloc_low | ( | struct physmem_pool * | pool, | |
| phys_size_t | size, | |||
| unsigned int | align_order | |||
| ) |
Allocate a low region of physical memory.
This function tries to allocate a block of physical memory from the given pool, at the highest possible address.
| pool | The physical memory pool to allocate from. | |
| size | The number of bytes to allocate. | |
| align_order | log2 of required alignment. |
Definition at line 98 of file physmem.c.
References physmem_pool::addr, PHYSMEM_ALLOC_ERR, and round_up.
Referenced by malloc().
1.6.3