include/byteorder.h File Reference

Byte order conversion helpers. More...

#include <compiler.h>
#include <types.h>
#include <arch/byteorder.h>

Go to the source code of this file.

Defines

Byte Swapping

#define swab32(x)
 Swap the order of bytes in a 32-bit word.
#define swab16(x)   ((((x) & 0xff) << 8) | (((x) >> 8) & 0xff))
 Swap the order of bytes in a 16-bit word.

Conversion to/from Little Endian values



#define LE16(x)   ((le16_t __force)(x))
 Create a 16-bit little endian constant.
#define LE32(x)   ((le32_t __force)(x))
 Create a 32-bit little endian constant.
static uint16_t le16_to_cpu (le16_t x)
 Convert a 16-bit word from little endian to native byte order.
static uint32_t le32_to_cpu (le32_t x)
 Convert a 32-bit word from little endian to native byte order.
static le16_t cpu_to_le16 (uint16_t x)
 Convert a 16-bit word from native to little endian byte order.
static le32_t cpu_to_le32 (uint32_t x)
 Convert a 32-bit word from native to little endian byte order.

Conversion to/from Big Endian values



#define BE16(x)
 Create a 16-bit big endian constant.
#define BE32(x)
 Create a 32-bit big endian constant.
static uint16_t be16_to_cpu (be16_t x)
 Convert a 16-bit word from big endian to native byte order.
static uint32_t be32_to_cpu (be32_t x)
 Convert a 32-bit word from big endian to native byte order.
static be16_t cpu_to_be16 (uint16_t x)
 Convert a 16-bit word from native to big endian byte order.
static be32_t cpu_to_be32 (uint32_t x)
 Convert a 32-bit word from native to big endian byte order.

Detailed Description

Byte order conversion helpers.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

Definition in file byteorder.h.

Generated on Thu Apr 29 15:18:22 2010 for display-training by  doxygen 1.6.3