include/bitops.h File Reference

Generic bit operations. More...

#include <assert.h>
#include <compiler.h>
#include <stdbool.h>
#include <types.h>
#include <util.h>
#include <arch/bitops.h>

Go to the source code of this file.

Defines

#define bit_mask(ws, nr)   (1 << ((nr) & ((ws) - 1)))
 Generate a ws-bit mask with only bit nr set.
#define bit_word(ws, nr)   ((nr) / (ws))
 Return the offset of the ws-bit word containing bit nr in a multi-word bitfield.
#define set_bit(nr, bitmap)
 Set bit nr in bitmap.
#define clear_bit(nr, bitmap)
 Clear bit nr in bitmap.
#define toggle_bit(nr, bitmap)
 Toggle bit nr in bitmap.
#define test_bit(nr, bitmap)   priv_test_bit_ws(nr, bitmap, 8 * sizeof(*(bitmap)))
 Test bit nr in bitmap.
#define bit_word_reverse(word)   compiler_brev(word)
 Reverse the order of the bits in word.
#define bit_word_find_first_one_bit(word)   compiler_ctz(word)
 Find the first bit set in word, counting from the LSB.
#define bit_word_find_last_one_bit(word)   (31 - compiler_clz(word))
 Find the last bit set in word, counting from the LSB.
#define bit_word_find_first_zero_bit(word)   bit_word_find_first_one_bit(~word)
 Find the first bit cleared in word, counting from the LSB.
#define bit_word_find_last_zero_bit(word)   bit_word_find_last_one_bit(~word)
 Find the last bit cleared in word, counting from the LSB.

Functions

static unsigned int bit_array_find_first_one_bit (const bit_word_t *bitmap, unsigned int len)
 Find the first bit set in bitmap, counting from the LSB of each word.

Detailed Description

Generic bit operations.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

Definition in file bitops.h.

Generated on Thu Apr 29 15:18:22 2010 for display-training by  doxygen 1.6.3