Tiny Simple File System (TSFS), block device based

Data Structures

struct  tsfs_file
 Holds information about a specific file within a file system. More...
struct  tsfs_header
 Header structure. Holds generic information about the file system. More...
struct  tsfs_read_request
 Holds current read request being processed by a file system. More...
struct  tsfs_filetable_entry
 Holds information on one file in the file table. More...
struct  tsfs
 Holds information on a TSFS instance. More...

Defines

#define TSFS_ID   0x17c1
 Unique ID to identify TSFS.
#define TSFS_FILENAME_LEN   8
 Max characters in a filename.
#define TSFS_MAX_FILES   31
 Max number of files supported.
#define TSFS_BLOCKSIZE   512
 Size of block in bytes.

Enumerations

enum  tsfs_seek_origin { SEEK_SET, SEEK_CUR, SEEK_END }
 

The relative starting point of seek operations.

More...

Functions

status_t tsfs_init (struct tsfs *tsfs, struct block_device *system_blockdevice, struct workqueue_task *system_ready_task)
 Initiates a Tiny Simple File System.
status_t tsfs_open (struct tsfs *tsfs, const char *filename, struct tsfs_file *filehandle)
 Opens a file by populating a file handle.
status_t tsfs_seek (struct tsfs_file *file, int32_t offset, enum tsfs_seek_origin origin)
 Manualy move the file cursor.
status_t tsfs_read (struct tsfs *tsfs, struct tsfs_file *file, void *buffer, uint32_t length, struct workqueue_task *task)
 Reads a chunk of data from a file to a buffer.
void tsfs_get_filename (struct tsfs *tsfs, uint_fast8_t file_index, uint8_t *buffer)
 Reads the filename of an indexed file into a buffer.
static uint32_t tsfs_get_file_size (struct tsfs_file *file)
 Get the file size in bytes for file file.
static uint32_t tsfs_nr_files (struct tsfs *tsfs)
 Returns the number of files present in a file system.
static uint32_t tsfs_volume_size (struct tsfs *tsfs)
 Returns the size of the entire volume.
static uint32_t tsfs_is_ready (struct tsfs *tsfs)
 Check if file system is ready for use.



static void tsfs_buf_list_done (struct block_device *bdev, struct block_request *breq, struct slist *buf_list)
 Block device list complete callback.
static void tsfs_read_page_done (struct block_device *bdev, struct block_request *breq)
 Block device request complete callback.

Detailed Description

file system.

This module provides mechanisms for data stored in a TSFS file system. Note: All data is stored using big endigan encoding, and translated to CPU specific endianess after being read into the file system.

In order to improve execution times most functions in this module assume input parameters are clean. This means that there are no sanity on any parameters unless it is explisitly stated in this document.


Define Documentation

#define TSFS_BLOCKSIZE   512

Size of block in bytes.

Definition at line 79 of file tsfs.h.

Referenced by tsfs_init(), and tsfs_read().

#define TSFS_FILENAME_LEN   8

Max characters in a filename.

Definition at line 68 of file tsfs.h.

Referenced by tsfs_get_filename().

#define TSFS_ID   0x17c1

Unique ID to identify TSFS.

Definition at line 66 of file tsfs.h.

#define TSFS_MAX_FILES   31

Max number of files supported.

Definition at line 75 of file tsfs.h.

Referenced by tsfs_init().


Enumeration Type Documentation

The relative starting point of seek operations.

Enumerator:
SEEK_SET 

Seek relative to beginning of file.

SEEK_CUR 

Seek relative to current cursor position.

SEEK_END 

Seek relative to end of file.

Definition at line 193 of file tsfs.h.


Function Documentation

static void tsfs_buf_list_done ( struct block_device bdev,
struct block_request breq,
struct slist buf_list 
) [static]

Block device list complete callback.

Definition at line 67 of file tsfs.c.

static uint32_t tsfs_get_file_size ( struct tsfs_file file  )  [inline, static]

Get the file size in bytes for file file.

Returns:
Size given in bytes for file file

Definition at line 223 of file tsfs.h.

References tsfs_file::end, and tsfs_file::start.

void tsfs_get_filename ( struct tsfs tsfs,
uint_fast8_t  file_index,
uint8_t buffer 
)

Reads the filename of an indexed file into a buffer.

Note:
buffer must be able to hold at least TSFS_FILENAME_LEN bytes.
Parameters:
tsfs TSFS structure which holds file system information
file_index Index of file which name is to be fetched
buffer Buffer where filename will be written

Definition at line 475 of file tsfs.c.

References tsfs_filetable_entry::filename, memcpy(), and TSFS_FILENAME_LEN.

status_t tsfs_init ( struct tsfs tsfs,
struct block_device bdev,
struct workqueue_task init_done_task 
)

Initiates a Tiny Simple File System.

The block device specified by system_blockdevice has to have a block size of TSFS_BLOCKSIZE bytes.

Immediately after returning from this function, the file system will have status ERR_BUSY. The system is ready for use when the status changes to STATUS_OK. This can be polled for, or the parameter init_done_task can be used to specify a task to be scheduled when the system is ready.

In case the data loaded from the block device is not TSFS compatible the file system will not schedule the callback task, and set its own status to ERR_BAD_FORMAT. At this point the file system has to be re-initialized with a valid block device if it is to be used.

Parameters:
tsfs TSFS structure which holds file system information
bdev Block device to read data from
init_done_task Callback task for when system is ready for use

Definition at line 232 of file tsfs.c.

References assert, tsfs::bdev, board_extram_pool, tsfs::buffer_data, CPU_DMA_ALIGN, tsfs::current_read_request, ERR_BUSY, ERR_NO_MEMORY, malloc(), physmem_alloc(), PHYSMEM_ALLOC_ERR, tsfs::status, STATUS_OK, tsfs_read_request::task, TSFS_BLOCKSIZE, and TSFS_MAX_FILES.

static uint32_t tsfs_is_ready ( struct tsfs tsfs  )  [inline, static]

Check if file system is ready for use.

Returns:
Returns true if a file system tsfs is ready for use

Definition at line 253 of file tsfs.h.

References tsfs::bdev, tsfs::status, and STATUS_OK.

static uint32_t tsfs_nr_files ( struct tsfs tsfs  )  [inline, static]

Returns the number of files present in a file system.

Returns:
The number of files in the file system tsfs

Definition at line 233 of file tsfs.h.

References tsfs::header, and tsfs_header::nr_files.

status_t tsfs_open ( struct tsfs tsfs,
const char *  filename,
struct tsfs_file filehandle 
)

Opens a file by populating a file handle.

Searches through the filetable of tsfs and opens the first file that matches the filename string. Note that this can be a pointer to any normal character array, even though TSFS filenames do not have a termchar

Parameters:
tsfs TSFS structure which holds file system information
filename Name of file to be opened
filehandle File structure to store results
Return values:
\ref STATUS_OK if successful.
\ref ERR_INVALID_ARG if file is not found.

Definition at line 404 of file tsfs.c.

References tsfs_file::cursor, tsfs_file::end, ERR_INVALID_ARG, tsfs_filetable_entry::file_offset, tsfs_filetable_entry::file_size, tsfs::header, tsfs_header::nr_files, tsfs_file::start, and STATUS_OK.

status_t tsfs_read ( struct tsfs tsfs,
struct tsfs_file file,
void *  buffer,
uint32_t  length,
struct workqueue_task task 
)

Reads a chunk of data from a file to a buffer.

Any file system can only issue one read request at a time, and hence if the system is busy reading another file tsfs_read will return ERR_BUSY. The user application should pick up on this and reschedule its read attempt.

The task is scheduled to execute once the copy operation is complete, but only if tsfs_read returns STATUS_OK. If it returns any error message, the task is not scheduled.

The length parameter is trimmed to never exceed the length of the file.

Parameters:
tsfs TSFS structure which holds file system information
file Handle of the file to be read from
buffer Pointer to buffer where data is read to
length Number of bytes to read
task Task to be scheduled upon successful completion
Return values:
\ref STATUS_OK if successful
\ref ERR_INVALID_ARG if trying to read at the end of a file, or trying to read 0 bytes.
\ref ERR_BUSY if file system is busy reading from another file.

Definition at line 317 of file tsfs.c.

References tsfs_read_request::buffer, tsfs::current_read_request, tsfs_read_request::cursor, tsfs_file::cursor, tsfs_file::end, ERR_BUSY, ERR_INVALID_ARG, ilog2(), tsfs::lba_in_buf, tsfs_read_request::remaining_bytes, tsfs::status, STATUS_OK, tsfs_read_request::task, and TSFS_BLOCKSIZE.

static void tsfs_read_page_done ( struct block_device bdev,
struct block_request breq 
) [static]

Block device request complete callback.

Definition at line 76 of file tsfs.c.

References block_free_request(), block_request::context, tsfs::current_breq, and tsfs::page_read_callback.

status_t tsfs_seek ( struct tsfs_file file,
int32_t  offset,
enum tsfs_seek_origin  origin 
)

Manualy move the file cursor.

Available offsets are found in tsfs_seek_origin. Note that to offset inwards from the end of the file, negative values should be used for offset. It is possible to seek the file cursor to any value, even invalid ones, so care should be taken when using this function. If an invalid value is passed for origin, the application will execute unhandled_case()

Parameters:
file File to seek in
offset Number of bytes to move the cursor
origin Position from which offset is counted
Returns:
Returns STATUS_OK if successful

Definition at line 442 of file tsfs.c.

References tsfs_file::cursor, tsfs_file::end, SEEK_CUR, SEEK_END, SEEK_SET, tsfs_file::start, STATUS_OK, and unhandled_case.

static uint32_t tsfs_volume_size ( struct tsfs tsfs  )  [inline, static]

Returns the size of the entire volume.

Returns:
The size of file system tsfs

Definition at line 243 of file tsfs.h.

References tsfs::header, and tsfs_header::volume_size.

Generated on Thu Apr 29 15:18:23 2010 for display-training by  doxygen 1.6.3