|
Modules | |
| ATxmega SPI internals | |
Defines | |
| #define | MAXLOOPS 255 |
| Maximum number of polling loops. | |
| #define | SPI_MASTER_NATIVE_GET_BASE(spim_p) (&((struct spi_master_priv *)spim_p)->base.base) |
| Get base definition of spi_master. | |
| #define | SPI_DEVICE_NATIVE_GET_BASE(spid_p) (&((struct spi_device_priv *)spid_p)->base) |
| Get base definition of native spi_device. | |
| #define | SPI_ID_LAST 11 |
| Last SPI ID. | |
| #define | SPI_ID_UART_FIRST 4 |
| First SPI ID which is a uart. | |
| #define | spi_id_is_valid(spi_id) (spi_id <= SPI_ID_LAST) |
| Test if SPI Module ID is valid. | |
| #define | SPI_ID_NATIVE_IS_ENABLED false |
| true if native SPI is enabled | |
| #define | SPI_ID_UART_IS_ENABLED false |
| true if uart SPI is enabled | |
| #define | SPI_MASTER_TYPE_NAME(spi_id) spi_master_type##spi_id |
| Get spi_master derived type name from spi_id. | |
| #define | DECLARE_SPI_MASTER(spi_id, varname) struct SPI_MASTER_TYPE_NAME(spi_id) varname |
| Declare a spi_master derived struct for given SPI Module ID. | |
| #define | SPI_DEVICE_TYPE_NAME(spi_id) spi_device_type##spi_id |
| Get spi_device derived type name from spi_id. | |
| #define | DECLARE_SPI_DEVICE(spi_id, varname) struct SPI_DEVICE_TYPE_NAME(spi_id) varname |
| Declare a spi_device derived struct for given SPI Module ID. | |
Typedefs | |
| typedef uint8_t | maxloops_t |
| Defintion of poll loop counter variable. | |
Functions | |
| static void | spi_poll (struct workqueue_task *task) |
| Poll SPI registers for required actions. | |
| void | spi_priv_master_setup_device (spi_id_t spi_id, struct spi_device *device, spi_flags_t flags, unsigned long baud_rate, board_spi_select_id_t sel_id) |
| Private setup SPI device. | |
| void | spi_priv_select_device (struct spi_master *master, struct spi_device *device) |
| Private select SPI device. | |
| void | spi_priv_deselect_device (struct spi_master *master, struct spi_device *device) |
| Private deselect SPI device. | |
| void | spi_priv_master_init (spi_id_t spi_id, struct spi_master *master) |
| Private init SPI master. | |
| static struct spi_master * | spi_master_get_base (spi_id_t spi_id, void *priv) |
| Multiplex statements based on spi_id. | |
| static size_t | spi_master_get_size (spi_id_t spi_id) |
| Get spi_master derived struct size for the given SPI Module ID. | |
| static struct spi_device * | spi_device_get_base (spi_id_t spi_id, void *priv) |
| Get base defintion of spi_device. | |
| static size_t | spi_device_get_size (spi_id_t spi_id) |
| Get spi_device derived struct size for the given SPI Module ID. | |
| static void | spi_priv_enable (spi_id_t spi_id) |
| Private SPI enable. | |
| static void | spi_priv_disable (spi_id_t spi_id) |
| Private SPI disable. | |
| static bool | spi_priv_is_enabled (spi_id_t spi_id) |
| Private SPI is enabled. | |
| static bool | spi_priv_is_int_flag_set (struct spi_master *spim) |
| Test if SPI interrupt flag is set. | |
| static uint8_t | spi_priv_read_data (struct spi_master *spim) |
| SPI read data register. | |
| static void | spi_priv_write_data (struct spi_master *spim, uint8_t data) |
| SPI write data register. | |
| static void | spi_priv_master_setup_device_regs (struct spi_device *device, spi_flags_t flags, unsigned long baud_rate) |
| Setup SPI device register specifics. | |
| static void | spi_priv_select_device_regs (struct spi_master *spim, struct spi_device *device) |
| Select SPI device register specifics. | |
| static void | spi_priv_deselect_device_regs (struct spi_master *spim, struct spi_device *device) |
| Deselect SPI device register specifics. | |
| static void | spi_priv_master_init_regs (spi_id_t spi_id, struct spi_master *spim) |
| Init SPI master register specifics. | |
| #define DECLARE_SPI_DEVICE | ( | spi_id, | |||
| varname | ) | struct SPI_DEVICE_TYPE_NAME(spi_id) varname |
Declare a spi_device derived struct for given SPI Module ID.
| spi_id | SPI Module ID | |
| varname | Name to declare it as |
Definition at line 331 of file spi_mega_xmega.h.
| #define DECLARE_SPI_MASTER | ( | spi_id, | |||
| varname | ) | struct SPI_MASTER_TYPE_NAME(spi_id) varname |
Declare a spi_master derived struct for given SPI Module ID.
| spi_id | SPI Module ID | |
| varname | Name to declare it as |
Definition at line 257 of file spi_mega_xmega.h.
| #define MAXLOOPS 255 |
Maximum number of polling loops.
This is the maximum number of loops run in the polling function before it must reschedule itself.
Definition at line 69 of file spi_mega_xmega.c.
Referenced by spi_poll().
| #define SPI_DEVICE_NATIVE_GET_BASE | ( | spid_p | ) | (&((struct spi_device_priv *)spid_p)->base) |
Get base definition of native spi_device.
| spid_p | Pointer to spi_device_priv |
Referenced by spi_device_get_base().
| #define SPI_DEVICE_TYPE_NAME | ( | spi_id | ) | spi_device_type##spi_id |
Get spi_device derived type name from spi_id.
| spi_id | SPI Module ID |
Definition at line 323 of file spi_mega_xmega.h.
| #define spi_id_is_valid | ( | spi_id | ) | (spi_id <= SPI_ID_LAST) |
Test if SPI Module ID is valid.
| spi_id | SPI Module ID |
| true | Id is valid | |
| false | Not a valid id |
Definition at line 232 of file spi_mega_xmega.h.
Referenced by spi_device_get_base(), spi_device_get_size(), spi_disable(), spi_enable(), spi_is_enabled(), spi_master_get_base(), and spi_master_get_size().
| #define SPI_ID_NATIVE_IS_ENABLED false |
| #define SPI_ID_UART_IS_ENABLED false |
| #define SPI_MASTER_NATIVE_GET_BASE | ( | spim_p | ) | (&((struct spi_master_priv *)spim_p)->base.base) |
Get base definition of spi_master.
| spim_p | Pointer to private derived spi_master |
Referenced by spi_master_get_base().
| #define SPI_MASTER_TYPE_NAME | ( | spi_id | ) | spi_master_type##spi_id |
Get spi_master derived type name from spi_id.
| spi_id | SPI Module ID |
Definition at line 249 of file spi_mega_xmega.h.
| typedef uint8_t maxloops_t |
Defintion of poll loop counter variable.
For internal use only.
This helps the compiler in optimizing the loop to be as fast as possible
Definition at line 79 of file spi_mega_xmega.c.
| static struct spi_device* spi_device_get_base | ( | spi_id_t | spi_id, | |
| void * | priv | |||
| ) | [static, read] |
Get base defintion of spi_device.
| spi_id | SPI Module ID | |
| priv | Pointer to private declared SPI device struct |
Definition at line 340 of file spi_mega_xmega.h.
References assert, SPI_DEVICE_NATIVE_GET_BASE, and spi_id_is_valid.
| static size_t spi_device_get_size | ( | spi_id_t | spi_id | ) | [inline, static] |
Get spi_device derived struct size for the given SPI Module ID.
| spi_id | SPI Module ID |
Definition at line 355 of file spi_mega_xmega.h.
References assert, SPI_DEVICE_NATIVE_TYPE, and spi_id_is_valid.
| static struct spi_master* spi_master_get_base | ( | spi_id_t | spi_id, | |
| void * | priv | |||
| ) | [static, read] |
Multiplex statements based on spi_id.
This multiplexing definition is set up based on what SPI driver variants have been enabled thru config. For a single variant any testing on spi_id is bypassed, and for several spi_id is used for multiplexing.
The statements in native and uart are a bit off in concern to c-syntax, but contains the whole statement to be used for that variant.
| spi_id | SPI Module ID | |
| native | Statement to run if it's native based | |
| uart | Statement to run if it's uart based Get base defintion of spi_master | |
| spi_id | SPI Module ID | |
| priv | Pointer to private declared spi master |
Definition at line 294 of file spi_mega_xmega.h.
References assert, spi_id_is_valid, and SPI_MASTER_NATIVE_GET_BASE.
| static size_t spi_master_get_size | ( | spi_id_t | spi_id | ) | [inline, static] |
Get spi_master derived struct size for the given SPI Module ID.
| spi_id | SPI Module ID |
Definition at line 309 of file spi_mega_xmega.h.
References assert, spi_id_is_valid, and SPI_MASTER_NATIVE_TYPE.
| static void spi_poll | ( | struct workqueue_task * | task | ) | [static] |
Poll SPI registers for required actions.
For internal use only.
| task | Polling task structure |
1. Time between interrupt flag is set to write of data register for next transfer should be as short as possible. This to keep the time between transfers as short as possible.
2. Time between writing and checking the interrupt flag should be minimum 16 cycles long. Maximum speed of spi is half of cpu clock, and with a 8-bit transfer this ideally should happen within 16 cpu cycles.
Definition at line 102 of file spi_mega_xmega.c.
References spi_master_polled::base, container_of, nested_workqueue::current, main_workqueue, MAXLOOPS, spi_master::nwq, spi_master_polled::op, spi_master_polled::poll, spi_master_polled::read_data, spi_master::residue, SPI_OP_READ, SPI_OP_WRITE, spi_polled_is_buffer_op(), spi_polled_sched_next_buffer(), spi_polled_sched_poll(), spi_priv_is_int_flag_set(), spi_priv_read_data(), spi_priv_write_data(), spi_master::status, STATUS_OK, test_bit, workqueue_add_task(), and spi_master_polled::write_data.
| void spi_priv_deselect_device | ( | struct spi_master * | master, | |
| struct spi_device * | device | |||
| ) |
Private deselect SPI device.
| master | SPI master struct | |
| device | SPI device struct |
Referenced by spi_deselect_device().
| void spi_priv_deselect_device_regs | ( | struct spi_master * | spim, | |
| struct spi_device * | device | |||
| ) | [inline, static] |
Deselect SPI device register specifics.
| spim | SPI master struct | |
| device | SPI device struct |
Definition at line 170 of file spi_xmega.h.
| void spi_priv_disable | ( | spi_id_t | spi_id | ) | [inline, static] |
Private SPI disable.
| spi_id | SPI Module ID |
Definition at line 104 of file spi_xmega.h.
References spi_write_reg, sysclk_disable_module(), and SYSCLK_SPI.
Referenced by spi_disable().
| void spi_priv_enable | ( | spi_id_t | spi_id | ) | [inline, static] |
Private SPI enable.
| spi_id | SPI Module ID |
Definition at line 98 of file spi_xmega.h.
References SPI_BIT, spi_write_reg, sysclk_enable_module(), and SYSCLK_SPI.
Referenced by spi_enable().
| bool spi_priv_is_enabled | ( | spi_id_t | spi_id | ) | [inline, static] |
Private SPI is enabled.
| spi_id | SPI Module ID |
| true | SPI is enabled | |
| false | SPI is disabled |
Definition at line 110 of file spi_xmega.h.
References SPI_BIT, and spi_read_reg.
Referenced by spi_is_enabled().
| bool spi_priv_is_int_flag_set | ( | struct spi_master * | spim | ) | [inline, static] |
Test if SPI interrupt flag is set.
| spim | SPI master struct |
| true | Interrupt flag is set | |
| false | Interrupt flag is not set |
Definition at line 116 of file spi_xmega.h.
References spi_master_priv::regs, SPI_BIT, and spi_read_reg.
Referenced by spi_poll().
| void spi_priv_master_init | ( | spi_id_t | spi_id, | |
| struct spi_master * | master | |||
| ) |
Private init SPI master.
| spi_id | SPI Module ID | |
| master | SPI master struct |
Referenced by spi_master_init().
| void spi_priv_master_init_regs | ( | spi_id_t | spi_id, | |
| struct spi_master * | spim | |||
| ) | [inline, static] |
Init SPI master register specifics.
| spi_id | SPI Module ID | |
| spim | SPI master struct |
Definition at line 175 of file spi_xmega.h.
References spi_master_priv::regs, SPI_BIT, spi_read_reg, and spi_write_reg.
| void spi_priv_master_setup_device | ( | spi_id_t | spi_id, | |
| struct spi_device * | device, | |||
| spi_flags_t | flags, | |||
| unsigned long | baud_rate, | |||
| board_spi_select_id_t | sel_id | |||
| ) |
Private setup SPI device.
| spi_id | SPI Module ID | |
| device | SPI device struct | |
| flags | Flags | |
| baud_rate | Baud rate | |
| sel_id | Board select id |
Referenced by spi_master_setup_device().
| void spi_priv_master_setup_device_regs | ( | struct spi_device * | device, | |
| spi_flags_t | flags, | |||
| unsigned long | baud_rate | |||
| ) | [inline, static] |
Setup SPI device register specifics.
| device | SPI device struct | |
| flags | Flags | |
| baud_rate | Baud rate |
Definition at line 137 of file spi_xmega.h.
References spi_device_priv::ctrl, SPI_BF, and SPI_BIT.
| uint8_t spi_priv_read_data | ( | struct spi_master * | spim | ) | [inline, static] |
SPI read data register.
| spim | SPI master struct |
Definition at line 123 of file spi_xmega.h.
References spi_master_priv::regs, and spi_read_reg.
Referenced by spi_poll().
| void spi_priv_select_device | ( | struct spi_master * | master, | |
| struct spi_device * | device | |||
| ) |
Private select SPI device.
| master | SPI master struct | |
| device | SPI device struct |
Referenced by spi_select_device().
| void spi_priv_select_device_regs | ( | struct spi_master * | spim, | |
| struct spi_device * | device | |||
| ) | [inline, static] |
Select SPI device register specifics.
| spim | SPI master struct | |
| device | SPI device struct |
Definition at line 161 of file spi_xmega.h.
References spi_device_priv::ctrl, spi_master_priv::regs, and spi_write_reg.
| void spi_priv_write_data | ( | struct spi_master * | spim, | |
| uint8_t | data | |||
| ) | [inline, static] |
SPI write data register.
| spim | SPI master struct | |
| data | Data byte to write |
Definition at line 130 of file spi_xmega.h.
References spi_master_priv::regs, and spi_write_reg.
Referenced by spi_poll().
1.6.3