|
Data Structures | |
| struct | mem_pool |
| Memory pool. More... | |
Functions | |
| void | mem_pool_init (struct mem_pool *pool, void *start, size_t size, size_t objsize, unsigned int align_order) |
| Initialize a memory pool. | |
| void | mem_pool_init_physmem (struct mem_pool *mempool, struct physmem_pool *phys_pool, unsigned int nr_objects, size_t objsize, unsigned int align_order) |
| Initialize a memory pool using the physmem allocator. | |
| void * | mem_pool_alloc (struct mem_pool *pool) |
| Allocate an object from a memory pool. | |
| void | mem_pool_free (struct mem_pool *pool, const void *obj) |
| Free an object previously allocated from a memory pool. | |
A memory pool contains a number of objects of the same size that can be allocated in constant time. This is useful for allocating request structures, etc.
Memory pool objects are managed in Last-In-First-Out (LIFO) order to maximize the chances of allocating a cache-hot object.
| void * mem_pool_alloc | ( | struct mem_pool * | pool | ) |
Allocate an object from a memory pool.
| pool | The memory pool from which the object is allocated. |
Referenced by buffer_alloc(), dataflash_alloc_req(), and membag_alloc().
| void mem_pool_free | ( | struct mem_pool * | pool, | |
| const void * | obj | |||
| ) |
Free an object previously allocated from a memory pool.
The caller is responsible for making sure obj was originally allocated from pool. If an object is freed into a different pool, the integrity of the pool can no longer be guaranteed.
| pool | The memory pool which the object belongs to. | |
| obj | The object to be freed. |
Referenced by buffer_free(), dataflash_free_req(), and membag_free().
| void mem_pool_init | ( | struct mem_pool * | pool, | |
| void * | start, | |||
| size_t | size, | |||
| size_t | objsize, | |||
| unsigned int | align_order | |||
| ) |
Initialize a memory pool.
This function will initialize a memory pool, populating its freelist with objects tightly packed into the specified memory range.
All objects in the pool are guaranteed to be aligned to a multiple of
bytes. For example, if align_order is 4, each object will start on a 16-byte boundary.
| pool | The memory pool to be initialized. | |
| start | The memory area to be used for object storage. | |
| size | The size of the memory area in bytes. | |
| objsize | The size of each object in bytes. | |
| align_order | log2 of the minimum object alignment in bytes. |
Referenced by membag_pool_init_physmem().
| void mem_pool_init_physmem | ( | struct mem_pool * | mempool, | |
| struct physmem_pool * | phys_pool, | |||
| unsigned int | nr_objects, | |||
| size_t | objsize, | |||
| unsigned int | align_order | |||
| ) |
Initialize a memory pool using the physmem allocator.
This function will grab enough physical memory for nr_objects and use this to initialize mempool.
| mempool | The memory pool to be initialized. | |
| phys_pool | The physical memory pool from which to grab memory | |
| nr_objects | The number of objects in the pool | |
| objsize | The size of each object in bytes. | |
| align_order | log2 of the minimum object alignment in bytes. |
Referenced by buffer_pool_init().
1.6.3