Data in Huge Data Memory Space
[Utility Library]

Collaboration diagram for Data in Huge Data Memory Space:

Modules

 Hugemem implementation for 8-bit AVR.

Defines

#define HUGEMEM_NULL   0
 Hugemem null pointer, similar to NULL, but works across different platforms.

Typedefs

typedef uint32_t hugemem_ptr_t
 Type to use for pointers to huge memory.

Functions

hugemem_ptr_t hugemem_alloc (struct physmem_pool *pool, phys_size_t size, unsigned int align_order)
 Allocate a region of huge memory.
static uint_fast8_t hugemem_read8 (const hugemem_ptr_t from)
 Read 8-bit value stored at huge memory address from.
uint_fast16_t hugemem_read16 (const hugemem_ptr_t from)
 Read 16-bit value stored at huge memory address from.
uint_fast32_t hugemem_read32 (const hugemem_ptr_t from)
 Read 32-bit value stored at huge memory address from.
static void hugemem_write8 (hugemem_ptr_t to, uint_fast8_t val)
 Write 8-bit value val to huge memory address to.
void hugemem_write16 (hugemem_ptr_t to, uint_fast16_t val)
 Write 16-bit value val to huge memory address to.
void hugemem_write32 (hugemem_ptr_t to, uint_fast32_t val)
 Write 32-bit value val to huge memory address to.
void hugemem_read_block (void *to, const hugemem_ptr_t from, size_t size)
 Read size bytes from huge memory address from into buffer at address to.
void hugemem_write_block (hugemem_ptr_t to, const void *from, size_t size)
 Write size bytes from buffer at address from to huge memory address to.

Detailed Description

Due to shortcomings of the GCC compiler for 8-bit AVR, custom functions are needed for access to data beyond the 64 kB boundary, i.e., addresses that are larger than 16-bit.

The definition of huge memory space can differ between architectures, so the implementation is architecture specific.

This module supplies functions for copying a number of bytes between huge and 64 kB data memory space, and is needed solely for code compatibility across compilers.


Define Documentation

#define HUGEMEM_NULL   0

Hugemem null pointer, similar to NULL, but works across different platforms.

Definition at line 66 of file hugemem.h.

Referenced by hugemem_alloc().


Typedef Documentation

Type to use for pointers to huge memory.

Definition at line 64 of file hugemem.h.


Function Documentation

hugemem_ptr_t hugemem_alloc ( struct physmem_pool pool,
phys_size_t  size,
unsigned int  align_order 
)

Allocate a region of huge memory.

This function tries to allocate a block of huge memory from the given pool, at the highest possible address.

Parameters:
pool The huge memory pool to allocate from.
size The number of bytes to allocate.
align_order log2 of required alignment.
Returns:
A valid hugemem address, or HUGEMEM_NULL if there isn't sufficient memory available.
Precondition:
Not in interrupt context.

Definition at line 55 of file hugemem.c.

References HUGEMEM_NULL, physmem_alloc(), and PHYSMEM_ALLOC_ERR.

uint_fast16_t hugemem_read16 ( const hugemem_ptr_t  from  ) 

Read 16-bit value stored at huge memory address from.

Definition at line 44 of file arch_hugemem.c.

References CPU_REG.

uint_fast32_t hugemem_read32 ( const hugemem_ptr_t  from  ) 

Read 32-bit value stored at huge memory address from.

Definition at line 62 of file arch_hugemem.c.

References CPU_REG.

uint_fast8_t hugemem_read8 ( const hugemem_ptr_t  from  )  [inline, static]

Read 8-bit value stored at huge memory address from.

Definition at line 68 of file hugemem.h.

References CPU_REG.

Referenced by gfx_copy_hugemem_pixels_to_screen().

void hugemem_read_block ( void *  to,
const hugemem_ptr_t  from,
size_t  size 
)

Read size bytes from huge memory address from into buffer at address to.

Definition at line 82 of file arch_hugemem.c.

References assert, and CPU_REG.

Referenced by gfx_draw_char_hugemem().

void hugemem_write16 ( hugemem_ptr_t  to,
uint_fast16_t  val 
)

Write 16-bit value val to huge memory address to.

Definition at line 104 of file arch_hugemem.c.

References CPU_REG.

void hugemem_write32 ( hugemem_ptr_t  to,
uint_fast32_t  val 
)

Write 32-bit value val to huge memory address to.

Definition at line 118 of file arch_hugemem.c.

References CPU_REG.

void hugemem_write8 ( hugemem_ptr_t  to,
uint_fast8_t  val 
) [inline, static]

Write 8-bit value val to huge memory address to.

Definition at line 88 of file hugemem.h.

References CPU_REG.

void hugemem_write_block ( hugemem_ptr_t  to,
const void *  from,
size_t  size 
)

Write size bytes from buffer at address from to huge memory address to.

Definition at line 134 of file arch_hugemem.c.

References assert, and CPU_REG.

Generated on Thu Apr 29 15:18:23 2010 for display-training by  doxygen 1.6.3