Check box widget
[Widget toolkit]

Collaboration diagram for Check box widget:

Functions

struct wtk_check_boxwtk_check_box_create (struct win_window *parent, struct win_area const *area, char const *caption, bool selected, win_command_t command_data)
struct win_windowwtk_check_box_as_child (struct wtk_check_box *check_box)
void wtk_check_box_toggle (struct wtk_check_box *check_box)
void wtk_check_box_set (struct wtk_check_box *check_box, bool selected)
bool wtk_check_box_is_selected (struct wtk_check_box const *check_box)
void wtk_check_box_size_hint (struct win_point *size, const char *caption)
 Get minimum widget size.



enum  wtk_check_box_state { WTK_CHECKBOX_NORMAL, WTK_CHECKBOX_PRESSED }
static bool wtk_check_box_handler (struct win_window *win, enum win_event_type type, void const *data)



#define WTK_CHECKBOX_BOX_SIZE   8
 Size of checkbox square.
#define WTK_CHECKBOX_BOX_X   0
 Checkbox square X offset.
#define WTK_CHECKBOX_BOX_Y   0
 Checkbox square Y offset.
#define WTK_CHECKBOX_CAPTION_X   (WTK_CHECKBOX_BOX_SIZE + 4)
 Checkbox caption text X offset.
#define WTK_CHECKBOX_CAPTION_Y   0
 Checkbox caption text Y offset.
#define WTK_CHECKBOX_BOX_COLOR   GFX_COLOR(0, 0, 0)
 Checkbox square frame color.
#define WTK_CHECKBOX_SELECT_COLOR   GFX_COLOR(128, 0, 0)
 Checkbox square select mark color.
#define WTK_CHECKBOX_CAPTION_COLOR   GFX_COLOR(255, 255, 255)
 Checkbox caption text color.

Define Documentation

#define WTK_CHECKBOX_BOX_COLOR   GFX_COLOR(0, 0, 0)

Checkbox square frame color.

Definition at line 234 of file wtk.h.

Referenced by wtk_check_box_handler().

#define WTK_CHECKBOX_BOX_SIZE   8

Size of checkbox square.

Definition at line 209 of file wtk.h.

Referenced by wtk_check_box_handler(), and wtk_check_box_size_hint().

#define WTK_CHECKBOX_BOX_X   0

Checkbox square X offset.

Definition at line 214 of file wtk.h.

Referenced by wtk_check_box_handler().

#define WTK_CHECKBOX_BOX_Y   0

Checkbox square Y offset.

Definition at line 219 of file wtk.h.

Referenced by wtk_check_box_handler().

#define WTK_CHECKBOX_CAPTION_COLOR   GFX_COLOR(255, 255, 255)

Checkbox caption text color.

Definition at line 244 of file wtk.h.

Referenced by wtk_check_box_handler().

#define WTK_CHECKBOX_CAPTION_X   (WTK_CHECKBOX_BOX_SIZE + 4)

Checkbox caption text X offset.

Definition at line 224 of file wtk.h.

Referenced by wtk_check_box_handler(), and wtk_check_box_size_hint().

#define WTK_CHECKBOX_CAPTION_Y   0

Checkbox caption text Y offset.

Definition at line 229 of file wtk.h.

Referenced by wtk_check_box_handler(), and wtk_check_box_size_hint().

#define WTK_CHECKBOX_SELECT_COLOR   GFX_COLOR(128, 0, 0)

Checkbox square select mark color.

Definition at line 239 of file wtk.h.

Referenced by wtk_check_box_handler().


Enumeration Type Documentation

Valid states for check box, relevant to pointer and keyboard operations.

For internal use only.

Enumerator:
WTK_CHECKBOX_NORMAL 

Normal state, no highlight or press.

WTK_CHECKBOX_PRESSED 

Widget pressed, action occurs when released.

Definition at line 54 of file wtk_check_box.c.


Function Documentation

struct win_window* wtk_check_box_as_child ( struct wtk_check_box check_box  )  [read]

This function returns a reference to the window that should be used when managing the widget, such as move, resize, destroy and reparenting.

Parameters:
check_box Check box widget to manage.
Returns:
Window to be used for managing the check box.

Definition at line 89 of file wtk_check_box.c.

References assert, and wtk_check_box::container.

struct wtk_check_box* wtk_check_box_create ( struct win_window parent,
struct win_area const *  area,
char const *  caption,
bool  selected,
win_command_t  command 
) [read]

This function creates a new check box widget. It allocates required memory and intializes necessary windows to create the widget. If there is not enough memory, the function returns NULL.

To destroy the widget and all its contents, and free its memory, call win_destroy() on the check box' child reference, given by wtk_check_box_as_child(), like this: "win_destroy(wtk_check_box_as_child(my_check_box_ptr));". Usually it will be destroyed automatically when it's parent is destroyed.

Parameters:
parent Parent window, possibly wtk_frame_as_parent(my_frame_ptr).
area Area of the internal contents.
caption Pointer to caption string. Will be copied into widget.
selected Initial state of check box, true if checked/selected.
command Command to send to parent window. Must be non-zero to be enabled.
Returns:
Pointer to check box, or NULL if failed.

Definition at line 333 of file wtk_check_box.c.

References win_attributes::area, assert, win_attributes::background, win_attributes::behavior, wtk_check_box::caption, wtk_check_box::command, wtk_check_box::container, win_attributes::custom, win_attributes::event_handler, membag_alloc(), membag_free(), wtk_check_box::selected, wtk_check_box::state, strlen(), WIN_BEHAVIOR_REDRAW_PARENT, win_create(), wtk_check_box_handler(), WTK_CHECKBOX_NORMAL, and wtk_copy_string().

static bool wtk_check_box_handler ( struct win_window win,
enum win_event_type  type,
void const *  data 
) [static]
bool wtk_check_box_is_selected ( struct wtk_check_box const *  check_box  ) 

This function returns true if the check box is selected.

Returns:
True if check box is selected.

Definition at line 130 of file wtk_check_box.c.

References assert, and wtk_check_box::selected.

void wtk_check_box_set ( struct wtk_check_box check_box,
bool  selected 
)

This function sets the value of the check box according to the "selected" parameter. The graphics will be updated if the box is visible.

Parameters:
check_box Check box to update.
selected Value to set for checkbox. True if check box is selected, false otherwise

Definition at line 118 of file wtk_check_box.c.

References assert, wtk_check_box::container, wtk_check_box::selected, and win_redraw().

void wtk_check_box_size_hint ( struct win_point size,
const char *  caption 
)

Get minimum widget size.

This function returns the minimum size that is required for showing the full widget and the caption.

Return values:
size Suggested size for the widget
Parameters:
caption Pointer to caption string to use for widget.

Definition at line 302 of file wtk_check_box.c.

References assert, gfx_get_string_bounding_box(), font::height, max_s, font::scale, sysfont, WTK_CHECKBOX_BOX_SIZE, WTK_CHECKBOX_CAPTION_X, and WTK_CHECKBOX_CAPTION_Y.

void wtk_check_box_toggle ( struct wtk_check_box check_box  ) 

This function toggles the value of a check box. If it is not selected, it will be set to a selected/checked state, and vice versa. The graphics will be updated if the box is visible.

Parameters:
check_box Check box to toggle.

Definition at line 102 of file wtk_check_box.c.

References assert, wtk_check_box::container, wtk_check_box::selected, and win_redraw().

Referenced by wtk_check_box_handler().

Generated on Thu Apr 29 15:18:22 2010 for display-training by  doxygen 1.6.3