drivers/gfx/hx8347a/gfx_hx8347a.c File Reference

Implementation of graphics routines for HX8347A compatible displays. More...

#include <clk/sys.h>
#include <gpio.h>
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
#include <delay.h>
#include <assert.h>
#include <gfx/gfx.h>
#include "hx8347a_regs.h"

Go to the source code of this file.

Functions

static void gfx_set_register (uint8_t address, uint8_t bitmask)
static void gfx_clear_register (uint8_t address, uint8_t bitmask)
static void gfx_reset_display (void)
static void gfx_exit_standby (void)
static void gfx_display_init_all (void)
void gfx_init (void)
 Initialize the low-level graphics device driver.
void gfx_sync (void)
 Synchronize access to the display.
void gfx_set_clipping (gfx_coord_t min_x, gfx_coord_t min_y, gfx_coord_t max_x, gfx_coord_t max_y)
 Set the clipping region.
void gfx_set_orientation (uint8_t flags)
 Change display orientation.
gfx_coord_t gfx_get_width (void)
 Return the current width of the screen.
gfx_coord_t gfx_get_height (void)
 Return the current height of the screen.
gfx_color_t gfx_color (uint8_t r, uint8_t g, uint8_t b)
 Generate native color value from R/G/B values.
gfx_color_t gfx_get_pixel (gfx_coord_t x, gfx_coord_t y)
 Get the color of a pixel on the display.
void gfx_draw_pixel (gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
 Draw a single pixel on the screen.
void gfx_draw_line_pixel (gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
 Draw a single pixel on the screen (for lines, apparently).
void gfx_set_top_left_limit (gfx_coord_t x, gfx_coord_t y)
 Set the top-left limit for the display.
void gfx_set_bottom_right_limit (gfx_coord_t x, gfx_coord_t y)
 Set the bottom-right limit for the display.
void gfx_set_limits (gfx_coord_t x1, gfx_coord_t y1, gfx_coord_t x2, gfx_coord_t y2)
 Set the limits for the display.

Variables

gfx_coord_t gfx_width
 Current width of screen.
gfx_coord_t gfx_height
 Current height of screen.

Detailed Description

Implementation of graphics routines for HX8347A compatible displays.

Copyright (C) 2009 - 2010 Atmel Corporation. All rights reserved.

Definition in file gfx_hx8347a.c.


Function Documentation

static void gfx_clear_register ( uint8_t  address,
uint8_t  bitmask 
) [static]

For internal use only.

Read-modify-write shortcut to clear bits in a register.

Definition at line 80 of file gfx_hx8347a.c.

References gfx_read_register(), and gfx_write_register().

Referenced by gfx_exit_standby().

static void gfx_display_init_all ( void   )  [static]

For internal use only.

Full display init function as described in EDT appnote

Definition at line 109 of file gfx_hx8347a.c.

References gfx_write_register(), and udelay().

Referenced by gfx_init().

static void gfx_exit_standby ( void   )  [static]

For internal use only.

Send display commands to exit standby mode.

Definition at line 100 of file gfx_hx8347a.c.

References gfx_clear_register(), gfx_set_register(), and udelay().

Referenced by gfx_init().

static void gfx_reset_display ( void   )  [static]

For internal use only.

Reset display using digital control interface.

Definition at line 90 of file gfx_hx8347a.c.

References gpio_set_value(), and udelay().

Referenced by gfx_init().

static void gfx_set_register ( uint8_t  address,
uint8_t  bitmask 
) [static]

For internal use only.

Read-modify-write shortcut to set bits in a register.

Definition at line 70 of file gfx_hx8347a.c.

References gfx_read_register(), and gfx_write_register().

Referenced by gfx_exit_standby().

Generated on Thu Apr 29 15:18:22 2010 for display-training by  doxygen 1.6.3