include/gfx/gfx.h File Reference

General graphics routines header file. More...

#include <assert.h>
#include <hugemem.h>
#include <progmem.h>

Go to the source code of this file.

Data Structures

struct  font
 Storage structure for font metadata. More...
struct  gfx_bitmap
 Storage structure for bitmap pixel data and metadata. More...

Defines

Circle Sector Definitions

#define GFX_OCTANT0   (1 << 0)
 Bitmask for drawing circle octant 0.
#define GFX_OCTANT1   (1 << 1)
 Bitmask for drawing circle octant 1.
#define GFX_OCTANT2   (1 << 2)
 Bitmask for drawing circle octant 2.
#define GFX_OCTANT3   (1 << 3)
 Bitmask for drawing circle octant 3.
#define GFX_OCTANT4   (1 << 4)
 Bitmask for drawing circle octant 4.
#define GFX_OCTANT5   (1 << 5)
 Bitmask for drawing circle octant 5.
#define GFX_OCTANT6   (1 << 6)
 Bitmask for drawing circle octant 6.
#define GFX_OCTANT7   (1 << 7)
 Bitmask for drawing circle octant 7.
#define GFX_QUADRANT0   (GFX_OCTANT0 | GFX_OCTANT1)
 Bitmask for drawing circle quadrant 0.
#define GFX_QUADRANT1   (GFX_OCTANT2 | GFX_OCTANT3)
 Bitmask for drawing circle quadrant 1.
#define GFX_QUADRANT2   (GFX_OCTANT4 | GFX_OCTANT5)
 Bitmask for drawing circle quadrant 2.
#define GFX_QUADRANT3   (GFX_OCTANT6 | GFX_OCTANT7)
 Bitmask for drawing circle quadrant 3.
#define GFX_LEFTHALF   (GFX_QUADRANT3 | GFX_QUADRANT0)
 Bitmask for drawing left half of circle.
#define GFX_TOPHALF   (GFX_QUADRANT0 | GFX_QUADRANT1)
 Bitmask for drawing top half of circle.
#define GFX_RIGHTHALF   (GFX_QUADRANT1 | GFX_QUADRANT2)
 Bitmask for drawing right half of circle.
#define GFX_BOTTOMHALF   (GFX_QUADRANT2 | GFX_QUADRANT3)
 Bitmask for drawing bottom half of circle.
#define GFX_WHOLE   0xFF
 Bitmask for drawing whole circle.
Flags for gfx_set_orientation()

#define GFX_FLIP_X   1
 Bitmask for flipping X for gfx_set_orientation.
#define GFX_FLIP_Y   2
 Bitmask for flipping Y for gfx_set_orientation.
#define GFX_SWITCH_XY   4
 Bitmask for swapping X and Y for gfx_set_orientation.

Enumerations

enum  font_data_type { FONT_LOC_PROGMEM, FONT_LOC_HUGEMEM }

Functions

static uint_fast8_t gfx_font_get_height (struct font *font)
 Get scaled height of a font.
static uint_fast8_t gfx_font_get_width (struct font *font)
 Get scaled width of a font.
Display driver management functions

void gfx_init (void)
 Initialize the low-level graphics device driver.
void gfx_sync (void)
 Synchronize access to the display.
Display Geometry

void gfx_set_orientation (uint8_t flags)
 Change display orientation.
gfx_coord_t gfx_get_width (void)
 Return the current width of the screen.
gfx_coord_t gfx_get_height (void)
 Return the current height of the screen.
Display Clipping

The display driver uses software and hardware clipping. In the graphics drivers software clipping is referred to as clipping and hardware clipping as limits.

Software clipping is used to ensure that nothing outside the set region is draw to the screen by any of the drawing functions. Eliminating unwanted drawing to the display will give a higher performance on displays which has a low bandwidth from the CPU. Software is enabled by the CONFIG_GFX_USE_CLIPPING configuration symbol. Clipping region is set with the gfx_set_clipping function.

Hardware clipping is used in the supported display drivers to efficiently draw primitives on a subset of the display. Example: when drawing a filled rectangle the limits is set to the size of the rectangle, and the driver sends the correct number of pixels to fill the entire rectangle. Without hardware clipping/limits the driver will have to to move the graphics ram (GRAM) position/pointer manually. Hardware clipping/limits is not used like software clipping to eliminate drawing outside a given region. Hardware clipping is set with the gfx_set_top_left_limit, gfx_set_bottom_right_limit and gfx_set_limits functions. In display drivers that do not use hardware clipping these functions will not have any effect.

void gfx_set_clipping (gfx_coord_t min_x, gfx_coord_t min_y, gfx_coord_t max_x, gfx_coord_t max_y)
 Set the clipping region.
void gfx_set_top_left_limit (gfx_coord_t x, gfx_coord_t y)
 Set the top-left limit for the display.
void gfx_set_bottom_right_limit (gfx_coord_t x, gfx_coord_t y)
 Set the bottom-right limit for the display.
void gfx_set_limits (gfx_coord_t x1, gfx_coord_t y1, gfx_coord_t x2, gfx_coord_t y2)
 Set the limits for the display.
Low-level pixel drawing operations

gfx_color_t gfx_color (uint8_t r, uint8_t g, uint8_t b)
 Generate native color value from R/G/B values.
void gfx_draw_pixel (gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
 Draw a single pixel on the screen.
void gfx_draw_line_pixel (gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
 Draw a single pixel on the screen (for lines, apparently).
gfx_color_t gfx_get_pixel (gfx_coord_t x, gfx_coord_t y)
 Get the color of a pixel on the display.
void gfx_duplicate_pixel (gfx_color_t color, uint32_t count)
 Draw multiple pixels all having the same color.
void gfx_copy_pixels_to_screen (const gfx_color_t *pixels, uint32_t count)
 Copy a block of pixels from data memory to screen.
void gfx_copy_progmem_pixels_to_screen (const gfx_color_t __progmem_arg *pixels, uint32_t count)
 Copy a block of pixels from program memory to screen.
void gfx_copy_hugemem_pixels_to_screen (const hugemem_ptr_t pixels, uint32_t count)
 Copy a block of pixels from hugemem to screen.
void gfx_copy_pixels_from_screen (gfx_color_t *pixels, uint32_t count)
 Copy a block of pixels from screen to data memory.
Graphics Drawing Primitives

void gfx_draw_char (char c, gfx_coord_t x, gfx_coord_t y, struct font *font, gfx_color_t color, gfx_color_t background_color)
 Draws a character to the display.
void gfx_draw_string (char *str, gfx_coord_t x, gfx_coord_t y, struct font *font, gfx_color_t color, gfx_color_t background_color)
 Draws a string to the display.
void gfx_draw_progmem_string (const char __progmem_arg *str, gfx_coord_t x, gfx_coord_t y, struct font *font, gfx_color_t color, gfx_color_t background_color)
void gfx_get_string_bounding_box (char const *str, struct font *font, gfx_coord_t *width, gfx_coord_t *height)
 Computes the bounding box of a string.
void gfx_get_progmem_string_bounding_box (const char __progmem_arg *str, struct font *font, gfx_coord_t *width, gfx_coord_t *height)
 Computes the bounding box of a string stored in progmem.

Variables

Screen geometry and clipping variables

For internal use only.

These global variables should not be accessed directly. They cannot be marked as private/static since they are shared within multiple C files of the graphics drivers.

Use gfx_set_clipping to change clipping region.

gfx_coord_t gfx_min_x
 Minimum X of current clipping region.
gfx_coord_t gfx_min_y
 Maximum Y of current clipping region.
gfx_coord_t gfx_max_x
 Minimum X of current clipping region.
gfx_coord_t gfx_max_y
 Maximum Y of current clipping region.
gfx_coord_t gfx_width
 Current width of screen.
gfx_coord_t gfx_height
 Current height of screen.

Bitmap functions and structures



enum  gfx_bitmap_type { BITMAP_SOLID, BITMAP_RAM, BITMAP_PROGMEM }
void gfx_draw_bitmap (const struct gfx_bitmap *bmp, gfx_coord_t x, gfx_coord_t y)
 Draw a bitmap.
void gfx_draw_bitmap_tiled (const struct gfx_bitmap *bmp, gfx_coord_t x1, gfx_coord_t y1, gfx_coord_t x2, gfx_coord_t y2, gfx_coord_t tile_origin_x, gfx_coord_t tile_origin_y)
 Draw a bitmap to the screen tiled to cover the output area.
void gfx_put_bitmap (const struct gfx_bitmap *bmp, gfx_coord_t map_x, gfx_coord_t map_y, gfx_coord_t x, gfx_coord_t y, gfx_coord_t width, gfx_coord_t height)
 Write a rectangular block of pixels from a bitmap to the screen.

Detailed Description

General graphics routines header file.

Copyright (C) 2009 - 2010 Atmel Corporation. All rights reserved.

Definition in file gfx.h.

Generated on Thu Apr 29 15:18:22 2010 for display-training by  doxygen 1.6.3