util/gfx/wtk_slider.c File Reference

Slider widget implementation. More...

#include <stdint.h>
#include <stdlib.h>
#include <assert.h>
#include <membag.h>
#include <string.h>
#include <gfx/wtk.h>

Go to the source code of this file.

Data Structures

struct  wtk_slider
 Slider control struct. More...



enum  wtk_slider_state { WTK_SLIDER_NORMAL, WTK_SLIDER_MOVING }
 

Valid states for slider, relevant to pointer operations.

More...
struct win_windowwtk_slider_as_child (struct wtk_slider *slider)
 Get pointer to slider window.
bool wtk_slider_is_moving (struct wtk_slider const *slider)
 Get slider status.
uint8_t wtk_slider_get_value (struct wtk_slider const *slider)
 Get slider value.
bool wtk_slider_set_value (struct wtk_slider *slider, uint8_t value)
 Set new slider value.
static bool wtk_slider_handler (struct win_window *win, enum win_event_type type, void const *data)
 Slider event handler.
struct wtk_sliderwtk_slider_create (struct win_window *parent, struct win_area const *area, uint8_t maximum, uint8_t value, uint8_t option, win_command_t command)
 Create a new slider widget.

Detailed Description

Slider widget implementation.

Copyright (C) 2009 - 2010 Atmel Corporation. All rights reserved.

Definition in file wtk_slider.c.

Generated on Thu Apr 29 14:09:58 2010 for display-demo by  doxygen 1.6.3