util/gfx/wtk.c File Reference

Graphical Widget toolkit. More...

#include <stdint.h>
#include <stdlib.h>
#include <assert.h>
#include <membag.h>
#include <string.h>
#include "gfx/wtk.h"

Go to the source code of this file.

Functions

uint8_t wtk_rescale_value (uint8_t value, uint8_t from_scale, uint8_t to_scale)
 Rescale 8-bit value.
void wtk_copy_string (char *dest, char const *source)
void wtk_shade_pixel (gfx_color_t *pixel, uint8_t alpha)

Detailed Description

Graphical Widget toolkit.

Copyright (C) 2009 - 2010 Atmel Corporation. All rights reserved.

Definition in file wtk.c.

Generated on Thu Apr 29 14:09:58 2010 for display-demo by  doxygen 1.6.3