pll_config Struct Reference
[PLL Management]

Hardware-specific representation of PLL configuration. More...

#include <pll.h>


Detailed Description

Hardware-specific representation of PLL configuration.

This structure contains one or more device-specific values representing the current PLL configuration. The contents of this structure is typically different from platform to platform, and the user should not access any fields except through the PLL configuration API.

Definition at line 69 of file pll.h.


The documentation for this struct was generated from the following file:
Generated on Thu Apr 29 14:10:02 2010 for display-demo by  doxygen 1.6.3