include/gfx/wtk.h File Reference

Graphical Widget toolkit. More...

#include <app/wtk.h>
#include <gfx/win.h>
#include <gfx/sysfont.h>

Go to the source code of this file.

Defines

Slider widget command event configuration options.

For use with the option parameter of wtk_slider_create

#define WTK_SLIDER_CMD_NONE   (0 << 0)
 Never issue command events. (Default option).
#define WTK_SLIDER_CMD_MOVE   (1 << 0)
 Issue command event whenever slider value is updated.
#define WTK_SLIDER_CMD_RELEASE   (1 << 1)
 Issue command event whenever slider is released.
Slider widget orientation configuration options.

For use with the option parameter of wtk_slider_create

#define WTK_SLIDER_HORIZONTAL   (0 << 0)
 Slider is horizontally oriented. (Default option).
#define WTK_SLIDER_VERTICAL   (1 << 2)
 Slider is vertically oriented.
Slider widget invert configuration options.

For use with the option parameter of wtk_slider_create

#define WTK_SLIDER_INVERT   (1 << 3)
 Slider value is inverted.
Progress bar orientation configuration options.

For use with the option parameter of wtk_progress_bar_create

#define WTK_PROGRESS_BAR_HORIZONTAL   (0 << 0)
 Progress bar is horizontally oriented.
#define WTK_PROGRESS_BAR_VERTICAL   (1 << 0)
 Progress bar is vertically oriented.
Progress bar widget invert configuration options.

For use with the option parameter of wtk_progress_bar_create

#define WTK_PROGRESS_BAR_INVERT   (1 << 1)
 Progress bar is inverted.

Typedefs

typedef bool(* wtk_frame_handler_t )(struct wtk_frame *frame, win_command_t command_data)
 Frame command event handler callback.
typedef bool(* wtk_basic_frame_command_handler_t )(struct wtk_basic_frame *basic_frame, win_command_t command_data)
 Basic frame command event handler callback.
typedef void(* wtk_basic_frame_draw_handler_t )(struct win_window *win, struct win_clip_region const *clip)
 Basic frame draw event handler callback.

Functions

struct wtk_framewtk_frame_create (struct win_window *parent, struct win_area const *area, char const *caption, bool allow_resize, wtk_frame_handler_t frame_handler, void *custom_data)
struct win_windowwtk_frame_as_parent (struct wtk_frame *frame)
struct win_windowwtk_frame_as_child (struct wtk_frame *frame)
void * wtk_frame_get_custom_data (struct wtk_frame const *frame)
struct wtk_basic_framewtk_basic_frame_create (struct win_window *parent, const struct win_area *area, struct gfx_bitmap *background, wtk_basic_frame_draw_handler_t draw_handler, wtk_basic_frame_command_handler_t frame_handler, void *custom_data)
 Create basic frame widget.
struct win_windowwtk_basic_frame_as_child (struct wtk_basic_frame *basic_frame)
 Get reference to basic frame window.
void * wtk_basic_frame_get_custom_data (const struct wtk_basic_frame *basic_frame)
 Get basic frame custom data.
struct wtk_buttonwtk_button_create (struct win_window *parent, struct win_area const *area, char const *caption, win_command_t command_data)
struct win_windowwtk_button_as_child (struct wtk_button *button)
void wtk_button_size_hint (struct win_point *size, const char *caption)
 Get minimum widget size.
struct wtk_check_boxwtk_check_box_create (struct win_window *parent, struct win_area const *area, char const *caption, bool selected, win_command_t command_data)
struct win_windowwtk_check_box_as_child (struct wtk_check_box *check_box)
void wtk_check_box_toggle (struct wtk_check_box *check_box)
void wtk_check_box_set (struct wtk_check_box *check_box, bool selected)
bool wtk_check_box_is_selected (struct wtk_check_box const *check_box)
void wtk_check_box_size_hint (struct win_point *size, const char *caption)
 Get minimum widget size.
struct wtk_radio_groupwtk_radio_group_create (void)
struct wtk_radio_buttonwtk_radio_button_create (struct win_window *parent, struct win_area const *area, char const *caption, bool selected, struct wtk_radio_group *group, win_command_t command_data)
struct win_windowwtk_radio_button_as_child (struct wtk_radio_button *radio_button)
void wtk_radio_button_select (struct wtk_radio_button *radio_button)
bool wtk_radio_button_is_selected (struct wtk_radio_button const *radio_button)
void wtk_radio_button_size_hint (struct win_point *size, const char *caption)
 Get minimum widget size.
struct wtk_sliderwtk_slider_create (struct win_window *parent, struct win_area const *area, uint8_t maximum, uint8_t value, uint8_t option, win_command_t command_data)
 Create a new slider widget.
struct win_windowwtk_slider_as_child (struct wtk_slider *slider)
 Get pointer to slider window.
bool wtk_slider_is_moving (struct wtk_slider const *slider)
 Get slider status.
uint8_t wtk_slider_get_value (struct wtk_slider const *slider)
 Get slider value.
bool wtk_slider_set_value (struct wtk_slider *slider, uint8_t value)
 Set new slider value.
struct wtk_labelwtk_label_create (struct win_window *parent, struct win_area const *area, char const *caption, bool align_right)
struct win_windowwtk_label_as_child (struct wtk_label *label)
bool wtk_label_change (struct wtk_label *label, const char *caption)
 Set new caption for label, return false if out of mem.
void wtk_label_size_hint (struct win_point *size, const char *caption)
 Get minimum widget size.
struct wtk_progress_barwtk_progress_bar_create (struct win_window *parent, struct win_area const *area, uint8_t maximum, uint8_t value, gfx_color_t fill_color, gfx_color_t background_color, uint8_t option)
 Create a new progress bar widget.
struct win_windowwtk_progress_bar_as_child (struct wtk_progress_bar *bar)
 Get pointer to progress bar window.
uint8_t wtk_progress_bar_get_value (struct wtk_progress_bar *bar)
 Get progress bar value.
bool wtk_progress_bar_set_value (struct wtk_progress_bar *bar, uint8_t value)
 Set new progress bar value.
void wtk_progress_bar_set_colors (struct wtk_progress_bar *bar, gfx_color_t color1, gfx_color_t color2)
 Set new progress bar colors.
uint8_t wtk_rescale_value (uint8_t value, uint8_t from_scale, uint8_t to_scale)
 Rescale 8-bit value.
void wtk_copy_string (char *dest, char const *source)
void wtk_shade_pixel (gfx_color_t *pixel, uint8_t alpha)

Detailed Description

Graphical Widget toolkit.

Copyright (C) 2009 - 2010 Atmel Corporation. All rights reserved.

Definition in file wtk.h.

Generated on Thu Apr 29 14:09:58 2010 for display-demo by  doxygen 1.6.3