include/gfx/win.h File Reference

Graphical Window system. More...

#include <app/win.h>
#include "gfx/gfx.h"
#include "membag.h"

Go to the source code of this file.

Data Structures

struct  win_point
 Geometric type describing a point or vector on screen, relative or absolute. More...
struct  win_area
 Geometric type describing an area on screen. More...
struct  win_clip_region
 Geometric type describing a clipping region, used when drawing windows. More...
struct  win_pointer_event
 Event data for all pointer events, e.g. touch screen or mouse. More...
struct  win_keyboard_event
 Event data for all keyboard events, e.g. full keyboards or smaller matrices. More...
struct  win_command_event
 Event data for command events, e.g. a button widget action command. More...
struct  win_event
 Event data for all events. More...
struct  win_attributes
 Window attribute data. More...

Defines

#define WIN_ATTR_POSITION   (1 << 0)
 Attribute mask for updating window position.
#define WIN_ATTR_SIZE   (1 << 1)
 Attribute mask for updating window size.
#define WIN_ATTR_BACKGROUND   (1 << 2)
 Attribute mask for updating window background type and color/pixmap.
#define WIN_ATTR_EVENTHANDLER   (1 << 3)
 Attribute mask for updating window event handler.
#define WIN_ATTR_BEHAVIOR   (1 << 4)
 Attribute mask for updating window behavior flags.
#define WIN_ATTR_CUSTOM   (1 << 5)
 Attribute mask for updating window custom data.
#define WIN_BEHAVIOR_RAISE_ON_PRESS   (1 << 0)
 Behavior mask for raising a window if itself or children are pressed.
#define WIN_BEHAVIOR_REDRAW_PARENT   (1 << 1)
 Behavior mask for requiring redraw of parent, e.g. transparent windows.

Typedefs

typedef bool(* win_event_handler_t )(struct win_window *win, enum win_event_type type, const void *data)
 Function pointer type for window event handlers.
typedef uint8_t win_behavior_t
 Data type holding window behavior flags.
typedef uint8_t win_attribute_mask_t
 Datatype holding attribute masks, used when updating attributes.

Enumerations

enum  win_pointer_event_type { WIN_POINTER_PRESS, WIN_POINTER_MOVE, WIN_POINTER_RELEASE }
 

Valid pointer event types.

More...
enum  win_keyboard_event_type { WIN_KEYBOARD_PRESS, WIN_KEYBOARD_RELEASE }
 

Valid keyboard event types.

More...
enum  win_event_type {
  WIN_EVENT_POINTER, WIN_EVENT_KEYBOARD, WIN_EVENT_COMMAND, WIN_EVENT_RAISE,
  WIN_EVENT_UNRAISE, WIN_EVENT_GETFOCUS, WIN_EVENT_LOSEFOCUS, WIN_EVENT_DRAW,
  WIN_EVENT_ATTRIBUTES, WIN_EVENT_DESTROY
}
 

Valid event types sent to a window event handler.

More...

Functions

void win_init (void)
 Initialize window system, set up root window, hook into touch driver.
struct win_windowwin_get_root (void)
 Get pointer to root window, i.e. desktop window.
struct win_windowwin_get_parent (const struct win_window *win)
 Get pointer to parent window, or NULL for root window.
void win_reset_root_geometry (void)
 Reset root window geometry to fullscreen, in case screen orientation change.
void win_set_attributes (struct win_window *win, const struct win_attributes *new_attributes, win_attribute_mask_t attribute_mask)
 Update window attributes, selected by the attribute mask.
void win_set_area (struct win_window *win, const struct win_area *new_area, win_attribute_mask_t attribute_mask)
 Update window position and/or size.
struct win_attributeswin_get_attributes (const struct win_window *win)
 Get a pointer to the window attribute struct.
struct win_areawin_get_area (const struct win_window *win)
 Get a pointer to the window area struct.
void * win_get_custom_data (const struct win_window *win)
 Get window custom data.
struct win_windowwin_create (struct win_window *parent, const struct win_attributes *attributes)
 Create a window and return its pointer. Use win_destroy() to free memory.
void win_destroy (struct win_window *win)
 Destroy a window and its contents including children, freeing up memory.
void win_reparent (struct win_window *child, struct win_window *new_parent)
 Change a window's parent.
void win_show (struct win_window *win)
 Show window. Will draw it on screen if parent is visible as well.
void win_redraw (const struct win_window *win)
 Redraw window and its contents, if visible.
void win_hide (struct win_window *win)
 Hide a window, removing it from screen if is was visible.
void win_raise (struct win_window *win)
 Raise window to top of all its siblings.
void win_lower (struct win_window *win)
 Lower window to bottom of all its siblings.
void win_queue_pointer_event (const struct win_pointer_event *event)
 Add a pointer event to the internal event queue.
void win_queue_keyboard_event (const struct win_keyboard_event *event)
 Add a keyboard event to the internal event queue.
void win_queue_command_event (const struct win_command_event *event)
 Add a command event to the internal event queue.
void win_process_events (void)
 Process all pending events from the internal queue.
void win_set_keyboard_focus (struct win_window *win)
 Set keyboard focus window or NULL, i.e. receiver of keyboard events.
void win_grab_pointer (struct win_window *win)
 Set pointer focus window or NULL, i.e. override pointer event receiver.
void win_translate_win_to_root (struct win_window const *start_win, struct win_point *return_pos)
 Compute window position on root window.
bool win_is_inside_clip (const struct win_clip_region *clip, const struct win_point *point)
 Return true if point is inside clipping region.
bool win_is_inside_area (const struct win_area *area, const struct win_point *point)
 Return true if point is inside area.
bool win_is_inside_window (const struct win_window *win, const struct win_point *point)
 Return true if global point is inside window.
void win_compute_union (struct win_area *area, const struct win_area *merge)
 Compute smallest box containing both areas, update first parameter.
bool win_compute_intersection (struct win_clip_region *clip, const struct win_area *area)
 Compute the intersection of clipping region and area, update clip.
bool win_compute_clipping (const struct win_window *win, const struct win_area *dirty_area, struct win_clip_region *clip)
 Compute clipping region in absolute coordinates from window and dirty area.

Detailed Description

Graphical Window system.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

Definition in file win.h.

Generated on Thu Apr 29 14:09:58 2010 for display-demo by  doxygen 1.6.3