|
Modules | |
| Slider widget options | |
Functions | |
| struct wtk_slider * | wtk_slider_create (struct win_window *parent, struct win_area const *area, uint8_t maximum, uint8_t value, uint8_t option, win_command_t command_data) |
| Create a new slider widget. | |
| struct win_window * | wtk_slider_as_child (struct wtk_slider *slider) |
| Get pointer to slider window. | |
| bool | wtk_slider_is_moving (struct wtk_slider const *slider) |
| Get slider status. | |
| uint8_t | wtk_slider_get_value (struct wtk_slider const *slider) |
| Get slider value. | |
| bool | wtk_slider_set_value (struct wtk_slider *slider, uint8_t value) |
| Set new slider value. | |
|
| |
| enum | wtk_slider_state { WTK_SLIDER_NORMAL, WTK_SLIDER_MOVING } |
Valid states for slider, relevant to pointer operations. More... | |
| static bool | wtk_slider_handler (struct win_window *win, enum win_event_type type, void const *data) |
| Slider event handler. | |
|
| |
| #define | WTK_SLIDER_PARENT_MOVE_SUPPORT 0 |
| Move support for sliders. | |
| #define | WTK_SLIDER_KNOB_WIDTH 10 |
| Width of the slider knob, including borders, in pixels. | |
| #define | WTK_SLIDER_BORDER_COLOR GFX_COLOR(0, 0, 0) |
| Color of all the slider's borders. | |
| #define | WTK_SLIDER_BACKGROUND_COLOR GFX_COLOR(128, 128, 128) |
| Color of the slider's background. | |
| #define | WTK_SLIDER_KNOB_COLOR_NORMAL GFX_COLOR(128, 0, 0) |
| Color of the slider knob when normal. | |
| #define | WTK_SLIDER_KNOB_COLOR_MOVING GFX_COLOR(255, 255, 255) |
| Color of the slider knob when moving. | |
| #define WTK_SLIDER_BACKGROUND_COLOR GFX_COLOR(128, 128, 128) |
Color of the slider's background.
Definition at line 329 of file wtk.h.
Referenced by wtk_slider_handler().
| #define WTK_SLIDER_BORDER_COLOR GFX_COLOR(0, 0, 0) |
Color of all the slider's borders.
Definition at line 324 of file wtk.h.
Referenced by wtk_slider_handler().
| #define WTK_SLIDER_KNOB_COLOR_MOVING GFX_COLOR(255, 255, 255) |
Color of the slider knob when moving.
Definition at line 339 of file wtk.h.
Referenced by wtk_slider_handler().
| #define WTK_SLIDER_KNOB_COLOR_NORMAL GFX_COLOR(128, 0, 0) |
Color of the slider knob when normal.
Definition at line 334 of file wtk.h.
Referenced by wtk_slider_handler().
| #define WTK_SLIDER_KNOB_WIDTH 10 |
Width of the slider knob, including borders, in pixels.
Definition at line 319 of file wtk.h.
Referenced by wtk_slider_create(), wtk_slider_handler(), and wtk_slider_set_value().
| #define WTK_SLIDER_PARENT_MOVE_SUPPORT 0 |
Move support for sliders.
This define enables and disables move support for sliders. Move support is needed if the application is using moving parent widgets/windows. If not needed, disable it to save CPU cycles.
Set to 1 to enable move support or 0 to disable move support.
| enum wtk_slider_state |
Valid states for slider, relevant to pointer operations.
For internal use only.
| WTK_SLIDER_NORMAL |
Normal state, no highlight or movement. |
| WTK_SLIDER_MOVING |
Slider is pressed, highlighted and moving. |
Definition at line 54 of file wtk_slider.c.
| struct win_window* wtk_slider_as_child | ( | struct wtk_slider * | slider | ) | [read] |
Get pointer to slider window.
Returns a reference to the window that should be used when managing the widget, such as destroying, moving or reparenting it.
| slider | Pointer to wtk_slider struct to manage. |
Definition at line 101 of file wtk_slider.c.
References assert, and wtk_slider::container.
Referenced by app_tank_launch().
| struct wtk_slider* wtk_slider_create | ( | struct win_window * | parent, | |
| struct win_area const * | area, | |||
| uint8_t | maximum, | |||
| uint8_t | value, | |||
| uint8_t | option, | |||
| win_command_t | command | |||
| ) | [read] |
Create a new slider widget.
Allocates the necessary memory and intializes the window and data for slider widgets. If there is not enough memory, the function returns NULL.
To destroy a slider widget and all its contents, and free its memory, call win_destroy() on the slider's child reference, given by wtk_slider_as_child(), like this: "win_destroy(wtk_slider_as_child(my_slider_ptr));".
Slider widgets fill the specified area and perform a mapping of the slider knob's position to a value between 0 and maximum. The length of the slider cannot exceed 255 pixels.
By default, the value 0 corresponds to the top-most position for a vertical slider, and the left-most position for a horizontal one. The slider's orientation and inversion of the value can be configured.
A slider can be configured to issue command events whenever its value is changed by a pointer and/or when a pointer releases it.
Refer to <gfx/wtk.h> for available configuration options.
| parent | Pointer to parent win_window struct. | |
| area | Pointer to win_area struct with position and size of the slider. | |
| maximum | Maximum value of the slider. | |
| value | Initial value of the slider. | |
| option | Configuration options for slider. See Slider widget options | |
| command | Command to send to parent window. Must be non-zero if used. |
Definition at line 466 of file wtk_slider.c.
References win_attributes::area, assert, win_attributes::background, win_attributes::behavior, wtk_slider::command, wtk_slider::container, win_attributes::custom, win_attributes::event_handler, wtk_slider::maximum, membag_alloc(), membag_free(), wtk_slider::option, wtk_slider::position, wtk_slider::root_pos, win_area::size, wtk_slider::state, wtk_slider::value, win_create(), win_translate_win_to_root(), wtk_rescale_value(), WTK_SLIDER_CMD_MOVE, WTK_SLIDER_CMD_RELEASE, wtk_slider_handler(), WTK_SLIDER_INVERT, WTK_SLIDER_KNOB_WIDTH, WTK_SLIDER_NORMAL, and WTK_SLIDER_VERTICAL.
Referenced by app_tank_launch().
| uint8_t wtk_slider_get_value | ( | struct wtk_slider const * | slider | ) |
Get slider value.
Returns the slider value, inverted if such behavior is configured.
| slider | Pointer to wtk_slider struct to get value from. |
Definition at line 132 of file wtk_slider.c.
References assert, wtk_slider::maximum, wtk_slider::option, wtk_slider::value, and WTK_SLIDER_INVERT.
Referenced by tank_worker(), and widget_frame_command_handler().
| static bool wtk_slider_handler | ( | struct win_window * | win, | |
| enum win_event_type | type, | |||
| void const * | data | |||
| ) | [static] |
Slider event handler.
This is the window event handler for slider widgets. It handles the three relevant event types sent to a slider's container window, i.e., drawing, pointer and destroy events.
For POINTER events, the slider value is only updated when the pointer moves, and not upon press or release events. The handler will grab the pointer and allow for it to move outside the actual widget window and still control the slider knob.
| win | Window receiving the event. | |
| type | The event type. | |
| data | Custom data, depending on event type. |
Definition at line 213 of file wtk_slider.c.
References assert, wtk_slider::command, wtk_slider::container, win_command_event::data, gfx_draw_filled_rect, gfx_draw_rect, wtk_slider::maximum, membag_free(), wtk_slider::option, win_clip_region::origin, wtk_slider::position, win_command_event::recipient, wtk_slider::root_pos, win_command_event::sender, win_area::size, wtk_slider::state, win_pointer_event::type, wtk_slider::value, WIN_EVENT_DESTROY, WIN_EVENT_DRAW, WIN_EVENT_POINTER, win_get_area(), win_get_custom_data(), win_grab_pointer(), WIN_POINTER_MOVE, WIN_POINTER_PRESS, WIN_POINTER_RELEASE, win_queue_command_event(), win_redraw(), win_translate_win_to_root(), wtk_rescale_value(), WTK_SLIDER_BACKGROUND_COLOR, WTK_SLIDER_BORDER_COLOR, WTK_SLIDER_CMD_MOVE, WTK_SLIDER_CMD_RELEASE, WTK_SLIDER_KNOB_COLOR_MOVING, WTK_SLIDER_KNOB_COLOR_NORMAL, WTK_SLIDER_KNOB_WIDTH, WTK_SLIDER_MOVING, WTK_SLIDER_NORMAL, and WTK_SLIDER_VERTICAL.
Referenced by wtk_slider_create().
| bool wtk_slider_is_moving | ( | struct wtk_slider const * | slider | ) |
Get slider status.
Returns whether or not the slider is currently being manipulated by pointer events, i.e., it is moving.
| slider | Pointer to wtk_slider struct to get status of. |
Definition at line 117 of file wtk_slider.c.
References assert, wtk_slider::state, and WTK_SLIDER_MOVING.
| bool wtk_slider_set_value | ( | struct wtk_slider * | slider, | |
| uint8_t | value | |||
| ) |
Set new slider value.
Updates the current value and issues a redrawing of the slider if its value was indeed changed. In this case, the new position of the slider knob is also computed.
| slider | Pointer to wtk_slider struct to set new value for. | |
| value | New value for the slider. |
Definition at line 155 of file wtk_slider.c.
References assert, wtk_slider::container, wtk_slider::maximum, wtk_slider::option, wtk_slider::position, win_area::size, wtk_slider::value, win_get_area(), win_redraw(), wtk_rescale_value(), WTK_SLIDER_INVERT, WTK_SLIDER_KNOB_WIDTH, and WTK_SLIDER_VERTICAL.
1.6.3