Widget toolkit
[Graphical display system]

Collaboration diagram for Widget toolkit:

Modules

 Frame widget
 Basic frame widget
 Button widget
 Check box widget
 Radio button widget
 Slider widget
 Label widget
 Progress bar widget

Typedefs

typedef uint16_t wtk_string_size_t
 Datatype holding size of strings.

Functions

uint8_t wtk_rescale_value (uint8_t value, uint8_t from_scale, uint8_t to_scale)
 Rescale 8-bit value.
void wtk_copy_string (char *dest, char const *source)
void wtk_shade_pixel (gfx_color_t *pixel, uint8_t alpha)



typedef uint8_t wtk_radio_group_size_t
 Datatype holding reference count for radio button groups.
#define WTK_RADIOBUTTON_RADIUS   4
 Radius of radio button circle.
#define WTK_RADIOBUTTON_BUTTON_X   (WTK_RADIOBUTTON_RADIUS)
 Radio button circle center X offset.
#define WTK_RADIOBUTTON_BUTTON_Y   (WTK_RADIOBUTTON_RADIUS)
 Radio button circle center Y offset.
#define WTK_RADIOBUTTON_CAPTION_X   ((WTK_RADIOBUTTON_RADIUS * 2) + 4)
 Radio button caption text X offset.
#define WTK_RADIOBUTTON_CAPTION_Y   0
 Radio button caption text Y offset.
#define WTK_RADIOBUTTON_BUTTON_COLOR   GFX_COLOR(0, 0, 0)
 Radio button circle color.
#define WTK_RADIOBUTTON_SELECT_COLOR   GFX_COLOR(128, 0, 0)
 Radio button select mark color.
#define WTK_RADIOBUTTON_CAPTION_COLOR   GFX_COLOR(255, 255, 255)
 Radio button caption text color.



#define WTK_FRAME_TOPBORDER   2
 Top frame border size.
#define WTK_FRAME_BOTTOMBORDER   4
 Bottom frame border size.
#define WTK_FRAME_RESIZE_RADIUS   7
 Radius of resize handle (second quadrant of circle).
#define WTK_FRAME_RESIZE_WIDTH   (WTK_FRAME_RESIZE_RADIUS + 1)
 Width of resize handle.
#define WTK_FRAME_RESIZE_HEIGHT   (WTK_FRAME_RESIZE_RADIUS + 1)
 Height of resize handle.
#define WTK_FRAME_MIN_WIDTH   (WTK_FRAME_RESIZE_WIDTH - WTK_FRAME_RIGHTBORDER)
 Minimum width of contents window of a frame.
#define WTK_FRAME_MIN_HEIGHT   (WTK_FRAME_RESIZE_HEIGHT - WTK_FRAME_BOTTOMBORDER)
 Minimum height of contents window of a frame.
#define WTK_FRAME_TITLEBAR_HEIGHT   9
 Height of titlebar area.
#define WTK_FRAME_CAPTION_X   3
 Caption text X offset inside title bar.
#define WTK_FRAME_CAPTION_Y   1
 Caption text Y offset inside title bar.
#define WTK_FRAME_BACKGROUND_COLOR   GFX_COLOR(192, 192, 128)
 Background color of frame contents window.
#define WTK_FRAME_BORDER_COLOR   GFX_COLOR(240, 240, 240)
 Frame border color.
#define WTK_FRAME_TITLEBAR_COLOR   GFX_COLOR(128, 128, 255)
 Background color of frame title bar.
#define WTK_FRAME_CAPTION_COLOR   GFX_COLOR(255, 255, 255)
 Caption text foreground color.
#define WTK_FRAME_RESIZE_COLOR   GFX_COLOR(64, 192, 192)
 Resize handle color.
#define WTK_FRAME_SHADESIZE   4
 Size of drop shadow area outside left/bottom/right border. 0 = no shadow.
#define WTK_FRAME_SHADES   { 252, 242, 220, 180 }
 Shade factor of drop shadow, first number is farthest from border.
#define WTK_DRAG_THRESHOLD   4
 Distance from origin before dragging operation kicks in.
#define WTK_DRAG_HANDLE_RADIUS   4
 Radius of drag origin and target handles.
#define WTK_DRAG_PIXMAP_SIZE   (WTK_DRAG_HANDLE_RADIUS * 2 + 1)
 Pixmap pixel count for storing drag handle background graphics.
#define WTK_DRAG_ORIGIN_COLOR   GFX_COLOR(255, 0, 0)
 Drag origin handle color.
#define WTK_DRAG_TARGET_COLOR   GFX_COLOR(0, 255, 0)
 Drag target handle color.



#define WTK_BUTTON_BACKGROUND_COLOR   GFX_COLOR(128, 128, 128)
 Color of button background (text color when highlighted).
#define WTK_BUTTON_CAPTION_COLOR   GFX_COLOR(255, 255, 255)
 Color of button text (background color when highlighted).



#define WTK_CHECKBOX_BOX_X   0
 Checkbox square X offset.
#define WTK_CHECKBOX_BOX_Y   0
 Checkbox square Y offset.
#define WTK_CHECKBOX_CAPTION_X   (WTK_CHECKBOX_BOX_SIZE + 4)
 Checkbox caption text X offset.
#define WTK_CHECKBOX_CAPTION_Y   0
 Checkbox caption text Y offset.
#define WTK_CHECKBOX_BOX_COLOR   GFX_COLOR(0, 0, 0)
 Checkbox square frame color.
#define WTK_CHECKBOX_SELECT_COLOR   GFX_COLOR(128, 0, 0)
 Checkbox square select mark color.
#define WTK_CHECKBOX_CAPTION_COLOR   GFX_COLOR(255, 255, 255)
 Checkbox caption text color.



#define WTK_SLIDER_KNOB_WIDTH   10
 Width of the slider knob, including borders, in pixels.
#define WTK_SLIDER_BORDER_COLOR   GFX_COLOR(0, 0, 0)
 Color of all the slider's borders.
#define WTK_SLIDER_BACKGROUND_COLOR   GFX_COLOR(128, 128, 128)
 Color of the slider's background.
#define WTK_SLIDER_KNOB_COLOR_NORMAL   GFX_COLOR(128, 0, 0)
 Color of the slider knob when normal.
#define WTK_SLIDER_KNOB_COLOR_MOVING   GFX_COLOR(255, 255, 255)
 Color of the slider knob when moving.

Detailed Description

The Widget toolkit implements many common widgets for use on a graphical display using the functionality of Window system and Graphics library

The following widgets are implemented:

Todo:
group some of the largest event handler functions into smaller helpers. They look too big and complex. By splitting up in smaller functions, the code would be easier to read and follow.
Todo:
generalize shaded frame to work for e.g. menu window as well. Now it's taylored for a wtk_frame. It could easily be changed to shade any rectangular area. The shading itself would be the same, only how to get the coordinates differ.
Todo:
ensure proper handling if resize through win_set_area is used on frame, since now it would resize container without doing anything to the other windows. The contents and resize window would look strange, malsized and malplaced. Somehow catch the ATTRIBUTES event and use the wtk_resize_frame() function. Move works fine though, since container is the parent window.
Todo:
optimize/generalize code for controls like checkbox, radiobutton, label, since A LOT of the code is equal: container frame, caption etc.

Define Documentation

#define WTK_BUTTON_BACKGROUND_COLOR   GFX_COLOR(128, 128, 128)

Color of button background (text color when highlighted).

Definition at line 192 of file wtk.h.

Referenced by wtk_button_handler().

#define WTK_BUTTON_CAPTION_COLOR   GFX_COLOR(255, 255, 255)

Color of button text (background color when highlighted).

Definition at line 197 of file wtk.h.

Referenced by wtk_button_handler().

#define WTK_CHECKBOX_BOX_COLOR   GFX_COLOR(0, 0, 0)

Checkbox square frame color.

Definition at line 234 of file wtk.h.

Referenced by wtk_check_box_handler().

#define WTK_CHECKBOX_BOX_X   0

Checkbox square X offset.

Definition at line 214 of file wtk.h.

Referenced by wtk_check_box_handler().

#define WTK_CHECKBOX_BOX_Y   0

Checkbox square Y offset.

Definition at line 219 of file wtk.h.

Referenced by wtk_check_box_handler().

#define WTK_CHECKBOX_CAPTION_COLOR   GFX_COLOR(255, 255, 255)

Checkbox caption text color.

Definition at line 244 of file wtk.h.

Referenced by wtk_check_box_handler().

#define WTK_CHECKBOX_CAPTION_X   (WTK_CHECKBOX_BOX_SIZE + 4)

Checkbox caption text X offset.

Definition at line 224 of file wtk.h.

Referenced by wtk_check_box_handler(), and wtk_check_box_size_hint().

#define WTK_CHECKBOX_CAPTION_Y   0

Checkbox caption text Y offset.

Definition at line 229 of file wtk.h.

Referenced by wtk_check_box_handler(), and wtk_check_box_size_hint().

#define WTK_CHECKBOX_SELECT_COLOR   GFX_COLOR(128, 0, 0)

Checkbox square select mark color.

Definition at line 239 of file wtk.h.

Referenced by wtk_check_box_handler().

#define WTK_DRAG_HANDLE_RADIUS   4

Radius of drag origin and target handles.

Definition at line 160 of file wtk.h.

Referenced by wtk_continue_drag(), wtk_start_drag(), and wtk_stop_drag().

#define WTK_DRAG_ORIGIN_COLOR   GFX_COLOR(255, 0, 0)

Drag origin handle color.

Definition at line 170 of file wtk.h.

Referenced by wtk_start_drag().

#define WTK_DRAG_PIXMAP_SIZE   (WTK_DRAG_HANDLE_RADIUS * 2 + 1)

Pixmap pixel count for storing drag handle background graphics.

Definition at line 165 of file wtk.h.

Referenced by wtk_continue_drag(), wtk_start_drag(), and wtk_stop_drag().

#define WTK_DRAG_TARGET_COLOR   GFX_COLOR(0, 255, 0)

Drag target handle color.

Definition at line 175 of file wtk.h.

Referenced by wtk_continue_drag(), and wtk_start_drag().

#define WTK_DRAG_THRESHOLD   4

Distance from origin before dragging operation kicks in.

Definition at line 155 of file wtk.h.

Referenced by wtk_is_drag_threshold_exceeded().

#define WTK_FRAME_BACKGROUND_COLOR   GFX_COLOR(192, 192, 128)

Background color of frame contents window.

Definition at line 120 of file wtk.h.

#define WTK_FRAME_BORDER_COLOR   GFX_COLOR(240, 240, 240)

Frame border color.

Definition at line 125 of file wtk.h.

Referenced by wtk_frame_handler().

#define WTK_FRAME_BOTTOMBORDER   4

Bottom frame border size.

Definition at line 75 of file wtk.h.

Referenced by wtk_frame_handler(), and wtk_resize_frame().

#define WTK_FRAME_CAPTION_COLOR   GFX_COLOR(255, 255, 255)

Caption text foreground color.

Definition at line 135 of file wtk.h.

Referenced by wtk_frame_handler().

#define WTK_FRAME_CAPTION_X   3

Caption text X offset inside title bar.

Definition at line 110 of file wtk.h.

Referenced by wtk_frame_handler().

#define WTK_FRAME_CAPTION_Y   1

Caption text Y offset inside title bar.

Definition at line 115 of file wtk.h.

Referenced by wtk_frame_handler().

#define WTK_FRAME_MIN_HEIGHT   (WTK_FRAME_RESIZE_HEIGHT - WTK_FRAME_BOTTOMBORDER)

Minimum height of contents window of a frame.

Definition at line 100 of file wtk.h.

Referenced by wtk_resize_frame().

#define WTK_FRAME_MIN_WIDTH   (WTK_FRAME_RESIZE_WIDTH - WTK_FRAME_RIGHTBORDER)

Minimum width of contents window of a frame.

Definition at line 95 of file wtk.h.

Referenced by wtk_resize_frame().

#define WTK_FRAME_RESIZE_COLOR   GFX_COLOR(64, 192, 192)

Resize handle color.

Definition at line 140 of file wtk.h.

Referenced by wtk_frame_handler().

#define WTK_FRAME_RESIZE_HEIGHT   (WTK_FRAME_RESIZE_RADIUS + 1)

Height of resize handle.

Definition at line 90 of file wtk.h.

Referenced by wtk_frame_create(), and wtk_resize_frame().

#define WTK_FRAME_RESIZE_RADIUS   7

Radius of resize handle (second quadrant of circle).

Definition at line 80 of file wtk.h.

Referenced by wtk_frame_handler().

#define WTK_FRAME_RESIZE_WIDTH   (WTK_FRAME_RESIZE_RADIUS + 1)

Width of resize handle.

Definition at line 85 of file wtk.h.

Referenced by wtk_frame_create(), and wtk_resize_frame().

#define WTK_FRAME_SHADES   { 252, 242, 220, 180 }

Shade factor of drop shadow, first number is farthest from border.

Definition at line 150 of file wtk.h.

#define WTK_FRAME_SHADESIZE   4

Size of drop shadow area outside left/bottom/right border. 0 = no shadow.

Definition at line 145 of file wtk.h.

Referenced by wtk_resize_frame().

#define WTK_FRAME_TITLEBAR_COLOR   GFX_COLOR(128, 128, 255)

Background color of frame title bar.

Definition at line 130 of file wtk.h.

Referenced by wtk_frame_handler().

#define WTK_FRAME_TITLEBAR_HEIGHT   9

Height of titlebar area.

Definition at line 105 of file wtk.h.

Referenced by wtk_frame_create(), wtk_frame_handler(), and wtk_resize_frame().

#define WTK_FRAME_TOPBORDER   2

Top frame border size.

Definition at line 70 of file wtk.h.

Referenced by wtk_frame_create(), wtk_frame_handler(), and wtk_resize_frame().

#define WTK_RADIOBUTTON_BUTTON_COLOR   GFX_COLOR(0, 0, 0)

Radio button circle color.

Definition at line 284 of file wtk.h.

Referenced by wtk_radio_button_handler().

#define WTK_RADIOBUTTON_BUTTON_X   (WTK_RADIOBUTTON_RADIUS)

Radio button circle center X offset.

Definition at line 264 of file wtk.h.

Referenced by wtk_radio_button_handler().

#define WTK_RADIOBUTTON_BUTTON_Y   (WTK_RADIOBUTTON_RADIUS)

Radio button circle center Y offset.

Definition at line 269 of file wtk.h.

Referenced by wtk_radio_button_handler(), and wtk_radio_button_size_hint().

#define WTK_RADIOBUTTON_CAPTION_COLOR   GFX_COLOR(255, 255, 255)

Radio button caption text color.

Definition at line 294 of file wtk.h.

Referenced by wtk_radio_button_handler().

#define WTK_RADIOBUTTON_CAPTION_X   ((WTK_RADIOBUTTON_RADIUS * 2) + 4)

Radio button caption text X offset.

Definition at line 274 of file wtk.h.

Referenced by wtk_radio_button_handler(), and wtk_radio_button_size_hint().

#define WTK_RADIOBUTTON_CAPTION_Y   0

Radio button caption text Y offset.

Definition at line 279 of file wtk.h.

Referenced by wtk_radio_button_handler(), and wtk_radio_button_size_hint().

#define WTK_RADIOBUTTON_RADIUS   4

Radius of radio button circle.

Definition at line 259 of file wtk.h.

Referenced by wtk_radio_button_handler(), and wtk_radio_button_size_hint().

#define WTK_RADIOBUTTON_SELECT_COLOR   GFX_COLOR(128, 0, 0)

Radio button select mark color.

Definition at line 289 of file wtk.h.

Referenced by wtk_radio_button_handler().

#define WTK_SLIDER_BACKGROUND_COLOR   GFX_COLOR(128, 128, 128)

Color of the slider's background.

Definition at line 329 of file wtk.h.

Referenced by wtk_slider_handler().

#define WTK_SLIDER_BORDER_COLOR   GFX_COLOR(0, 0, 0)

Color of all the slider's borders.

Definition at line 324 of file wtk.h.

Referenced by wtk_slider_handler().

#define WTK_SLIDER_KNOB_COLOR_MOVING   GFX_COLOR(255, 255, 255)

Color of the slider knob when moving.

Definition at line 339 of file wtk.h.

Referenced by wtk_slider_handler().

#define WTK_SLIDER_KNOB_COLOR_NORMAL   GFX_COLOR(128, 0, 0)

Color of the slider knob when normal.

Definition at line 334 of file wtk.h.

Referenced by wtk_slider_handler().

#define WTK_SLIDER_KNOB_WIDTH   10

Width of the slider knob, including borders, in pixels.

Definition at line 319 of file wtk.h.

Referenced by wtk_slider_create(), wtk_slider_handler(), and wtk_slider_set_value().


Typedef Documentation

Datatype holding reference count for radio button groups.

Definition at line 255 of file wtk.h.

Datatype holding size of strings.

Definition at line 51 of file wtk.h.


Function Documentation

void wtk_copy_string ( char *  dest,
char const *  source 
)

This function copies the string contents, including the zero terminator, from source to destination. The caller is responsible for providing memory for the destination string, either on the stack, static, or dynamically allocated.

Parameters:
dest Destination string.
source Source string, zero terminated.

Referenced by wtk_button_create(), wtk_check_box_create(), wtk_frame_create(), wtk_label_change(), wtk_label_create(), and wtk_radio_button_create().

uint8_t wtk_rescale_value ( uint8_t  value,
uint8_t  from_scale,
uint8_t  to_scale 
)

Rescale 8-bit value.

For internal use only.

This function is used by, e.g., the slider widget for computing the slider knob position from a given value and vice versa. It returns a value with the same data width as the input, meaning value cannot exceed from_scale, or overflows will occur.

The formula is:

 new_value = (value / from_scale) * to_scale 
Todo:
Revisit, support larger integers given a config symbol.
Parameters:
value Value to rescale.
from_scale Maximum of old scale for value.
to_scale Maximum of scale for new value.
Returns:
Rescaled 8-bit value.

Referenced by wtk_progress_bar_create(), wtk_progress_bar_set_value(), wtk_slider_create(), wtk_slider_handler(), and wtk_slider_set_value().

void wtk_shade_pixel ( gfx_color_t pixel,
uint8_t  alpha 
)

This function shades one pixel. Alpha equal to 0 gives a black pixel. Alpha equal to 255 gives an untouched pixel.

Note:
Color format is "red:green:blue" (5:6:5), but bytes are swapped, so the result is not rrrrr:gggggg:bbbbb, but ggg:bbbbb:rrrrr:ggg.
Parameters:
pixel Pointer to pixel to shade.
alpha Shade value. Lower value gives blacker pixel.
Generated on Thu Apr 29 14:09:59 2010 for display-demo by  doxygen 1.6.3