AT45 DataFlash Device Driver

Collaboration diagram for AT45 DataFlash Device Driver:

Data Structures

struct  at45_device
 AT45 DataFlash device. More...

Modules

 AT45 device driver internals

Typedefs

typedef bool(* at45_next_call_t )(struct at45_device *at45d)

Enumerations

enum  at45_device_flag { AT45_FLAG_VALID, AT45_FLAG_PROTECTED }
 

AT45 device flags.

More...

Functions

bool at45_wait_ready (struct at45_device *at45d)
 Actively wait for AT45 device to be ready.
bool at45_identify (struct at45_device *at45d)
 Identify AT45 device.
void at45_device_init (struct at45_device *at45d, spi_id_t spi_id, struct spi_master *spim, struct spi_device *spid)
 Initialize AT45 struct.
static void at45_request (struct at45_device *at45d, struct workqueue_task *task)
 Request exclusive access to AT45 device.
static void at45_release (struct at45_device *at45d)
 Release exclusive access to AT45 device.
static void at45_select (struct at45_device *at45d)
 Select AT45 device (Chip select).
static void at45_deselect (struct at45_device *at45d)
 De-select AT45 device (Chip de-select).
static void at45_write_cmd (struct at45_device *at45d, uint8_t size)
 Write command and other opcodes to AT45 device.
static void at45_read_rsp (struct at45_device *at45d, uint8_t size)
 Read response from AT45 device.
static void at45_cmd_read_status_reg (struct at45_device *at45d)
 Write AT45 device command: read status register.
static void at45_cmd_read_id (struct at45_device *at45d)
 Write AT45 device command: read ID.
static void at45_cmd_cont_array_read (struct at45_device *at45d, uint16_t page, uint16_t pos)
 Write AT45 device command: continous array read.
static void at45_cmd_buffer_1_write (struct at45_device *at45d, uint16_t pos)
 Write AT45 device command: buffer 1 write.
static void at45_cmd_main_memory_to_buffer_1_transfer (struct at45_device *at45d, uint16_t page)
 Write AT45 device command: main memory to buffer 1 transfer.
static void at45_cmd_buffer_1_main_memory_program_with_erase (struct at45_device *at45d, uint16_t page)
 Write AT45 device command: buffer 1 main memory program with erase.
static void at45_read_buf_list (struct at45_device *at45d, struct slist *buf_list)
 Read from AT45 device into buffer list.
static void at45_write_buf_list (struct at45_device *at45d, struct slist *buf_list)
 Write from buffer list into AT45 device.
static bool at45_rsp_status_is_ready (struct at45_device *at45d)
 Test if AT45 device status register bit is set to ready.
static bool at45_rsp_status_is_protected (struct at45_device *at45d)
 Test if AT45 device status register bit is set to protected.

Detailed Description

This is a driver for AT45 DataFlash devices.

It's initalized by at45_device_init() with a pre-allocated at45_device and SPI ID, master and device references.

Exclusive access is requested with at45_request(), and on access granted the supplied workqueue_task is scheduled to run and it's possible to call different access methods. These access methods can initiate some driver action which will re-schedule the task when ready.

Exclusive access must be ended with at45_release(). And this will start any other pending requests, or set it available.


Typedef Documentation

typedef bool(* at45_next_call_t)(struct at45_device *at45d)

For internal use only.

Next function definition for chained calls

Definition at line 75 of file at45_device.h.


Enumeration Type Documentation

AT45 device flags.

Enumerator:
AT45_FLAG_VALID 

Valid AT45 device detected.

AT45_FLAG_PROTECTED 

Device is protected from write operations.

Definition at line 63 of file at45_device.h.


Function Documentation

static void at45_cmd_buffer_1_main_memory_program_with_erase ( struct at45_device at45d,
uint16_t  page 
) [inline, static]

Write AT45 device command: buffer 1 main memory program with erase.

Parameters:
at45d AT45 device struct
page Page address
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 294 of file at45_device.h.

References assert, AT45_CMD_BUFFER_1_MAIN_MEMORY_PROGRAM_WITH_ERASE, AT45_PAGE_ADDR_MASK, at45_write_cmd(), and at45_device::cmdrsp.

static void at45_cmd_buffer_1_write ( struct at45_device at45d,
uint16_t  pos 
) [inline, static]

Write AT45 device command: buffer 1 write.

Parameters:
at45d AT45 device struct
pos Position in page
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 253 of file at45_device.h.

References assert, AT45_CMD_BUFFER_1_WRITE, AT45_PAGE_POS_MASK, at45_write_cmd(), and at45_device::cmdrsp.

static void at45_cmd_cont_array_read ( struct at45_device at45d,
uint16_t  page,
uint16_t  pos 
) [inline, static]

Write AT45 device command: continous array read.

Parameters:
at45d AT45 device struct
page Page address
pos Position in page
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 228 of file at45_device.h.

References assert, AT45_CMD_CONTINOUS_ARRAY_READ, AT45_PAGE_ADDR_MASK, AT45_PAGE_POS_MASK, at45_write_cmd(), and at45_device::cmdrsp.

static void at45_cmd_main_memory_to_buffer_1_transfer ( struct at45_device at45d,
uint16_t  page 
) [inline, static]

Write AT45 device command: main memory to buffer 1 transfer.

Parameters:
at45d AT45 device struct
page Page address
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 274 of file at45_device.h.

References assert, AT45_CMD_MAIN_MEMORY_TO_BUFFER_1_TRANSFER, AT45_PAGE_ADDR_MASK, at45_write_cmd(), and at45_device::cmdrsp.

static void at45_cmd_read_id ( struct at45_device at45d  )  [inline, static]

Write AT45 device command: read ID.

Parameters:
at45d AT45 device struct
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 213 of file at45_device.h.

References AT45_CMD_READ_ID, at45_write_cmd(), and at45_device::cmdrsp.

static void at45_cmd_read_status_reg ( struct at45_device at45d  )  [inline, static]

Write AT45 device command: read status register.

Parameters:
at45d AT45 device struct
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 200 of file at45_device.h.

References AT45_CMD_READ_STATUS_REG, at45_write_cmd(), and at45_device::cmdrsp.

static void at45_deselect ( struct at45_device at45d  )  [inline, static]

De-select AT45 device (Chip de-select).

Parameters:
at45d AT45 device struct
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 150 of file at45_device.h.

References spi_deselect_device(), at45_device::spi_id, at45_device::spid, and at45_device::spim.

void at45_device_init ( struct at45_device at45d,
spi_id_t  spi_id,
struct spi_master spim,
struct spi_device spid 
)

Initialize AT45 struct.

Parameters:
at45d AT45 device struct
spi_id SPI Module ID
spim SPI master struct
spid SPI device struct
bool at45_identify ( struct at45_device at45d  ) 

Identify AT45 device.

Extract status and device ID from device and process it.

Parameters:
at45d AT45 device struct
Return values:
false Not done yet. The task supplied in at45_request will be resceduled when it's ready to be called again.
true Operation completed. Variables at45d::size, at45d::page_size and at45d::flags have now been populated.

Referenced by dataflash_detect().

static void at45_read_buf_list ( struct at45_device at45d,
struct slist buf_list 
) [inline, static]

Read from AT45 device into buffer list.

Parameters:
at45d AT45 device struct
buf_list List of buffers
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 314 of file at45_device.h.

References at45_device::spi_id, spi_read_buf_list(), and at45_device::spim.

static void at45_read_rsp ( struct at45_device at45d,
uint8_t  size 
) [inline, static]

Read response from AT45 device.

This will read the response from the AT45 device into at45_device::cmdrsp .

When the response have been read the task will be rescheduled.

Parameters:
at45d AT45 device struct
size Size to be read
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 186 of file at45_device.h.

References assert, at45_device::cmdrsp, at45_device::spi_id, spi_read(), and at45_device::spim.

static void at45_release ( struct at45_device at45d  )  [inline, static]

Release exclusive access to AT45 device.

Parameters:
at45d AT45 device struct
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 126 of file at45_device.h.

References spi_release_bus(), and at45_device::spim.

static void at45_request ( struct at45_device at45d,
struct workqueue_task task 
) [inline, static]

Request exclusive access to AT45 device.

Once exclusive access is granted the task is scheduled to run.

Exclusive access must be ended with at45_release() in order for other requests to be run.

Parameters:
at45d AT45 device struct
task Task to run when ready

Definition at line 113 of file at45_device.h.

References spi_request_bus(), and at45_device::spim.

Referenced by dataflash_submit().

static bool at45_rsp_status_is_protected ( struct at45_device at45d  )  [inline, static]

Test if AT45 device status register bit is set to protected.

Parameters:
at45d AT45 device struct
Precondition:
Status register must have been read with at45_cmd_read_status_register first

Definition at line 353 of file at45_device.h.

References AT45_STATUS_PROTECT, and at45_device::cmdrsp.

static bool at45_rsp_status_is_ready ( struct at45_device at45d  )  [inline, static]

Test if AT45 device status register bit is set to ready.

Parameters:
at45d AT45 device struct
Precondition:
Status register must have been read with at45_cmd_read_status_register first

Definition at line 341 of file at45_device.h.

References AT45_STATUS_RDY, and at45_device::cmdrsp.

static void at45_select ( struct at45_device at45d  )  [inline, static]

Select AT45 device (Chip select).

Parameters:
at45d AT45 device struct
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 138 of file at45_device.h.

References at45_device::spi_id, spi_select_device(), at45_device::spid, and at45_device::spim.

bool at45_wait_ready ( struct at45_device at45d  ) 

Actively wait for AT45 device to be ready.

This must be called over and overagain until it returns true.

Parameters:
at45d AT45 device struct
Return values:
false Not done yet. The task supplied in at45_request will be resceduled when it's ready to be called again.
true Operation completed. Variables size, page_size and flags in at45 have now been populated.
static void at45_write_buf_list ( struct at45_device at45d,
struct slist buf_list 
) [inline, static]

Write from buffer list into AT45 device.

Parameters:
at45d AT45 device struct
buf_list List of buffers
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 328 of file at45_device.h.

References at45_device::spi_id, spi_write_buf_list(), and at45_device::spim.

static void at45_write_cmd ( struct at45_device at45d,
uint8_t  size 
) [inline, static]

Write command and other opcodes to AT45 device.

This will write the command from at45::cmdrsp to the AT45 device.

When the command have been written the task will be rescheduled.

Parameters:
at45d AT45 device struct
size Size to be written
Precondition:
Can only be called when exclusive access have been gained with at45_request

Definition at line 167 of file at45_device.h.

References assert, at45_device::cmdrsp, at45_device::spi_id, spi_write(), and at45_device::spim.

Referenced by at45_cmd_buffer_1_main_memory_program_with_erase(), at45_cmd_buffer_1_write(), at45_cmd_cont_array_read(), at45_cmd_main_memory_to_buffer_1_transfer(), at45_cmd_read_id(), and at45_cmd_read_status_reg().

Generated on Thu Apr 29 14:10:01 2010 for display-demo by  doxygen 1.6.3