chip/atxmega128a1/include/chip/spi.h File Reference

ATxmega128A1 specific SPI API. More...

#include <regs/xmega_spi.h>
#include <chip/memory-map.h>
#include <clk/sys.h>
#include <spi/spi_xmega.h>
#include <spi/spi_mega_xmega.h>

Go to the source code of this file.

Defines

#define SPI_ID_UART_FIRST   4
 First SPI ID which is a uart.
#define SPI_ID_LAST   11
 Last SPI ID.
#define SPI_ID_NATIVE_IS_ENABLED   false
 true if native SPI is enabled
#define SPI_ID_UART_IS_ENABLED   false
 true if uart SPI is enabled
spi_master derived type connections

#define spi_master_type0   SPI_MASTER_NATIVE_TYPE
#define spi_master_type1   SPI_MASTER_NATIVE_TYPE
#define spi_master_type2   SPI_MASTER_NATIVE_TYPE
#define spi_master_type3   SPI_MASTER_NATIVE_TYPE
spi_device derived type connections

#define spi_device_type0   SPI_DEVICE_NATIVE_TYPE
#define spi_device_type1   SPI_DEVICE_NATIVE_TYPE
#define spi_device_type2   SPI_DEVICE_NATIVE_TYPE
#define spi_device_type3   SPI_DEVICE_NATIVE_TYPE

Detailed Description

ATxmega128A1 specific SPI API.

Copyright (C) 2009 Atmel Corporation. All rights reserved.

Definition in file spi.h.

Generated on Thu Apr 29 14:09:58 2010 for display-demo by  doxygen 1.6.3