| Xmega Application Note | |||||
Copyright (c) 2010, Atmel Corporation All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
3. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file usb_drv.c.
#include "config.h"
#include "conf_usb.h"
#include "usb_drv.h"

Go to the source code of this file.
Functions | |
| uint8_t | usb_config_ep (uint8_t config0, uint8_t config1) |
| This function configures an endpoint with the selected type. | |
| void | usb_halt_endpoint (uint8_t ep_num) |
| This function sends a STALL handshake for the next Host request. A STALL handshake will be send for each next request untill a SETUP or a Clear Halt Feature occurs for this endpoint. | |
| uint8_t | usb_init_device (void) |
| This function initializes the USB device controller and configures the Default Control Endpoint. | |
| uint8_t | usb_read_packet (uint8_t ep_num, uint8_t *rbuf, uint8_t data_length) |
| This function moves the data stored in the selected endpoint fifo to the address specified by *rbuf. | |
| uint8_t | usb_select_enpoint_interrupt (void) |
| This function select the endpoint where an event occurs and returns the number of this endpoint. If no event occurs on the endpoints, this function returns 0. | |
| uint8_t | usb_send_packet (uint8_t ep_num, uint8_t *tbuf, uint8_t data_length) |
| This function moves the data pointed by tbuf to the selected endpoint fifo and sends it through the USB. | |
| uint8_t usb_config_ep | ( | uint8_t | config0, | |
| uint8_t | config1 | |||
| ) |
This function configures an endpoint with the selected type.
| config0 | ||
| config1 |
| Is_endpoint_configured. |
Definition at line 59 of file usb_drv.c.
References Is_endpoint_configured, Usb_allocate_memory, and Usb_enable_endpoint.
00060 { 00061 Usb_enable_endpoint(); 00062 UECFG0X = config0; 00063 UECFG1X = (UECFG1X & (1<<ALLOC)) | config1; 00064 Usb_allocate_memory(); 00065 return (Is_endpoint_configured()); 00066 }
| void usb_halt_endpoint | ( | uint8_t | ep_num | ) |
This function sends a STALL handshake for the next Host request. A STALL handshake will be send for each next request untill a SETUP or a Clear Halt Feature occurs for this endpoint.
| ep_num | number of the addressed endpoint |
Definition at line 153 of file usb_drv.c.
References Usb_enable_stall_handshake, and Usb_select_endpoint.
00154 { 00155 Usb_select_endpoint(ep_num); 00156 Usb_enable_stall_handshake(); 00157 }
| uint8_t usb_init_device | ( | void | ) |
This function initializes the USB device controller and configures the Default Control Endpoint.
| status |
Definition at line 165 of file usb_drv.c.
References DIRECTION_OUT, EP_CONTROL, Is_usb_endpoint_enabled, Is_usb_id_device, NYET_DISABLED, ONE_BANK, SIZE_64, TYPE_CONTROL, usb_configure_endpoint, Usb_select_device, and Usb_select_endpoint.
Referenced by ISR(), and usb_start_device().
00166 { 00167 Usb_select_device(); 00168 if(Is_usb_id_device()) 00169 { 00170 Usb_select_endpoint(EP_CONTROL); 00171 if(!Is_usb_endpoint_enabled()) 00172 { 00173 return usb_configure_endpoint(EP_CONTROL, \ 00174 TYPE_CONTROL, \ 00175 DIRECTION_OUT, \ 00176 SIZE_64, \ 00177 ONE_BANK, \ 00178 NYET_DISABLED); 00179 } 00180 } 00181 return false; 00182 }
| uint8_t usb_read_packet | ( | uint8_t | ep_num, | |
| uint8_t * | rbuf, | |||
| uint8_t | data_length | |||
| ) |
This function moves the data stored in the selected endpoint fifo to the address specified by *rbuf.
| ep_num | number of the addressed endpoint | |
| rbuf | aaddress of the first data to write with the USB data | |
| data_length | number of bytes to read |
| address | of the next uint8_t to send. |
Definition at line 131 of file usb_drv.c.
References Is_usb_read_enabled, Usb_read_byte, and Usb_select_endpoint.
00132 { 00133 uint8_t remaining_length; 00134 00135 remaining_length = data_length; 00136 Usb_select_endpoint(ep_num); 00137 00138 while(Is_usb_read_enabled() && (0 != remaining_length)){ 00139 *rbuf = Usb_read_byte(); 00140 remaining_length--; 00141 rbuf++; 00142 } 00143 return remaining_length; 00144 }
| uint8_t usb_select_enpoint_interrupt | ( | void | ) |
This function select the endpoint where an event occurs and returns the number of this endpoint. If no event occurs on the endpoints, this function returns 0.
| endpoint | number. |
Definition at line 75 of file usb_drv.c.
References Usb_interrupt_flags.
00076 { 00077 uint8_t interrupt_flags; 00078 uint8_t ep_num; 00079 00080 ep_num = 0; 00081 interrupt_flags = Usb_interrupt_flags(); 00082 00083 while(ep_num < 9){ 00084 if (interrupt_flags & 1){ 00085 return (ep_num); 00086 }else{ 00087 ep_num++; 00088 interrupt_flags = interrupt_flags >> 1; 00089 } 00090 } 00091 return 0; 00092 }
| uint8_t usb_send_packet | ( | uint8_t | ep_num, | |
| uint8_t * | tbuf, | |||
| uint8_t | data_length | |||
| ) |
This function moves the data pointed by tbuf to the selected endpoint fifo and sends it through the USB.
| ep_num | number of the addressed endpoint | |
| *tbuf | address of the first data to send | |
| data_length | number of bytes to send |
| address | of the next byte to send. |
Definition at line 106 of file usb_drv.c.
References Is_usb_write_enabled, Usb_select_endpoint, and Usb_write_byte.
00107 { 00108 uint8_t remaining_length; 00109 00110 remaining_length = data_length; 00111 Usb_select_endpoint(ep_num); 00112 while(Is_usb_write_enabled() && (0 != remaining_length)){ 00113 Usb_write_byte(*tbuf); 00114 remaining_length--; 00115 tbuf++; 00116 } 00117 return remaining_length; 00118 }
Generated on Mon Jan 18 09:26:12 2010 for AVR1907 Xplain USB Gateway by 1.5.5
|