| Xmega Application Note | |||||
Copyright (c) 2010, Atmel Corporation All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
3. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file avr_compiler.h.
#include <stdint.h>
#include <stdbool.h>
#include <stdlib.h>


Go to the source code of this file.
Defines | |
| #define | AVR_ENTER_CRITICAL_REGION() |
| This macro will protect the following code from interrupts. | |
| #define | AVR_LEAVE_CRITICAL_REGION() SREG = saved_sreg; |
| This macro must always be used in conjunction with AVR_ENTER_CRITICAL_REGION so the interrupts are enabled again. | |
| #define | F_CPU 2000000UL |
| Define default CPU frequency, if this is not already defined. | |
| #define AVR_ENTER_CRITICAL_REGION | ( | ) |
Value:
uint8_t volatile saved_sreg = SREG; \
cli();
Definition at line 58 of file avr_compiler.h.
Referenced by SW_USART_RX_Buffer_GetByte().
| #define AVR_LEAVE_CRITICAL_REGION | ( | ) | SREG = saved_sreg; |
This macro must always be used in conjunction with AVR_ENTER_CRITICAL_REGION so the interrupts are enabled again.
Definition at line 64 of file avr_compiler.h.
Referenced by SW_USART_RX_Buffer_GetByte().
| #define F_CPU 2000000UL |
Define default CPU frequency, if this is not already defined.
Definition at line 50 of file avr_compiler.h.
Generated on Mon Jan 18 09:26:09 2010 for AVR1907 Xplain USB Gateway by 1.5.5
|