| Xmega Application Note | |||||
#include <usb_descriptors.h>
Definition at line 201 of file usb_descriptors.h.
Data Fields | |
| uint8_t | bAlternateSetting |
| uint8_t | bDescriptorType |
| uint8_t | bInterfaceClass |
| uint8_t | bInterfaceNumber |
| uint8_t | bInterfaceProtocol |
| uint8_t | bInterfaceSubClass |
| uint8_t | bLength |
| uint8_t | bNumEndpoints |
| uint8_t | iInterface |
value to select alternate setting
Definition at line 205 of file usb_descriptors.h.
INTERFACE descriptor type
Definition at line 203 of file usb_descriptors.h.
Class code assigned by the USB
Definition at line 207 of file usb_descriptors.h.
Number of interface
Definition at line 204 of file usb_descriptors.h.
Protocol code assigned by the USB
Definition at line 209 of file usb_descriptors.h.
Sub-class code assigned by the USB
Definition at line 208 of file usb_descriptors.h.
size of this descriptor in bytes
Definition at line 202 of file usb_descriptors.h.
Number of EP except EP 0
Definition at line 206 of file usb_descriptors.h.
Index of string descriptor
Definition at line 210 of file usb_descriptors.h.
Generated on Mon Jan 18 09:26:15 2010 for AVR1907 Xplain USB Gateway by 1.5.5
|