AVR1631 - Energy Meter Reference Design with ATxmega32A4  Rev 1.0
 All Data Structures Files Functions Variables Typedefs Macros
clksys_driver.c File Reference

XMEGA Clock System driver source file. More...

#include "clksys_driver.h"

Go to the source code of this file.

Functions

void CCPWrite (volatile uint8_t *address, uint8_t value)
 CCP write helper function written in assembly.
void CLKSYS_XOSC_Config (OSC_FRQRANGE_t freqRange, bool lowPower32kHz, OSC_XOSCSEL_t xoscModeSelection)
 This function configures the external oscillator.
void CLKSYS_PLL_Config (OSC_PLLSRC_t clockSource, uint8_t factor)
 This function configures the internal high-frequency PLL.
uint8_t CLKSYS_Disable (uint8_t oscSel)
 This function disables the selected oscillator.
void CLKSYS_Prescalers_Config (CLK_PSADIV_t PSAfactor, CLK_PSBCDIV_t PSBCfactor)
 This function changes the prescaler configuration.
uint8_t CLKSYS_Main_ClockSource_Select (CLK_SCLKSEL_t clockSource)
 This function selects the main system clock source.
void CLKSYS_RTC_ClockSource_Enable (CLK_RTCSRC_t clockSource)
 This function selects a Real-Time Counter clock source.
void CLKSYS_AutoCalibration_Enable (uint8_t clkSource, bool extReference)
 This function enables automatic calibration of the selected internal oscillator.
void CLKSYS_XOSC_FailureDetection_Enable (void)
 This function enables the External Oscillator Failure Detection (XOSCFD) feature.
void CLKSYS_Configuration_Lock (void)
 This function lock the entire clock system configuration.

Detailed Description

XMEGA Clock System driver source file.

 This file contains the function implementations for the XMEGA Clock
 System driver.

 The driver is not intended for size and/or speed critical code, since
 most functions are just a few lines of code, and the function call
 overhead would decrease code performance. The driver is intended for
 rapid prototyping and documentation purposes for getting started with
 the XMEGA Clock System.

 For size and/or speed critical code, it is recommended to copy the
 function contents directly into your application instead of making
 a function call.

 Several functions use the following construct:
     "some_register = ... | (some_parameter ? SOME_BIT_bm : 0) | ..."
 Although the use of the ternary operator ( if ? then : else ) is
 discouraged, in some occasions the operator makes it possible to
 write pretty clean and neat code. In this driver, the construct is
 used to set or not set a configuration bit based on a boolean input
 parameter, such as the "some_parameter" in the example above.
Application note:
AVR1003: Using the XMEGA Clock System
Documentation
For comprehensive code documentation, supported compilers, compiler settings and supported devices see readme.html
Author
Atmel Corporation: http://www.atmel.com
Support email: avr@a.nosp@m.tmel.nosp@m..com
Revision:
2771
Date:
2009-09-11 11:54:26 +0200 (fr, 11 sep 2009)


Copyright (c) 2008, Atmel Corporation All rights reserved.

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

  1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
  1. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
  1. The name of ATMEL may not be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY ATMEL "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE EXPRESSLY AND SPECIFICALLY DISCLAIMED. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

Definition in file clksys_driver.c.

Function Documentation

void CCPWrite ( volatile uint8_t *  address,
uint8_t  value 
)

CCP write helper function written in assembly.

This function is written in assembly because of the timecritial operation of writing to the registers.

Parameters
addressA pointer to the address to write to.
valueThe value to put in to the register.

Definition at line 77 of file clksys_driver.c.

void CLKSYS_AutoCalibration_Enable ( uint8_t  clkSource,
bool  extReference 
)

This function enables automatic calibration of the selected internal oscillator.

Either the internal 32kHz RC oscillator or an external 32kHz crystal can be used as a calibration reference. The user must make sure that the selected reference is ready and running.

Parameters
clkSourceClock source to calibrate, either OSC_RC2MCREF_bm or OSC_RC32MCREF_bm.
extReferenceTrue if external crystal should be used as reference.

Definition at line 260 of file clksys_driver.c.

void CLKSYS_Configuration_Lock ( void  )

This function lock the entire clock system configuration.

This will lock the configuration until the next reset, or until the External Oscillator Failure Detections (XOSCFD) feature detects a failure and switches to internal 2MHz RC oscillator.

Definition at line 292 of file clksys_driver.c.

uint8_t CLKSYS_Disable ( uint8_t  oscSel)

This function disables the selected oscillator.

This function will disable the selected oscillator if possible. If it is currently used as a main system clock source, hardware will disregard the disable attempt, and this function will return zero. If it fails, change to another main system clock source and try again.

Parameters
oscSelBitmask of selected clock. Can be one of the following OSC_RC2MEN_bm, OSC_RC32MEN_bm, OSC_RC32KEN_bm, OSC_XOSCEN_bm, OSC_PLLEN_bm.
Returns
Non-zero if oscillator was disabled successfully.

Definition at line 187 of file clksys_driver.c.

uint8_t CLKSYS_Main_ClockSource_Select ( CLK_SCLKSEL_t  clockSource)

This function selects the main system clock source.

Hardware will disregard any attempts to select a clock source that is not enabled or not stable. If the change fails, make sure the source is ready and running and try again.

Parameters
clockSourceClock source to use as input for the system clock prescaler block.
Returns
Non-zero if change was successful.

Definition at line 225 of file clksys_driver.c.

void CLKSYS_PLL_Config ( OSC_PLLSRC_t  clockSource,
uint8_t  factor 
)

This function configures the internal high-frequency PLL.

Configuration of the internal high-frequency PLL to the correct values. It is used to define the input of the PLL and the factor of multiplication of the input clock source.

Note
Note that the oscillator cannot be used as a main system clock source without being enabled and stable first. Check the ready flag before using the clock. The macro CLKSYS_IsReady( _oscSel ) can be used to check this.
Parameters
clockSourceReference clock source for the PLL, must be above 0.4MHz.
factorPLL multiplication factor, must be from 1 to 31, inclusive.

Definition at line 167 of file clksys_driver.c.

void CLKSYS_Prescalers_Config ( CLK_PSADIV_t  PSAfactor,
CLK_PSBCDIV_t  PSBCfactor 
)

This function changes the prescaler configuration.

Change the configuration of the three system clock prescaler is one single operation. The user must make sure that the main CPU clock does not exceed recommended limits.

Parameters
PSAfactorPrescaler A division factor, OFF or 2 to 512 in powers of two.
PSBCfactorPrescaler B and C division factor, in the combination of (1,1), (1,2), (4,1) or (2,2).

Definition at line 206 of file clksys_driver.c.

void CLKSYS_RTC_ClockSource_Enable ( CLK_RTCSRC_t  clockSource)

This function selects a Real-Time Counter clock source.

Selects the clock source for use by the Real-Time Counter (RTC) and enables clock signal routing to the RTC module.

Parameters
clockSourceClock source to use for the RTC.

Definition at line 241 of file clksys_driver.c.

void CLKSYS_XOSC_Config ( OSC_FRQRANGE_t  freqRange,
bool  lowPower32kHz,
OSC_XOSCSEL_t  xoscModeSelection 
)

This function configures the external oscillator.

Note
Note that the oscillator cannot be used as a main system clock source without being enabled and stable first. Check the ready flag before using the clock. The macro CLKSYS_IsReady( _oscSel ) can be used to check this.
Parameters
freqRangeFrequency range for high-frequency crystal, does not apply for external clock or 32kHz crystals.
lowPower32kHzTrue of high-quality watch crystals are used and low-power oscillator is desired.
xoscModeSelectionCombined selection of oscillator type (or external clock) and startup times.

Definition at line 141 of file clksys_driver.c.

void CLKSYS_XOSC_FailureDetection_Enable ( void  )

This function enables the External Oscillator Failure Detection (XOSCFD) feature.

The feature will stay enabled until next reset. Note that the XOSCFD will issue the XOSCF Non-maskable Interrupt (NMI) regardless of any interrupt priorities and settings. Therefore, make sure that a handler is implemented for the XOSCF NMI when you enable it.

Definition at line 280 of file clksys_driver.c.